<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX28 standby error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288628#M34526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Victorien&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Seems like there is something wrong in battery driver's suspend callback, since you do NOT have an battery connected, I wonder whether battery driver would be active, can you add some debug message to see whether the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;mutex_lock&lt;/SPAN&gt; in &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;mxs_bat_suspend&lt;/SPAN&gt; routine has valid parameter. I remembered that on EVK board, there is fake battery circuit coming from regulator directly, can you double check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Nov 2013 02:11:56 GMT</pubDate>
    <dc:creator>AnsonHuang</dc:creator>
    <dc:date>2013-11-20T02:11:56Z</dc:date>
    <item>
      <title>iMX28 standby error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288627#M34525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm testing on an iMX28 EVK board the standby mode.&lt;/P&gt;&lt;P&gt;The command &lt;EM&gt;echo standby &amp;gt; /sys/power/state&lt;/EM&gt; works but I have an Oops error and it 's impossible to resume the processor. The log is&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;Freezing user space processes ... (elapsed 0.02 seconds) done.&lt;BR /&gt;Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.&lt;BR /&gt;Unable to handle kernel NULL pointer dereference at virtual address 000000dc&lt;BR /&gt;pgd = c7454000&lt;BR /&gt;[000000dc] *pgd=47dc3031, *pte=00000000, *ppte=00000000&lt;BR /&gt;Internal error: Oops: 817 [#1] PREEMPT&lt;BR /&gt;last sysfs file: /sys/devices/virtual/vc/vcsa63/dev&lt;BR /&gt;Modules linked in:&lt;BR /&gt;CPU: 0&amp;nbsp;&amp;nbsp;&amp;nbsp; Not tainted&amp;nbsp; (2.6.35.3-g215633e-dirty #71)&lt;BR /&gt;PC is at mutex_lock+0x10/0x24&lt;BR /&gt;LR is at mxs_bat_suspend+0x24/0x40&lt;BR /&gt;pc : [&amp;lt;c03c59cc&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;c02e6d48&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; psr: a0000013&lt;BR /&gt;sp : c7da7dd0&amp;nbsp; ip : c7da7de0&amp;nbsp; fp : c7da7ddc&lt;BR /&gt;r10: 00000002&amp;nbsp; r9 : 00000000&amp;nbsp; r8 : 00000000&lt;BR /&gt;r7 : c04ff75c&amp;nbsp; r6 : c04ff728&amp;nbsp; r5 : 000000dc&amp;nbsp; r4 : 00000000&lt;BR /&gt;r3 : c02e6d24&amp;nbsp; r2 : 00000000&amp;nbsp; r1 : 00000002&amp;nbsp; r0 : 000000dc&lt;BR /&gt;Flags: NzCv&amp;nbsp; IRQs on&amp;nbsp; FIQs on&amp;nbsp; Mode SVC_32&amp;nbsp; ISA ARM&amp;nbsp; Segment user&lt;BR /&gt;Control: 0005317f&amp;nbsp; Table: 47454000&amp;nbsp; DAC: 00000015&lt;BR /&gt;Process sh (pid: 1252, stack limit = 0xc7da6270)&lt;BR /&gt;Stack: (0xc7da7dd0 to 0xc7da8000)&lt;BR /&gt;7dc0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; c7da7df4 c7da7de0 c02e6d48 c03c59cc&lt;BR /&gt;7de0: 00000002 c03ebfa8 c7da7e04 c7da7df8 c02488e0 c02e6d34 c7da7e3c c7da7e08&lt;BR /&gt;7e00: c024b1ac c0248898 c7da7e3c c7da7e18 00000000 00000000 c7ce8300 c04ff728&lt;BR /&gt;7e20: c04ff728 00000002 00000000 c7fb3c98 c7da7e64 c7da7e40 c024bb00 c024b164&lt;BR /&gt;7e40: c04ff728 00000000 c04ff728 00000000 c051b1ac c04ff780 c7da7ea4 c7da7e68&lt;BR /&gt;7e60: c024be6c c024ba28 13cf29cc 00000023 13cf29cc 00000023 c04fe3d0 c74f7558&lt;BR /&gt;7e80: 00000000 00000000 00000001 003fffff c74f6000 00000008 c7da7ec4 c7da7ea8&lt;BR /&gt;7ea0: c007bdcc c024bb6c 00000000 00000001 00000007 c03ced50 c7da7edc c7da7ec8&lt;BR /&gt;7ec0: c007bfd8 c007bd8c c047f832 00000001 c7da7f04 c7da7ee0 c007b678 c007bf34&lt;BR /&gt;7ee0: 00000008 c7c19660 c7fb3c80 c7c037c0 c03e507c c7da7f70 c7da7f14 c7da7f08&lt;BR /&gt;7f00: c01fe288 c007b5f0 c7da7f44 c7da7f18 c011b1e8 c01fe278 c7da7f70 c7fba380&lt;BR /&gt;7f20: 00112888 00000008 c7da7f70 00112888 c7da6000 00000000 c7da7f6c c7da7f48&lt;BR /&gt;7f40: c00c3a40 c011b0e8 c004f644 c0060890 00000000 00000000 c7fba380 00000008&lt;BR /&gt;7f60: c7da7fa4 c7da7f70 c00c3b80 c00c3998 00000000 00000000 00200200 00000000&lt;BR /&gt;7f80: c0051b74 00000008 00112888 00000001 00000004 c0030b88 00000000 c7da7fa8&lt;BR /&gt;7fa0: c00309e0 c00c3b4c 00000008 00112888 00000001 00112888 00000008 00000000&lt;BR /&gt;7fc0: 00000008 00112888 00000001 00000004 00000020 0010f2a4 0010f294 00000000&lt;BR /&gt;7fe0: 00000000 be8925fc 000109ec 401871ac 60000010 00000001 00000000 00000000&lt;BR /&gt;Backtrace: &lt;BR /&gt;[&amp;lt;c03c59bc&amp;gt;] (mutex_lock+0x0/0x24) from [&amp;lt;c02e6d48&amp;gt;] (mxs_bat_suspend+0x24/0x40)&lt;BR /&gt;[&amp;lt;c02e6d24&amp;gt;] (mxs_bat_suspend+0x0/0x40) from [&amp;lt;c02488e0&amp;gt;] (platform_pm_suspend+0x58/0x64)&lt;BR /&gt; r5:c03ebfa8 r4:00000002&lt;BR /&gt;[&amp;lt;c0248888&amp;gt;] (platform_pm_suspend+0x0/0x64) from [&amp;lt;c024b1ac&amp;gt;] (pm_op+0x58/0xb8)&lt;BR /&gt;[&amp;lt;c024b154&amp;gt;] (pm_op+0x0/0xb8) from [&amp;lt;c024bb00&amp;gt;] (__device_suspend+0xe8/0x144)&lt;BR /&gt; r9:c7fb3c98 r8:00000000 r6:00000002 r5:c04ff728 r4:c04ff728&lt;BR /&gt;[&amp;lt;c024ba18&amp;gt;] (__device_suspend+0x0/0x144) from [&amp;lt;c024be6c&amp;gt;] (dpm_suspend_start+0x310/0x438)&lt;BR /&gt; r7:c04ff780 r6:c051b1ac r5:00000000 r4:c04ff728&lt;BR /&gt;[&amp;lt;c024bb5c&amp;gt;] (dpm_suspend_start+0x0/0x438) from [&amp;lt;c007bdcc&amp;gt;] (suspend_devices_and_enter+0x50/0x1a8)&lt;BR /&gt;[&amp;lt;c007bd7c&amp;gt;] (suspend_devices_and_enter+0x0/0x1a8) from [&amp;lt;c007bfd8&amp;gt;] (enter_state+0xb4/0xf4)&lt;BR /&gt; r7:c03ced50 r6:00000007 r5:00000001 r4:00000000&lt;BR /&gt;[&amp;lt;c007bf24&amp;gt;] (enter_state+0x0/0xf4) from [&amp;lt;c007b678&amp;gt;] (state_store+0x98/0xc0)&lt;BR /&gt; r5:00000001 r4:c047f832&lt;BR /&gt;[&amp;lt;c007b5e0&amp;gt;] (state_store+0x0/0xc0) from [&amp;lt;c01fe288&amp;gt;] (kobj_attr_store+0x20/0x24)&lt;BR /&gt;[&amp;lt;c01fe268&amp;gt;] (kobj_attr_store+0x0/0x24) from [&amp;lt;c011b1e8&amp;gt;] (sysfs_write_file+0x110/0x148)&lt;BR /&gt;[&amp;lt;c011b0d8&amp;gt;] (sysfs_write_file+0x0/0x148) from [&amp;lt;c00c3a40&amp;gt;] (vfs_write+0xb8/0x134)&lt;BR /&gt;[&amp;lt;c00c3988&amp;gt;] (vfs_write+0x0/0x134) from [&amp;lt;c00c3b80&amp;gt;] (sys_write+0x44/0x70)&lt;BR /&gt; r7:00000008 r6:c7fba380 r5:00000000 r4:00000000&lt;BR /&gt;[&amp;lt;c00c3b3c&amp;gt;] (sys_write+0x0/0x70) from [&amp;lt;c00309e0&amp;gt;] (ret_fast_syscall+0x0/0x2c)&lt;BR /&gt; r8:c0030b88 r7:00000004 r6:00000001 r5:00112888 r4:00000008&lt;BR /&gt;Code: e1a0c00d e92dd800 e24cb004 e3a02000 (e1001092) &lt;BR /&gt;---[ end trace b15d963b7f2c6a19 ]---&lt;/P&gt;

&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I press the power button, I still have an Oops error but the log is different :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;pswitch goto suspend&lt;BR /&gt;PM: Syncing filesystems ... done.&lt;BR /&gt;Freezing user space processes ... (elapsed 0.01 seconds) done.&lt;BR /&gt;Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.&lt;BR /&gt;Unable to handle kernel NULL pointer dereference at virtual address 000000dc&lt;BR /&gt;pgd = c0004000&lt;BR /&gt;[000000dc] *pgd=00000000&lt;BR /&gt;Internal error: Oops: 817 [#1] PREEMPT&lt;BR /&gt;last sysfs file: /sys/devices/virtual/vc/vcs63/dev&lt;BR /&gt;Modules linked in:&lt;BR /&gt;CPU: 0&amp;nbsp;&amp;nbsp;&amp;nbsp; Not tainted&amp;nbsp; (2.6.35.3-g215633e-dirty #71)&lt;BR /&gt;PC is at mutex_lock+0x10/0x24&lt;BR /&gt;LR is at mxs_bat_suspend+0x24/0x40&lt;BR /&gt;pc : [&amp;lt;c03c59cc&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;c02e6d48&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; psr: a0000013&lt;BR /&gt;sp : c7dc1e98&amp;nbsp; ip : c7dc1ea8&amp;nbsp; fp : c7dc1ea4&lt;BR /&gt;r10: 00000002&amp;nbsp; r9 : 00000000&amp;nbsp; r8 : 00000000&lt;BR /&gt;r7 : c04ff75c&amp;nbsp; r6 : c04ff728&amp;nbsp; r5 : 000000dc&amp;nbsp; r4 : 00000000&lt;BR /&gt;r3 : c02e6d24&amp;nbsp; r2 : 00000000&amp;nbsp; r1 : 00000002&amp;nbsp; r0 : 000000dc&lt;BR /&gt;Flags: NzCv&amp;nbsp; IRQs on&amp;nbsp; FIQs on&amp;nbsp; Mode SVC_32&amp;nbsp; ISA ARM&amp;nbsp; Segment kernel&lt;BR /&gt;Control: 0005317f&amp;nbsp; Table: 47510000&amp;nbsp; DAC: 00000017&lt;BR /&gt;Process pswitch (pid: 1106, stack limit = 0xc7dc0270)&lt;BR /&gt;Stack: (0xc7dc1e98 to 0xc7dc2000)&lt;BR /&gt;1e80:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; c7dc1ebc c7dc1ea8&lt;BR /&gt;1ea0: c02e6d48 c03c59cc 00000002 c03ebfa8 c7dc1ecc c7dc1ec0 c02488e0 c02e6d34&lt;BR /&gt;1ec0: c7dc1f04 c7dc1ed0 c024b1ac c0248898 c7dc1f04 c7dc1ee0 00000000 00000000&lt;BR /&gt;1ee0: c7ce8300 c04ff728 c04ff728 00000002 00000000 00000000 c7dc1f2c c7dc1f08&lt;BR /&gt;1f00: c024bb00 c024b164 c04ff728 00000000 c04ff728 00000000 c051b1ac c04ff780&lt;BR /&gt;1f20: c7dc1f6c c7dc1f30 c024be6c c024ba28 13f6438d 00000032 13f6438d 00000032&lt;BR /&gt;1f40: c04fe3d0 c751a558 00000000 00000000 00000001 003fffff 00000000 00000000&lt;BR /&gt;1f60: c7dc1f8c c7dc1f70 c007bdcc c024bb6c 00000000 00000001 00000000 c003cc38&lt;BR /&gt;1f80: c7dc1fa4 c7dc1f90 c007bfd8 c007bd8c c7dc1fcc c7c27f50 c7dc1fb4 c7dc1fa8&lt;BR /&gt;1fa0: c007c038 c007bf34 c7dc1fc4 c7dc1fb8 c003cc54 c007c028 c7dc1ff4 c7dc1fc8&lt;BR /&gt;1fc0: c0063674 c003cc48 00000000 00000000 c7dc1fd0 c7dc1fd0 c7c27f50 c00635ec&lt;BR /&gt;1fe0: c004f794 00000013 00000000 c7dc1ff8 c004f794 c00635fc 55555555 55555555&lt;BR /&gt;Backtrace: &lt;BR /&gt;[&amp;lt;c03c59bc&amp;gt;] (mutex_lock+0x0/0x24) from [&amp;lt;c02e6d48&amp;gt;] (mxs_bat_suspend+0x24/0x40)&lt;BR /&gt;[&amp;lt;c02e6d24&amp;gt;] (mxs_bat_suspend+0x0/0x40) from [&amp;lt;c02488e0&amp;gt;] (platform_pm_suspend+0x58/0x64)&lt;BR /&gt; r5:c03ebfa8 r4:00000002&lt;BR /&gt;[&amp;lt;c0248888&amp;gt;] (platform_pm_suspend+0x0/0x64) from [&amp;lt;c024b1ac&amp;gt;] (pm_op+0x58/0xb8)&lt;BR /&gt;[&amp;lt;c024b154&amp;gt;] (pm_op+0x0/0xb8) from [&amp;lt;c024bb00&amp;gt;] (__device_suspend+0xe8/0x144)&lt;BR /&gt; r9:00000000 r8:00000000 r6:00000002 r5:c04ff728 r4:c04ff728&lt;BR /&gt;[&amp;lt;c024ba18&amp;gt;] (__device_suspend+0x0/0x144) from [&amp;lt;c024be6c&amp;gt;] (dpm_suspend_start+0x310/0x438)&lt;BR /&gt; r7:c04ff780 r6:c051b1ac r5:00000000 r4:c04ff728&lt;BR /&gt;[&amp;lt;c024bb5c&amp;gt;] (dpm_suspend_start+0x0/0x438) from [&amp;lt;c007bdcc&amp;gt;] (suspend_devices_and_enter+0x50/0x1a8)&lt;BR /&gt;[&amp;lt;c007bd7c&amp;gt;] (suspend_devices_and_enter+0x0/0x1a8) from [&amp;lt;c007bfd8&amp;gt;] (enter_state+0xb4/0xf4)&lt;BR /&gt; r7:c003cc38 r6:00000000 r5:00000001 r4:00000000&lt;BR /&gt;[&amp;lt;c007bf24&amp;gt;] (enter_state+0x0/0xf4) from [&amp;lt;c007c038&amp;gt;] (pm_suspend+0x20/0x24)&lt;BR /&gt; r5:c7c27f50 r4:c7dc1fcc&lt;BR /&gt;[&amp;lt;c007c018&amp;gt;] (pm_suspend+0x0/0x24) from [&amp;lt;c003cc54&amp;gt;] (suspend_thread_fn+0x1c/0x24)&lt;BR /&gt;[&amp;lt;c003cc38&amp;gt;] (suspend_thread_fn+0x0/0x24) from [&amp;lt;c0063674&amp;gt;] (kthread+0x88/0x90)&lt;BR /&gt;[&amp;lt;c00635ec&amp;gt;] (kthread+0x0/0x90) from [&amp;lt;c004f794&amp;gt;] (do_exit+0x0/0x6d8)&lt;BR /&gt; r7:00000013 r6:c004f794 r5:c00635ec r4:c7c27f50&lt;BR /&gt;Code: e1a0c00d e92dd800 e24cb004 e3a02000 (e1001092) &lt;BR /&gt;---[ end trace b15d963b7f2c6a19 ]---&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try the solution describe in this post : &lt;A href="https://community.nxp.com/thread/279352"&gt;i.MX283 resets during standby in 5V only mode&lt;/A&gt; but it doesn't resolve my problem.&lt;/P&gt;&lt;P&gt;(actually, I don't have battery and I supply the board by 5V)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there someone who use this mode ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2013 16:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288627#M34525</guid>
      <dc:creator>victorien</dc:creator>
      <dc:date>2013-11-19T16:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 standby error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288628#M34526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Victorien&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Seems like there is something wrong in battery driver's suspend callback, since you do NOT have an battery connected, I wonder whether battery driver would be active, can you add some debug message to see whether the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;mutex_lock&lt;/SPAN&gt; in &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;mxs_bat_suspend&lt;/SPAN&gt; routine has valid parameter. I remembered that on EVK board, there is fake battery circuit coming from regulator directly, can you double check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2013 02:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288628#M34526</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-11-20T02:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 standby error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288629#M34527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your help. I find the solution.&lt;/P&gt;&lt;P&gt;The problem was that in the bootlet &lt;EM&gt;power_prep.c&lt;/EM&gt; I defined &lt;EM&gt;#define NO_DCDC_BATT_SOURCE. &lt;/EM&gt;Then, in &lt;EM&gt;linux/driver/mxs/linux.c&lt;/EM&gt;, function &lt;EM&gt;mxs_bat_probe&lt;/EM&gt;, The initialization of the mutex wasn't done (because we defined that we don't have battery). And the kernel crached in function &lt;EM&gt;mxs_bat_suspend&lt;/EM&gt; (&lt;EM&gt;linux/driver/mxs/linux.c&lt;/EM&gt;) when it tries to lock the mutex.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2013 17:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-standby-error/m-p/288629#M34527</guid>
      <dc:creator>victorien</dc:creator>
      <dc:date>2013-11-20T17:10:25Z</dc:date>
    </item>
  </channel>
</rss>