<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic L2.6.35_11.01.00_ER_source_bundle.tar.gz build failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/L2-6-35-11-01-00-ER-source-bundle-tar-gz-build-failed/m-p/161387#M3435</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial,Helvetica,sans-serif; font-size: 10pt;"&gt;Hi, &lt;BR /&gt; &lt;BR /&gt;I have downloaded "L2.6.35_11.01.00_ER_source_bundle.tar.gz" and done the instructions as per IMX53_Start_linux_bsp_userguide.pdf". I am getting lots of errors during the compilations. &lt;BR /&gt; &lt;BR /&gt;It seems that "&lt;A href="http://www.bitshrine.org/"&gt;www.bitshrine.org&lt;/A&gt;" does not necessary files needed. &lt;BR /&gt; &lt;BR /&gt;I got error like "mtdutils, linux-2.6.35.3.tar.b2, linux-2.6.35_imx" lots of files are missing in the repository. &lt;BR /&gt; &lt;BR /&gt;I have also cross checked that the "L2.6.35_11.01.00_ER_source_bundle.tar.gz" fully downloaded. &lt;BR /&gt; &lt;BR /&gt;Since we are struck here, we require your valuable inputs in this regards, &lt;BR /&gt; &lt;BR /&gt;Thanks, &lt;BR /&gt;Hariharan.V.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jul 2011 15:04:32 GMT</pubDate>
    <dc:creator>neeveehariharan</dc:creator>
    <dc:date>2011-07-05T15:04:32Z</dc:date>
    <item>
      <title>L2.6.35_11.01.00_ER_source_bundle.tar.gz build failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/L2-6-35-11-01-00-ER-source-bundle-tar-gz-build-failed/m-p/161387#M3435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial,Helvetica,sans-serif; font-size: 10pt;"&gt;Hi, &lt;BR /&gt; &lt;BR /&gt;I have downloaded "L2.6.35_11.01.00_ER_source_bundle.tar.gz" and done the instructions as per IMX53_Start_linux_bsp_userguide.pdf". I am getting lots of errors during the compilations. &lt;BR /&gt; &lt;BR /&gt;It seems that "&lt;A href="http://www.bitshrine.org/"&gt;www.bitshrine.org&lt;/A&gt;" does not necessary files needed. &lt;BR /&gt; &lt;BR /&gt;I got error like "mtdutils, linux-2.6.35.3.tar.b2, linux-2.6.35_imx" lots of files are missing in the repository. &lt;BR /&gt; &lt;BR /&gt;I have also cross checked that the "L2.6.35_11.01.00_ER_source_bundle.tar.gz" fully downloaded. &lt;BR /&gt; &lt;BR /&gt;Since we are struck here, we require your valuable inputs in this regards, &lt;BR /&gt; &lt;BR /&gt;Thanks, &lt;BR /&gt;Hariharan.V.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2011 15:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/L2-6-35-11-01-00-ER-source-bundle-tar-gz-build-failed/m-p/161387#M3435</guid>
      <dc:creator>neeveehariharan</dc:creator>
      <dc:date>2011-07-05T15:04:32Z</dc:date>
    </item>
  </channel>
</rss>