<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Burning Linux uImage into i.MX53 QSB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161368#M3432</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now I'm trying to burn Linux uImage I built into i.MX53 QSB. After executing tftpboot, however,&amp;nbsp;any key input is not accepted.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------&lt;/P&gt;&lt;SPAN&gt;MX53-LOCO U-Boot &amp;gt; tftpboot 0x00020000 uImage FEC: enable RMII gasket PHY indentify @ 0x0 = 0x0007c0f1 Using FEC0 device TFTP from server 172.16.1.15; our IP address is 172.16.15.45 Filename 'uImage'. Load address: 0x20000 Loading: FEC: Link is down 7809&lt;/SPAN&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;I'm not sure if the file transfer was sucessfully completed. It seems weird that the left side of RJ-45 LED was blinking all the way.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;I also tried to loadb command to send the image via serial I/F, but it didn't also make progress after just 2 bytes were transferred.&lt;/DIV&gt;&lt;DIV&gt;Can environment variable have something to do with this failure? I attach an file showing all the variables. Does anyone have an idea?&lt;/DIV&gt;&lt;DIV&gt;Best Regards,&lt;/DIV&gt;&lt;DIV&gt;Takashi Kawamoto&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jul 2011 11:28:27 GMT</pubDate>
    <dc:creator>brahman_river</dc:creator>
    <dc:date>2011-07-05T11:28:27Z</dc:date>
    <item>
      <title>Burning Linux uImage into i.MX53 QSB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161368#M3432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now I'm trying to burn Linux uImage I built into i.MX53 QSB. After executing tftpboot, however,&amp;nbsp;any key input is not accepted.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------&lt;/P&gt;&lt;SPAN&gt;MX53-LOCO U-Boot &amp;gt; tftpboot 0x00020000 uImage FEC: enable RMII gasket PHY indentify @ 0x0 = 0x0007c0f1 Using FEC0 device TFTP from server 172.16.1.15; our IP address is 172.16.15.45 Filename 'uImage'. Load address: 0x20000 Loading: FEC: Link is down 7809&lt;/SPAN&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;FEC: Link is down 7809&lt;/P&gt;&lt;P&gt;#&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;I'm not sure if the file transfer was sucessfully completed. It seems weird that the left side of RJ-45 LED was blinking all the way.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;I also tried to loadb command to send the image via serial I/F, but it didn't also make progress after just 2 bytes were transferred.&lt;/DIV&gt;&lt;DIV&gt;Can environment variable have something to do with this failure? I attach an file showing all the variables. Does anyone have an idea?&lt;/DIV&gt;&lt;DIV&gt;Best Regards,&lt;/DIV&gt;&lt;DIV&gt;Takashi Kawamoto&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2011 11:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161368#M3432</guid>
      <dc:creator>brahman_river</dc:creator>
      <dc:date>2011-07-05T11:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: Burning Linux uImage into i.MX53 QSB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161369#M3433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;If I were you, I'd run wireshark on the server.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2011 12:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161369#M3433</guid>
      <dc:creator>PhilEndecott</dc:creator>
      <dc:date>2011-07-05T12:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: Burning Linux uImage into i.MX53 QSB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161370#M3434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;As long as I see the sniffer log, Just a block of data is sent from TFTP server after i.MX53 QSB send Read Request, and no more data is transferred.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2011 00:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Burning-Linux-uImage-into-i-MX53-QSB/m-p/161370#M3434</guid>
      <dc:creator>brahman_river</dc:creator>
      <dc:date>2011-07-06T00:53:09Z</dc:date>
    </item>
  </channel>
</rss>