<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUse SPI on imx6q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Use-SPI-on-imx6q/m-p/287060#M34010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use spi for tranmit data path SPI1 SS0, Can I using function on uboot? Help me! Thank!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Oct 2013 08:22:36 GMT</pubDate>
    <dc:creator>levanthuan</dc:creator>
    <dc:date>2013-10-18T08:22:36Z</dc:date>
    <item>
      <title>Use SPI on imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-SPI-on-imx6q/m-p/287060#M34010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use spi for tranmit data path SPI1 SS0, Can I using function on uboot? Help me! Thank!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2013 08:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-SPI-on-imx6q/m-p/287060#M34010</guid>
      <dc:creator>levanthuan</dc:creator>
      <dc:date>2013-10-18T08:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: Use SPI on imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-SPI-on-imx6q/m-p/287061#M34011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I checked the i.MX6Q SabreSD board, there is a SPI NOR flash connected to CSPI1_SS0, so you can try using 'sf' command in uboot to write/read data on this SPI NOR flash, please see the help in uboot about 'sf' command and try it, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 09:06:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-SPI-on-imx6q/m-p/287061#M34011</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-10-28T09:06:57Z</dc:date>
    </item>
  </channel>
</rss>