<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: BitBurner 1.0.6.0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286919#M33954</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try using BitInit from the OTP TOOLs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that &lt;/P&gt;&lt;P&gt;burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from &lt;/P&gt;&lt;P&gt;the same directory as the BitInit.exe starts) .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jul 2013 02:54:37 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-07-15T02:54:37Z</dc:date>
    <item>
      <title>BitBurner 1.0.6.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286917#M33952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Freescale Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think ther is a possible Bug in the version 1.0.6.0 of the OTP tool BitBurner.&lt;/P&gt;&lt;P&gt;I'm able to burn the OTP bits of my i.MX283 with version 1.0.5.6, but with 1.0.6.0 it is impossible. If I write a new value to HW_OCOTP_CUST0 with 1.0.6.0 it will not be taken but with 1.0.5.6. it will.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 14:08:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286917#M33952</guid>
      <dc:creator>chris321</dc:creator>
      <dc:date>2013-06-11T14:08:08Z</dc:date>
    </item>
    <item>
      <title>Re: BitBurner 1.0.6.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286918#M33953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm also trying to write some fuses, with this version on IMX280 without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the tool's log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Friday, July 12, 2013 15:00:54&lt;/P&gt;&lt;P&gt;StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100001&lt;/P&gt;&lt;P&gt;Read back verify failed. Wrote: 0x00100001 Read: 0x00000000&lt;/P&gt;&lt;P&gt;StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000&lt;/P&gt;&lt;P&gt;Read back verify failed. Wrote: 0x00100000 Read: 0x00000000&lt;/P&gt;&lt;P&gt;StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000&lt;/P&gt;&lt;P&gt;Read back verify failed. Wrote: 0x00100000 Read: 0x00000000&lt;/P&gt;&lt;P&gt;StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000&lt;/P&gt;&lt;P&gt;Read back verify failed. Wrote: 0x00100000 Read: 0x00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2013 18:14:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286918#M33953</guid>
      <dc:creator>alexandresilva</dc:creator>
      <dc:date>2013-07-12T18:14:51Z</dc:date>
    </item>
    <item>
      <title>Re: BitBurner 1.0.6.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286919#M33954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try using BitInit from the OTP TOOLs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that &lt;/P&gt;&lt;P&gt;burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from &lt;/P&gt;&lt;P&gt;the same directory as the BitInit.exe starts) .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2013 02:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBurner-1-0-6-0/m-p/286919#M33954</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-15T02:54:37Z</dc:date>
    </item>
  </channel>
</rss>