<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 8mega pixel MIPI CSI-2 camera input in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286817#M33907</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know the frame rate of your camera.&lt;/P&gt;&lt;P&gt;Is it 3264 x 2448@30fps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now i have a camra with 2560x1440@30fps,but i can't get the image 2560x1440 image frome it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 May 2013 00:16:53 GMT</pubDate>
    <dc:creator>GaoJianzhong</dc:creator>
    <dc:date>2013-05-10T00:16:53Z</dc:date>
    <item>
      <title>8mega pixel MIPI CSI-2 camera input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286814#M33904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using 8mega pixel MIPI CSI-2 camera(3264 x 2448) on iMX6q&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it's find that get 1024 x 1024 pixel image from camera&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but more than 1024 x 1024 is not working..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i think that problem by IPU block&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i remove IPU block in camera input?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean "MIPI CSI-2 -&amp;gt; memory".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm using 3.0.15 kernel..(sabresd)&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2013 04:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286814#M33904</guid>
      <dc:creator>hyunhoshin</dc:creator>
      <dc:date>2013-03-07T04:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: 8mega pixel MIPI CSI-2 camera input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286815#M33905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Hyunho Shin,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;MIPI-CSI2 can receive frames up to 8192 x 4096 pixels, but if you need to process the image on some other IPU block (e.g. rotation, resize and etc), the frame size will be limited.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;For example, if you need to resize or rotate the image, it will need to pass through the image converter (IC) block and it will limit the input image to 4096x4096 and the output image to 1024x1024. See reference manual chapter &lt;/SPAN&gt;&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt;"&gt;36.3.1.5.3 Image Converter (IC)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt;"&gt;This should be the reason you have this limit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt;"&gt;Rgds&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt;"&gt;Rogerio Pimentel&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 14:14:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286815#M33905</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2013-03-14T14:14:11Z</dc:date>
    </item>
    <item>
      <title>Re: 8mega pixel MIPI CSI-2 camera input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286816#M33906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MIPI camera output size is 3264 x 2446 and camera interface output also 3264 x 2446&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i think, i don't need to use IC(image converter) block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but, i think maybe IC block is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how can i get 3264 x 2446 image without IC?&lt;/P&gt;&lt;P&gt;I'm using 3.0.15 kernel..(sabresd)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 00:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286816#M33906</guid>
      <dc:creator>hyunhoshin</dc:creator>
      <dc:date>2013-03-21T00:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: 8mega pixel MIPI CSI-2 camera input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286817#M33907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know the frame rate of your camera.&lt;/P&gt;&lt;P&gt;Is it 3264 x 2448@30fps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now i have a camra with 2560x1440@30fps,but i can't get the image 2560x1440 image frome it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2013 00:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286817#M33907</guid>
      <dc:creator>GaoJianzhong</dc:creator>
      <dc:date>2013-05-10T00:16:53Z</dc:date>
    </item>
    <item>
      <title>Re: 8mega pixel MIPI CSI-2 camera input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286818#M33908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i'm using 3264 x 2448 @ 11fps camera&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but i also could get 1920 x 1080@30fps without IC(Image Converter)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you using with IC, only get under 1024 x 1024 image&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2013 00:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286818#M33908</guid>
      <dc:creator>hyunhoshin</dc:creator>
      <dc:date>2013-05-10T00:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: 8mega pixel MIPI CSI-2 camera input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286819#M33909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;My camera have two modes:4lanes 1280x720@30, and 4lanes 2560x1440@30.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not use IC, and i can get the 1280x720@30 images.&lt;/P&gt;&lt;P&gt;But 2560x1440@30 is not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does i.mx6q can support 4lanes 2560x1440@30 camera?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2013 01:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8mega-pixel-MIPI-CSI-2-camera-input/m-p/286819#M33909</guid>
      <dc:creator>GaoJianzhong</dc:creator>
      <dc:date>2013-05-10T01:24:32Z</dc:date>
    </item>
  </channel>
</rss>