<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 VPU Zero Buffer Decode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285657#M33562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The thread is closed since the same DI is at.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/310455"&gt;https://community.freescale.com/thread/310455&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Aug 2013 07:02:22 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2013-08-19T07:02:22Z</dc:date>
    <item>
      <title>iMX6 VPU Zero Buffer Decode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285655#M33560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We need to use the VPU decoder in a zero-delay mode, i.e. we give the decoder a frame of H.264 data and the decoder performs the decode and provides the framebuffer, immediately.&amp;nbsp; It looks like according to the documentation if we set reorderEnable in the DecOpenParam structure, the decoder should operated in this mode.&amp;nbsp; &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;However we must feed 3 frames in before we get the first frame out. Previously we used iMX53 and this zero-delay decode worked fine. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Enclosed is a modified version of the mxc_vpu_test example.&amp;nbsp; The example was modified to read a .h264 files along with an index file that precisely feeds one frame per keystroke to the decoder.&amp;nbsp; The very first frame is made up of SPS, PPS and and I-Frame, all other frames are P frames.&amp;nbsp; A Readme file in the tgz file explains the changes.&amp;nbsp; You need to build this in the same directory as the original mxc_vpu_text.&amp;nbsp; You probably will have to modify the system directory and the example should build.&amp;nbsp; Also the binary is included see readme for launch instructions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess we are missing setting some parm somewhere to get into this zero-delay mode????&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339917"&gt;mxc_vpu_test_single_frame.tgz&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2013 22:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285655#M33560</guid>
      <dc:creator>SteveBakke</dc:creator>
      <dc:date>2013-07-22T22:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 VPU Zero Buffer Decode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285656#M33561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve, move your post to the i.MX Community so more eyes can take a look.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jul 2013 21:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285656#M33561</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-07-30T21:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 VPU Zero Buffer Decode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285657#M33562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The thread is closed since the same DI is at.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/310455"&gt;https://community.freescale.com/thread/310455&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Aug 2013 07:02:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-VPU-Zero-Buffer-Decode/m-p/285657#M33562</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-08-19T07:02:22Z</dc:date>
    </item>
  </channel>
</rss>