<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLinux Stops at &amp;quot;Freeing init memory: 204K&amp;quot;</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284901#M33355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom device that boots a Linux kernel built with LTIB. I am trying to boot the Freescale kernel L3.0.35_1.1.0_oneiric and it will not finish the boot. It stops displaying to the console or a selected video device after "Freeing init memory: 204K". Here is the bottom of the console output. Any ideas why the display stops?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regulator_init_complete: VDDIO: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: VDDA: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: vddpu: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)&lt;/P&gt;&lt;P&gt;eth0: Freescale FEC PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=1:&lt;/P&gt;&lt;P&gt;07, irq=-1)&lt;/P&gt;&lt;P&gt;usb 2-1: new high speed USB device number 2 using fsl-ehci&lt;/P&gt;&lt;P&gt;hub 2-1:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 2-1:1.0: 7 ports detected&lt;/P&gt;&lt;P&gt;usb 2-1.4: new low speed USB device number 3 using fsl-ehci&lt;/P&gt;&lt;P&gt;input: Dell Dell USB Keyboard as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1&lt;/P&gt;&lt;P&gt;.4:1.0/input/input0&lt;/P&gt;&lt;P&gt;generic-usb 0003:413C:2105.0001: input,hidraw0: USB HID v1.10 Keyboard [Dell Del&lt;/P&gt;&lt;P&gt;l USB Keyboard] on usb-fsl-ehci.1-1.4/input0&lt;/P&gt;&lt;P&gt;usb 2-1.3: new low speed USB device number 4 using fsl-ehci&lt;/P&gt;&lt;P&gt;input: Microsoft Basic Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-&lt;/P&gt;&lt;P&gt;1.3/2-1.3:1.0/input/input1&lt;/P&gt;&lt;P&gt;generic-usb 0003:045E:0084.0002: input,hidraw1: USB HID v1.10 Mouse [Microsoft B&lt;/P&gt;&lt;P&gt;asic Optical Mouse] on usb-fsl-ehci.1-1.3/input0&lt;/P&gt;&lt;P&gt;PHY: 1:07 - Link is Up - 1000/Full&lt;/P&gt;&lt;P&gt;IP-Config: Guessing netmask 255.0.0.0&lt;/P&gt;&lt;P&gt;IP-Config: Complete:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device=eth0, addr=124.0.0.0, mask=255.0.0.0, gw=255.255.255.255,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; host=124.0.0.0, domain=, nis-domain=(none),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=&lt;/P&gt;&lt;P&gt;EXT3-fs: barriers not enabled&lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): using internal journal&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): recovery complete&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext3 filesystem) on device 179:1.&lt;/P&gt;&lt;P&gt;Freeing init memory: 204K&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;***** STOPS HERE - THE CUSTOM KERNEL CONTINUES BOOTING TO A PROMPT *****&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;starting pid 1319, tty '': '/etc/rc.d/rcS'&lt;BR /&gt;Mounting /proc and /sys&lt;BR /&gt;Starting the hotplug events dispatcher udevd&lt;BR /&gt;udevd (1328): /proc/1328/oom_adj is deprecated, please use /proc/1328/oom_score_&lt;BR /&gt;adj instead.&lt;BR /&gt;Synthesizing initial hotplug events&lt;BR /&gt;Setting the hostname to freescale&lt;BR /&gt;Mounting filesystems&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;Running sysctl&lt;BR /&gt;Setting up networking on loopback device:&lt;BR /&gt;Setting up networking on eth0:&lt;BR /&gt;udhcpc (v1.20.2) started&lt;BR /&gt;Sending discover...&lt;BR /&gt;Sending select for 192.168.0.178...&lt;BR /&gt;Lease of 192.168.0.178 obtained, lease time 691200&lt;BR /&gt;Deleting routers&lt;BR /&gt;adding dns 192.168.0.4&lt;BR /&gt;starting pid 2432, tty '': '/etc/rc.d/rc_gpu.S'&lt;BR /&gt;starting pid 2438, tty '': '/etc/rc.d/rc_mxc.S'&lt;/P&gt;&lt;P&gt;arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/&lt;BR /&gt;10 09:20) 4.6.2 20110630 (prerelease)&lt;BR /&gt;root filesystem built on Wed, 20 Feb 2013 15:12:01 -0600&lt;BR /&gt;Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;freescale login:&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Mar 2013 23:44:47 GMT</pubDate>
    <dc:creator>PaulDeMetrotion</dc:creator>
    <dc:date>2013-03-05T23:44:47Z</dc:date>
    <item>
      <title>Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284901#M33355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom device that boots a Linux kernel built with LTIB. I am trying to boot the Freescale kernel L3.0.35_1.1.0_oneiric and it will not finish the boot. It stops displaying to the console or a selected video device after "Freeing init memory: 204K". Here is the bottom of the console output. Any ideas why the display stops?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regulator_init_complete: VDDIO: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: VDDA: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: vddpu: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)&lt;/P&gt;&lt;P&gt;eth0: Freescale FEC PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=1:&lt;/P&gt;&lt;P&gt;07, irq=-1)&lt;/P&gt;&lt;P&gt;usb 2-1: new high speed USB device number 2 using fsl-ehci&lt;/P&gt;&lt;P&gt;hub 2-1:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 2-1:1.0: 7 ports detected&lt;/P&gt;&lt;P&gt;usb 2-1.4: new low speed USB device number 3 using fsl-ehci&lt;/P&gt;&lt;P&gt;input: Dell Dell USB Keyboard as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1&lt;/P&gt;&lt;P&gt;.4:1.0/input/input0&lt;/P&gt;&lt;P&gt;generic-usb 0003:413C:2105.0001: input,hidraw0: USB HID v1.10 Keyboard [Dell Del&lt;/P&gt;&lt;P&gt;l USB Keyboard] on usb-fsl-ehci.1-1.4/input0&lt;/P&gt;&lt;P&gt;usb 2-1.3: new low speed USB device number 4 using fsl-ehci&lt;/P&gt;&lt;P&gt;input: Microsoft Basic Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-&lt;/P&gt;&lt;P&gt;1.3/2-1.3:1.0/input/input1&lt;/P&gt;&lt;P&gt;generic-usb 0003:045E:0084.0002: input,hidraw1: USB HID v1.10 Mouse [Microsoft B&lt;/P&gt;&lt;P&gt;asic Optical Mouse] on usb-fsl-ehci.1-1.3/input0&lt;/P&gt;&lt;P&gt;PHY: 1:07 - Link is Up - 1000/Full&lt;/P&gt;&lt;P&gt;IP-Config: Guessing netmask 255.0.0.0&lt;/P&gt;&lt;P&gt;IP-Config: Complete:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device=eth0, addr=124.0.0.0, mask=255.0.0.0, gw=255.255.255.255,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; host=124.0.0.0, domain=, nis-domain=(none),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=&lt;/P&gt;&lt;P&gt;EXT3-fs: barriers not enabled&lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): using internal journal&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): recovery complete&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext3 filesystem) on device 179:1.&lt;/P&gt;&lt;P&gt;Freeing init memory: 204K&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;***** STOPS HERE - THE CUSTOM KERNEL CONTINUES BOOTING TO A PROMPT *****&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;starting pid 1319, tty '': '/etc/rc.d/rcS'&lt;BR /&gt;Mounting /proc and /sys&lt;BR /&gt;Starting the hotplug events dispatcher udevd&lt;BR /&gt;udevd (1328): /proc/1328/oom_adj is deprecated, please use /proc/1328/oom_score_&lt;BR /&gt;adj instead.&lt;BR /&gt;Synthesizing initial hotplug events&lt;BR /&gt;Setting the hostname to freescale&lt;BR /&gt;Mounting filesystems&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;Running sysctl&lt;BR /&gt;Setting up networking on loopback device:&lt;BR /&gt;Setting up networking on eth0:&lt;BR /&gt;udhcpc (v1.20.2) started&lt;BR /&gt;Sending discover...&lt;BR /&gt;Sending select for 192.168.0.178...&lt;BR /&gt;Lease of 192.168.0.178 obtained, lease time 691200&lt;BR /&gt;Deleting routers&lt;BR /&gt;adding dns 192.168.0.4&lt;BR /&gt;starting pid 2432, tty '': '/etc/rc.d/rc_gpu.S'&lt;BR /&gt;starting pid 2438, tty '': '/etc/rc.d/rc_mxc.S'&lt;/P&gt;&lt;P&gt;arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/&lt;BR /&gt;10 09:20) 4.6.2 20110630 (prerelease)&lt;BR /&gt;root filesystem built on Wed, 20 Feb 2013 15:12:01 -0600&lt;BR /&gt;Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;freescale login:&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2013 23:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284901#M33355</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-03-05T23:44:47Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284902#M33356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you know which profile your customer select to build LTIB rootfs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The build instructions into the document is like:&lt;/P&gt;&lt;P&gt;1. Remove all previously-installed packages in /opt/freescale/pkgs/.&lt;/P&gt;&lt;P&gt;2. Install the LTIB package, not as root, in a location such as /home/user/:&lt;/P&gt;&lt;P&gt;tar zxvf L3.0.35_1.1.0_121218_source.tar.gz&lt;/P&gt;&lt;P&gt;./L3.0.35_1.1.0_121218_source/install&lt;/P&gt;&lt;P&gt;This command installs LTIB to your directory.&lt;/P&gt;&lt;P&gt;3. Build LTIB:&lt;/P&gt;&lt;P&gt;cd &amp;lt;LTIB directory&amp;gt;.&lt;/P&gt;&lt;P&gt;./ltib -m config&lt;/P&gt;&lt;P&gt;4. Select platform to Freescale iMX reference boards and exit, saving the changes. At&lt;/P&gt;&lt;P&gt;the next menu, select platform type as imx6q and package profile. Exit and save the&lt;/P&gt;&lt;P&gt;new configuration. Please note that only the profiles of Min profile, FSL gnome&lt;/P&gt;&lt;P&gt;release packages, and mfg firmware profile pass build tests.&lt;/P&gt;&lt;P&gt;NOTE&lt;/P&gt;&lt;P&gt;You can use the ./ltib -m selectype command to change the&lt;/P&gt;&lt;P&gt;profile after the first selection.&lt;/P&gt;&lt;P&gt;5. To build U-Boot for i.MX 6Dual/6Quad SABRE-SD board, select "Choose your&lt;/P&gt;&lt;P&gt;board for U-Boot" as "mx6q_sabresd". Please note this option is only for U-Boot.&lt;/P&gt;&lt;P&gt;For the kernel image, the current default kernel configuration builds a single image&lt;/P&gt;&lt;P&gt;that works for all i.MX6 boards except i.MX 6SoloLite boards.&lt;/P&gt;&lt;P&gt;--- Choose your board&lt;/P&gt;&lt;P&gt;board (mx6q_sabresd) ---&amp;gt;&lt;/P&gt;&lt;P&gt;7. Close the configuration screen saving the changes.&lt;/P&gt;&lt;P&gt;8. Run the following command:&lt;/P&gt;&lt;P&gt;./ltib&lt;/P&gt;&lt;P&gt;When this procedure is completed, the kernel image and the U-Boot images are&lt;/P&gt;&lt;P&gt;located at: rootfs/boot/&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2013 07:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284902#M33356</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-03-11T07:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284903#M33357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved - when I was copying the file system to the SD card, I did not perfrom a sync operation. Obviously this was required to complete the proper transfer of files to the SD card. After adding this step, I was able to boot past the freeing memory display. On to the next bug.....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2013 16:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284903#M33357</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-03-11T16:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284904#M33358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Xiaoli Zhang,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; can you explain what has to be done for imx6sololite. we are also getting the same freeing init memory issue while booting using the SDcard.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 11:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284904#M33358</guid>
      <dc:creator>reshmimarimgant</dc:creator>
      <dc:date>2013-06-10T11:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284905#M33359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you flashing image well by sync operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 12:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284905#M33359</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-06-10T12:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284906#M33360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we have an freescale i.MX6 Sololite kit. we downloaded BSP and&amp;nbsp;compiled it. we partitioned the SD card as per freescale user guide(running script) and copied the images.&amp;nbsp;while booting it is showing&amp;nbsp; an error and hanging. the error is&amp;nbsp;clearly mentioned in the attached log file. can you please guide&amp;nbsp;us&amp;nbsp; why the error is coming and how to resolve the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find the attached log file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Reshmi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 12:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284906#M33360</guid>
      <dc:creator>reshmimarimgant</dc:creator>
      <dc:date>2013-06-10T12:34:19Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Stops at "Freeing init memory: 204K"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284907#M33361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on our custom board we have used ksz9031interface to imx6solo. can you help me in uboot&amp;nbsp; changes that are need to be done as i am getting mac id 00:00:00:00:00:00 in uboot but its working fine when kernel is booted up. i am able to see mac address as well as communicated over the ksz9031 after the kernel is booted up. I want setup nfs for our custom board. We are also using ltib build system and uboot ver 2009.08 while linux kernel is 3.0.35.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deepak.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 14:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Stops-at-quot-Freeing-init-memory-204K-quot/m-p/284907#M33361</guid>
      <dc:creator>deepakbhagat</dc:creator>
      <dc:date>2015-08-13T14:23:36Z</dc:date>
    </item>
  </channel>
</rss>