<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q overheating ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284746#M33343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes we use 4.2.2-1.1.0-ga Android release.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Feb 2014 15:42:59 GMT</pubDate>
    <dc:creator>Chris1z</dc:creator>
    <dc:date>2014-02-10T15:42:59Z</dc:date>
    <item>
      <title>IMX6Q overheating ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284742#M33339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; For my project, I used a Saberlite to decode some HD video ( H264 / High@4.0&amp;nbsp; / 1920x1080 /25fps ) and to do some other stuff during the video play, I do this using android 4.2.2 , and I m very surprised with two things : &lt;/P&gt;&lt;P&gt;- first the chip is very hot :&lt;/P&gt;&lt;P&gt;When using the magical command in a adb shell : while true; do cat /sys/class/thermal/thermal_zone0/temp; sleep 1; done; &lt;/P&gt;&lt;P&gt;It's give me a temperature of 85°C at the end of the video. &lt;/P&gt;&lt;P&gt;=&amp;gt; And I observe this fact with all my Saberlite, and with a&amp;nbsp; RM3 ( blueship device ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- second : the video could be a little slow, the hardware decoder get some hard time to decode and to show all the frame. Where are all the horse power ! ( I don't exclude some bad coding stuff from my part, but the video is well decode on some others plateform ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under linux os, the video is decoded well and the chip is very hot too. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; So, is this normal for the chip to have such temperature, I don't want to have some premature aging. &lt;/P&gt;&lt;P&gt;=&amp;gt; Is the vpu android really well integrated for the video ? could we wait some new release to have something more powerful under android os ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank in advance for your answers !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yves&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 15:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284742#M33339</guid>
      <dc:creator>by</dc:creator>
      <dc:date>2014-02-07T15:46:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q overheating ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284743#M33340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In our experience with the iMX6, they do get very hot during GPU/VPU intensive tasks.&amp;nbsp; You will need to properly heat sink your final product.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you see the video is slow, you should check your serial port output or 'dmesg' to see if you have kernel logs indicating you reached the temperature threshold.&amp;nbsp; When the thermal driver reaches the temp threshold, it will start to scale CPU and GPU clocks in order to cool itself down.&amp;nbsp; When the clocks are scaled it will severely impact performance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 16:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284743#M33340</guid>
      <dc:creator>Chris1z</dc:creator>
      <dc:date>2014-02-07T16:07:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q overheating ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284744#M33341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yves,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;what you say sounds really strange. I just test "big buck bunny"&lt;/SPAN&gt;&lt;SPAN&gt; in Android 4.3: extra power consumption is around 1.5/2W and temperature raises only upto 60º-65ºC using a iMX6Q5 (commercial package) . Sabrelite uses an insdustrial or automotive package so should reach less temperature.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only way we have tested our custom boards raising high temperature is running a GPU benchmark when the CPU and GPU temperature reach the threshold. Playing not hardware accelerated video also consumes a lot of power but under our experience VPU doesn't consumes so much power.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW: I just delete the download link of "big buck bunny" because my reply was labeled as "waiting for moderators approval".:smileyconfused:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2014 11:17:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284744#M33341</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2014-02-10T11:17:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q overheating ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284745#M33342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK the hot vpu seems to be some kind of a normal comportement. Could you tell me if you use android with your experience ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yves&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2014 13:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284745#M33342</guid>
      <dc:creator>by</dc:creator>
      <dc:date>2014-02-10T13:56:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q overheating ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284746#M33343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes we use 4.2.2-1.1.0-ga Android release.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2014 15:42:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-overheating/m-p/284746#M33343</guid>
      <dc:creator>Chris1z</dc:creator>
      <dc:date>2014-02-10T15:42:59Z</dc:date>
    </item>
  </channel>
</rss>