<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NFS with the IMX27 board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160960#M3328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Default network (NFS, non-DHCP) configuration uses internal Freescale IP resources, that, of course, are not accessible for most (non Freescale) users.&lt;BR /&gt;&lt;BR /&gt;Please try static IP configuration during system configuring as follows :&lt;BR /&gt;&lt;BR /&gt;./ltib -c&lt;BR /&gt;&lt;BR /&gt;Select :&lt;BR /&gt;&lt;BR /&gt;Target System Configuration&lt;BR /&gt;Options -&amp;gt;&lt;BR /&gt;Start Networking&lt;BR /&gt;Network setup -&amp;gt;&lt;BR /&gt;Enable interface 0&lt;BR /&gt;[] IP address&lt;BR /&gt;…&lt;BR /&gt;&lt;BR /&gt;Then enter (target) IP, appropriate for your network,&lt;BR /&gt;say 192.168.1.150, netmask =255.255.255.0, set gateway&lt;BR /&gt;address, if your target MX27 board is placed in local&lt;BR /&gt;net (for example – 192.168.1.64) and finally – nameserver IP address (say, 192.168.1.83), where your NFS is hosted.&lt;BR /&gt;&lt;BR /&gt;After Linux kernel and file system are built, in target redboot the following may be entered as an example :&lt;BR /&gt;&lt;BR /&gt;load -r -b 0x100000 /iMX27/zImage&lt;BR /&gt;&lt;BR /&gt;exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=192.168.1.83:/ltib/ltib-imx27ads-20070522/rootfs init=/linuxrc ip=192.168.1.150:192.168.1.83"&lt;BR /&gt;&lt;BR /&gt;Message Edited by Yuri on &lt;SPAN class="date_text"&gt;2008-08-25&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;12:14 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Aug 2008 18:10:14 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2008-08-25T18:10:14Z</dc:date>
    <item>
      <title>NFS with the IMX27 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160957#M3325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I successfully cross compiled with LTIB the linphone application from the fs.bluewind.it website.&lt;BR /&gt;I downloaded the kernel on the board, the problem is that the rootfs.jffs2 is to big to fit on the NOR flash...&lt;BR /&gt;&lt;BR /&gt;So i tried to boot from nfs...&lt;BR /&gt;My daemon nfs is working correctly because i can mount it from a distant computer...&lt;BR /&gt;But I am not able to do it from the iMX27 board&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;&lt;U&gt;Here is what i did :&lt;/U&gt;&lt;/B&gt;&lt;BR /&gt;fis load kernel&lt;BR /&gt;exec -c "root=/dev/nfs nfsroot=192.168.49.30:/tftpboot console=ttymxc0&amp;nbsp; ip=192.168.49.179:192.168.49.30:192.168.49.254:255.255.255.0:imx27:&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" id="smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;ff"&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;&lt;U&gt;here is what i get :&lt;/U&gt;&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;eth0: using half-duplex 10Base-T (RJ-45)&lt;BR /&gt;&lt;BR /&gt;IP-Config: Complete:&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device=eth0, addr=192.168.49.179, mask=255.255.255.0, gw=192.168.49.254,&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; host=imx27, domain=, nis-domain=(none),&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bootserver=192.168.49.30, rootserver=192.168.49.30, rootpath=&lt;BR /&gt;&lt;BR /&gt;Looking up port of RPC 100003/2 on 192.168.49.30&lt;BR /&gt;&lt;BR /&gt;Looking up port of RPC 100005/1 on 192.168.49.30&lt;BR /&gt;&lt;BR /&gt;VFS: Mounted root (nfs filesystem).&lt;BR /&gt;&lt;BR /&gt;Freeing init memory: 192K&lt;BR /&gt;&lt;BR /&gt;Setting the hostname to freescale&lt;BR /&gt;Mounting /proc and /sys&lt;BR /&gt;Starting the hotplug events dispatcher udevd&lt;BR /&gt;Synthesizing initial hotplug events&lt;BR /&gt;Mounting filesystems&lt;BR /&gt;Starting syslogd and klogd&lt;BR /&gt;Running depmod&lt;BR /&gt;Setting up networking on loopback device:&lt;BR /&gt;Setting up networking on eth0:&lt;BR /&gt;&lt;BR /&gt;Adding static route for default gateway to 172.27.255.254:&lt;BR /&gt;nfs: server 192.168.49.30 not responding, still trying&lt;BR /&gt;&lt;BR /&gt;nfs: server 192.168.49.30 not responding, still trying&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Thanks for your help,&lt;BR /&gt;&lt;BR /&gt;aurelien&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2007 01:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160957#M3325</guid>
      <dc:creator>aurelihein</dc:creator>
      <dc:date>2007-11-06T01:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: NFS with the IMX27 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160958#M3326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You could try nfs over tcp instead of the default udp, in my case it works more reliable:&lt;BR /&gt;&lt;BR /&gt;nfsroot=192.168.49.30:/tftpboot,rsize=8192,wsize=8192,hard,intr,tcp,nolock&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2007 17:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160958#M3326</guid>
      <dc:creator>eriko</dc:creator>
      <dc:date>2007-11-06T17:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: NFS with the IMX27 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160959#M3327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;So everything was ok, actually the problem was my network configuration in the LTIB, My board changed its IP since I booted from NFS, so it couldn't find anymore the NFS server&lt;BR /&gt;thanks,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2007 17:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160959#M3327</guid>
      <dc:creator>aurelihein</dc:creator>
      <dc:date>2007-11-06T17:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: NFS with the IMX27 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160960#M3328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Default network (NFS, non-DHCP) configuration uses internal Freescale IP resources, that, of course, are not accessible for most (non Freescale) users.&lt;BR /&gt;&lt;BR /&gt;Please try static IP configuration during system configuring as follows :&lt;BR /&gt;&lt;BR /&gt;./ltib -c&lt;BR /&gt;&lt;BR /&gt;Select :&lt;BR /&gt;&lt;BR /&gt;Target System Configuration&lt;BR /&gt;Options -&amp;gt;&lt;BR /&gt;Start Networking&lt;BR /&gt;Network setup -&amp;gt;&lt;BR /&gt;Enable interface 0&lt;BR /&gt;[] IP address&lt;BR /&gt;…&lt;BR /&gt;&lt;BR /&gt;Then enter (target) IP, appropriate for your network,&lt;BR /&gt;say 192.168.1.150, netmask =255.255.255.0, set gateway&lt;BR /&gt;address, if your target MX27 board is placed in local&lt;BR /&gt;net (for example – 192.168.1.64) and finally – nameserver IP address (say, 192.168.1.83), where your NFS is hosted.&lt;BR /&gt;&lt;BR /&gt;After Linux kernel and file system are built, in target redboot the following may be entered as an example :&lt;BR /&gt;&lt;BR /&gt;load -r -b 0x100000 /iMX27/zImage&lt;BR /&gt;&lt;BR /&gt;exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=192.168.1.83:/ltib/ltib-imx27ads-20070522/rootfs init=/linuxrc ip=192.168.1.150:192.168.1.83"&lt;BR /&gt;&lt;BR /&gt;Message Edited by Yuri on &lt;SPAN class="date_text"&gt;2008-08-25&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;12:14 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2008 18:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-the-IMX27-board/m-p/160960#M3328</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2008-08-25T18:10:14Z</dc:date>
    </item>
  </channel>
</rss>