<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6 32kHz clock output specifications in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-32kHz-clock-output-specifications/m-p/284239#M33238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Provided that I use SABRE development board for Smart devices with the crystal suggested there, what quality can I expect of the 32kHz output clock in terms of accuracy, phase noise and rise/fall time. I'm outputting the 32kHz clock on the XTALOSC_REF_CLK_32K pin. I cannot find this information in any specification, but maybe I've missed it somewhere?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Jun 2013 13:23:52 GMT</pubDate>
    <dc:creator>emil</dc:creator>
    <dc:date>2013-06-10T13:23:52Z</dc:date>
    <item>
      <title>iMX6 32kHz clock output specifications</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-32kHz-clock-output-specifications/m-p/284239#M33238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Provided that I use SABRE development board for Smart devices with the crystal suggested there, what quality can I expect of the 32kHz output clock in terms of accuracy, phase noise and rise/fall time. I'm outputting the 32kHz clock on the XTALOSC_REF_CLK_32K pin. I cannot find this information in any specification, but maybe I've missed it somewhere?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 13:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-32kHz-clock-output-specifications/m-p/284239#M33238</guid>
      <dc:creator>emil</dc:creator>
      <dc:date>2013-06-10T13:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 32kHz clock output specifications</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-32kHz-clock-output-specifications/m-p/284240#M33239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) The output clock accuracy will be determined by the accuracy of the crystal used.&lt;/P&gt;&lt;P&gt;2) Unfortunately, we have no data on the phase noise of the output. This is not a parameter that is characterized on this device.&lt;/P&gt;&lt;P&gt;3) The pin on which &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;XTALOSC_REF_CLK_32K &lt;/SPAN&gt;is multiplexed is a GPIO-type output buffer. The output rise/fall times for GPIO-type outputs are shown in the datasheet in the section "General Purpose I/O AC Parameters".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Clay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Aug 2013 15:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-32kHz-clock-output-specifications/m-p/284240#M33239</guid>
      <dc:creator>Clay_Turner</dc:creator>
      <dc:date>2013-08-19T15:50:52Z</dc:date>
    </item>
  </channel>
</rss>