<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error building the XIP image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-the-XIP-image/m-p/284074#M33203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Hardly our Linux kernel can be built to work directly from NOR without DRAM memory.&lt;BR /&gt;We do not have such experience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Sep 2017 05:07:31 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2017-09-04T05:07:31Z</dc:date>
    <item>
      <title>Error building the XIP image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-the-XIP-image/m-p/284073#M33202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a very resource constraint application which uses a custom iMX6 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the parallel NOR flash for booting the kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried using the XIP image for executing the Kernel directly form the NOR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However it has the !ZBOOT_ROM constraint which i am not able to find anywhere in the boot option sin LTIB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using the L3.0.35_4.1.0 kernel version by the way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According the the help i need to manually provide the BSS and the text addresses of the image to be loaded in the kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me what is the default place in the NOR where the BSS and the text sections of the UImage are loaded? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Mar 2014 06:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-building-the-XIP-image/m-p/284073#M33202</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-03-08T06:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: Error building the XIP image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-the-XIP-image/m-p/284074#M33203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Hardly our Linux kernel can be built to work directly from NOR without DRAM memory.&lt;BR /&gt;We do not have such experience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 05:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-building-the-XIP-image/m-p/284074#M33203</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-09-04T05:07:31Z</dc:date>
    </item>
  </channel>
</rss>