<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to use self-generated updater.sb burning system kernel and file system on iMX28EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-self-generated-updater-sb-burning-system-kernel-and/m-p/283300#M33010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. By default, the i.MX28 EVK is shipped with HAB enabled. So please use the 'ivt' .sb file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Please connect the EVK board and the PC by the serial cable to see the boot up message from the Terminal screen. Then you can find where is stopped and debug the problem from the boot up log message.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jul 2013 08:46:09 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2013-07-22T08:46:09Z</dc:date>
    <item>
      <title>How to use self-generated updater.sb burning system kernel and file system on iMX28EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-self-generated-updater-sb-burning-system-kernel-and/m-p/283299#M33009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the latest version of the development kit L2.6.35_1.1.0_130130_source, after installation&lt;/P&gt;&lt;P&gt;Compiled updater.sb and updater_ivt.sb, replace the original text mfgtool&lt;/P&gt;&lt;P&gt;Parts, an error occurs during programming, in the log file mfgtool.log wrote:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Friday, July 19, 2013 16:31:14&lt;/P&gt;&lt;P&gt;1 - Panel A Start processing Singlechip NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Panel A Start type = "boot" body = "Recovery"&lt;/P&gt;&lt;P&gt;file = "updater.sb" timeout = "60" onError = "" text = "Booting&lt;/P&gt;&lt;P&gt;update firmware. ".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Panel A Finished type = "boot" body = "Recovery"&lt;/P&gt;&lt;P&gt;file = "updater.sb" timeout = "60" onError = "" text = "Booting&lt;/P&gt;&lt;P&gt;update firmware. "SUCCESS code = 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Panel A Start type = "boot" body = "Recovery"&lt;/P&gt;&lt;P&gt;file = "updater_ivt.sb" timeout = "60" onError = "" text = "Booting&lt;/P&gt;&lt;P&gt;update firmware. ".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Panel A Finished type = "boot" body = "Recovery"&lt;/P&gt;&lt;P&gt;file = "updater_ivt.sb" timeout = "60" onError = "" text = "Booting&lt;/P&gt;&lt;P&gt;update firmware. "SUCCESS code = 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Panel A Start type = "find" body = "Updater" file = ""&lt;/P&gt;&lt;P&gt;timeout = "180" onError = "" text = "".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Panel A Finished type = "find" body = "Updater"&lt;/P&gt;&lt;P&gt;file = "" timeout = "180" onError = "" text = "" FAIL code = -65536.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Panel A: 2 - Panel A Finished processing Singlechip NAND&lt;/P&gt;&lt;P&gt;: FAIL code = -65536.&lt;/P&gt;&lt;P&gt;I do not know which files need to be modified in order to compile the correct updater.sb, please mention&lt;/P&gt;&lt;P&gt;For help, thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2013 01:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-self-generated-updater-sb-burning-system-kernel-and/m-p/283299#M33009</guid>
      <dc:creator>xuning</dc:creator>
      <dc:date>2013-07-22T01:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to use self-generated updater.sb burning system kernel and file system on iMX28EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-self-generated-updater-sb-burning-system-kernel-and/m-p/283300#M33010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. By default, the i.MX28 EVK is shipped with HAB enabled. So please use the 'ivt' .sb file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Please connect the EVK board and the PC by the serial cable to see the boot up message from the Terminal screen. Then you can find where is stopped and debug the problem from the boot up log message.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2013 08:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-self-generated-updater-sb-burning-system-kernel-and/m-p/283300#M33010</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-07-22T08:46:09Z</dc:date>
    </item>
  </channel>
</rss>