<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 IPU DI display clock generation.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IPU-DI-display-clock-generation/m-p/283239#M32992</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right :&lt;BR /&gt;1. &lt;BR /&gt;It is possible to use "display clock from external source by setting this field if I select external source by di0_clk_ext in chapter &lt;SPAN style="font-size: 10pt;"&gt;38.5.193."&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;BR /&gt;Correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Feb 2014 08:39:09 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-02-07T08:39:09Z</dc:date>
    <item>
      <title>i.MX6 IPU DI display clock generation.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IPU-DI-display-clock-generation/m-p/283238#M32991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions about i.MX6SDL IPU display clock generation.&lt;/P&gt;&lt;P&gt;Please see my questions below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Q1]&lt;/P&gt;&lt;P&gt;Please see chapter 38.1.10.3 in IMX6SDLRM.&lt;/P&gt;&lt;P&gt;It says "The DI clock can be derived from IPU's clock (HSP_CLK) or from an external source (via the DIn_DISP_CLK - ipp_di_#_ext_clk pin)".&lt;/P&gt;&lt;P&gt;Next, please see chapter 38.5.194.&lt;/P&gt;&lt;P&gt;The discription explains about display clock generation only mede from HSP_CLK.&lt;/P&gt;&lt;P&gt;But I think I can generate display clock from external source by setting this field if I select external source by di0_clk_ext in chapter &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;38.5.193.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Q2]&lt;/P&gt;&lt;P&gt;I want to confirm how to set the fractional part of dix_disp_clk_period in chapter 38.5.194.&lt;/P&gt;&lt;P&gt;I understand display clock will be" HSP_CLK / (1 + 1/16)" if I set dix_disp_clk_period = 0x011.&lt;/P&gt;&lt;P&gt;And it will be "HSP_CLK / (1+ 1/2)" if I set dix_disp_clk_period = 0x018.&lt;/P&gt;&lt;P&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 04:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IPU-DI-display-clock-generation/m-p/283238#M32991</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-02-07T04:55:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 IPU DI display clock generation.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IPU-DI-display-clock-generation/m-p/283239#M32992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right :&lt;BR /&gt;1. &lt;BR /&gt;It is possible to use "display clock from external source by setting this field if I select external source by di0_clk_ext in chapter &lt;SPAN style="font-size: 10pt;"&gt;38.5.193."&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;BR /&gt;Correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 08:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IPU-DI-display-clock-generation/m-p/283239#M32992</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-02-07T08:39:09Z</dc:date>
    </item>
  </channel>
</rss>