<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx53 quickstart not booting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160774#M3288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Gary,&lt;/P&gt;&lt;P&gt;I had the same problem with the u-boot-2009.08 with the R board ( the one with 34708 PMIC ), solved applying the Freescale patches.&lt;BR /&gt;I had used the u-boot.2012.4 and the u-boot.2011.12 and both runs fine without patches on the DA9053 based board.&lt;BR /&gt;I think you have to apply the patches, but I' m not sure as I have never tested u-boot-2009.08 on the non-R board.&lt;BR /&gt;Maybe using a more recent u-boot you can solve your problem, but consider you will loose the splash screen ( well, I've never been able to use the splash on more recent u-boot versions) , and this is why I came back to u-boot.2009.08.&lt;BR /&gt;Hope this helps&lt;BR /&gt;Filippo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 May 2012 08:50:43 GMT</pubDate>
    <dc:creator>Filippo</dc:creator>
    <dc:date>2012-05-16T08:50:43Z</dc:date>
    <item>
      <title>imx53 quickstart not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160773#M3287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a problem with both the imx53 quickstart and my custom version of the quickstart design booting.&lt;/P&gt;&lt;P&gt;Sometimes the quickstart doesn't boot.&amp;nbsp; after a couple of power cycles I see data at the console.&lt;/P&gt;&lt;P&gt;Voltages seem to power on at the proper times using the DA9053.&amp;nbsp; Since the quickstart exhibits this booting problem and I have over 50 quickstart boards that do this, has anybody else had this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 May 2012 19:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160773#M3287</guid>
      <dc:creator>GaryWeitzman</dc:creator>
      <dc:date>2012-05-15T19:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 quickstart not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160774#M3288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Gary,&lt;/P&gt;&lt;P&gt;I had the same problem with the u-boot-2009.08 with the R board ( the one with 34708 PMIC ), solved applying the Freescale patches.&lt;BR /&gt;I had used the u-boot.2012.4 and the u-boot.2011.12 and both runs fine without patches on the DA9053 based board.&lt;BR /&gt;I think you have to apply the patches, but I' m not sure as I have never tested u-boot-2009.08 on the non-R board.&lt;BR /&gt;Maybe using a more recent u-boot you can solve your problem, but consider you will loose the splash screen ( well, I've never been able to use the splash on more recent u-boot versions) , and this is why I came back to u-boot.2009.08.&lt;BR /&gt;Hope this helps&lt;BR /&gt;Filippo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2012 08:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160774#M3288</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2012-05-16T08:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 quickstart not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160775#M3289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;CITE&gt;Filippo said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/imx53-quickstart-not-booting?groupUrl=imx53xcommunityhwdesignsupport&amp;amp;#4103961Comment69944"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;Gary,&lt;/P&gt;&lt;P&gt;I had the same problem with the u-boot-2009.08 with the R board ( the one with 34708 PMIC ), solved applying the Freescale patches.&lt;BR /&gt;I had used the u-boot.2012.4 and the u-boot.2011.12 and both runs fine without patches on the DA9053 based board.&lt;BR /&gt;I think you have to apply the patches, but I' m not sure as I have never tested u-boot-2009.08 on the non-R board.&lt;BR /&gt;Maybe using a more recent u-boot you can solve your problem, but consider you will loose the splash screen ( well, I've never been able to use the splash on more recent u-boot versions) , and this is why I came back to u-boot.2009.08.&lt;BR /&gt;Hope this helps&lt;BR /&gt;Filippo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Filippo,&lt;/P&gt;&lt;P&gt;That was the problem.&amp;nbsp; the software group found a patch and the problem went away!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2012 20:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-quickstart-not-booting/m-p/160775#M3289</guid>
      <dc:creator>GaryWeitzman</dc:creator>
      <dc:date>2012-05-18T20:42:31Z</dc:date>
    </item>
  </channel>
</rss>