<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 4 Camera input, vpu encode and image processing, is i.mx53 capable? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160728#M3278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am searching a hardware solution for the follow requirement:&lt;/P&gt;&lt;P&gt;1. 4 camera input, resolution 640*480. NTSC or PAL&lt;/P&gt;&lt;P&gt;2. The above 4 camera input will be encode with VPU h264 into SD Card.&lt;/P&gt;&lt;P&gt;3. At the same time, these 4 frames will be processed by a simpel image function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to reference for i.mx53, it can process up to 4 encode/decode work&amp;nbsp;simultaneously.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i.mx53 can afford to this work, is it right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jul 2011 22:30:13 GMT</pubDate>
    <dc:creator>YuLin</dc:creator>
    <dc:date>2011-07-01T22:30:13Z</dc:date>
    <item>
      <title>4 Camera input, vpu encode and image processing, is i.mx53 capable?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160728#M3278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am searching a hardware solution for the follow requirement:&lt;/P&gt;&lt;P&gt;1. 4 camera input, resolution 640*480. NTSC or PAL&lt;/P&gt;&lt;P&gt;2. The above 4 camera input will be encode with VPU h264 into SD Card.&lt;/P&gt;&lt;P&gt;3. At the same time, these 4 frames will be processed by a simpel image function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to reference for i.mx53, it can process up to 4 encode/decode work&amp;nbsp;simultaneously.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i.mx53 can afford to this work, is it right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 22:30:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160728#M3278</guid>
      <dc:creator>YuLin</dc:creator>
      <dc:date>2011-07-01T22:30:13Z</dc:date>
    </item>
    <item>
      <title>Re: 4 Camera input, vpu encode and image processing, is i.mx53 capable?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160729#M3279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;4 encode/decode instance is not the same as 4 camera inputs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don´t believe imx53 has more than 2 camera input. Well, you can use 4 USB cameras...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2011 19:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160729#M3279</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2011-07-06T19:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: 4 Camera input, vpu encode and image processing, is i.mx53 capable?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160730#M3280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;CITE&gt;Daiane Angolini said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/4-camera-input-vpu-encode-and?commentId=4103961%3AComment%3A22115&amp;amp;xg_source=msg_com_forum#4103961Comment22115"&gt;&lt;DIV&gt;&lt;P&gt;4 encode/decode instance is not the same as 4 camera inputs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;* I can understand it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don´t believe imx53 has more than 2 camera input. Well, you can use 4 USB cameras...&lt;/P&gt;&lt;P&gt;* Now I am trying 4 USB camera.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2011 22:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160730#M3280</guid>
      <dc:creator>YuLin</dc:creator>
      <dc:date>2011-07-06T22:23:10Z</dc:date>
    </item>
    <item>
      <title>Re: 4 Camera input, vpu encode and image processing, is i.mx53 capable?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160731#M3281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;VPU is the "block" which encode and decode video, like taking YUV and giving H264.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By default, imx53 BSP has one "special" camera input (csi). The camera input is done by some hardware specific (please, take a look on IPU documentation for details).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As I know, there is only CSI0 and CSI1, in other words, there is only 2 "hardware camera inputs".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case you´re using 4 USB, I don´t know if USB bus will be fast enough for all video instances.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But wait. There are cameras that gives H264, is it your case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2011 17:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160731#M3281</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2011-07-07T17:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: 4 Camera input, vpu encode and image processing, is i.mx53 capable?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160732#M3282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have question like yours too, but our usb cameras are H.264, not raw data, so we want to connect 8 cameras to iMX53, and use iMX53 to decode h264 stream at same time. Each camera is QVGA resolution.&lt;BR /&gt;I also want to know that i.MX53 can handle the task or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2012 03:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-Camera-input-vpu-encode-and-image-processing-is-i-mx53-capable/m-p/160732#M3282</guid>
      <dc:creator>JasonShi1z</dc:creator>
      <dc:date>2012-06-21T03:10:39Z</dc:date>
    </item>
  </channel>
</rss>