<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Gnome - video test with totem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gnome-video-test-with-totem/m-p/160700#M3277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I build the Gnome release and was testing audio/video with totem&lt;/P&gt;&lt;P&gt;Audio works fine, but when I open a video file: the terminal log indicates everything is fine, totem shows "playing", I can hear the audio, but no display-- is there anything I'm missing. I opened the video from the target (using touchscreen)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Video playback works perfect with gplay... clear and smooth playback only at 380mW on imx233 running at 454.7MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 03 Jul 2011 09:00:01 GMT</pubDate>
    <dc:creator>danix</dc:creator>
    <dc:date>2011-07-03T09:00:01Z</dc:date>
    <item>
      <title>Gnome - video test with totem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gnome-video-test-with-totem/m-p/160700#M3277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I build the Gnome release and was testing audio/video with totem&lt;/P&gt;&lt;P&gt;Audio works fine, but when I open a video file: the terminal log indicates everything is fine, totem shows "playing", I can hear the audio, but no display-- is there anything I'm missing. I opened the video from the target (using touchscreen)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Video playback works perfect with gplay... clear and smooth playback only at 380mW on imx233 running at 454.7MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jul 2011 09:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gnome-video-test-with-totem/m-p/160700#M3277</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2011-07-03T09:00:01Z</dc:date>
    </item>
  </channel>
</rss>