<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 Secure Boot HAB API within U-Boot calls freezing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282172#M32695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to call HAB API functions from within U-Boot on an i.MX6DL Quick Start board (Rev B3) and each time I do, U-Boot freezes (2009.08).&lt;BR /&gt;U-Boot has been booted using HAB and is at this point working and has the hab_status command from &lt;A _jive_internal="true" href="https://community.nxp.com/servlet/JiveServlet/download/325535-259256/secure_boot_on_imx6.pdf" title="https://community.freescale.com/servlet/JiveServlet/download/325535-259256/secure_boot_on_imx6.pdf"&gt;https://community.freescale.com/servlet/JiveServlet/download/325535-259256/secure_boot_on_imx6.pdf&lt;/A&gt; , this however, does work.&lt;/P&gt;&lt;P&gt;The first function I'm trying to call is hab_status_t(* entry )(void) - which I'm defining by doing this:&lt;/P&gt;&lt;P&gt;#define HAB_RVT_STATUS_ENTRY (*(uint32_t *) 0x00000098)&lt;/P&gt;&lt;P&gt;typedef hab_status_t hab_rvt_status_entry_t();&lt;/P&gt;&lt;P&gt;#define hab_rvt_status_entry ((hab_rvt_status_entry_t*)HAB_RVT_STATUS_ENTRY)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And then I'm calling hab_rvt_status_entry(); - this is where is freezes.&lt;/P&gt;&lt;P&gt;Other don't work either, I have tested status exit, status check, and image entry.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or ideas would be appreciated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2013 13:16:23 GMT</pubDate>
    <dc:creator>timstableford</dc:creator>
    <dc:date>2013-08-29T13:16:23Z</dc:date>
    <item>
      <title>i.MX6 Secure Boot HAB API within U-Boot calls freezing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282172#M32695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to call HAB API functions from within U-Boot on an i.MX6DL Quick Start board (Rev B3) and each time I do, U-Boot freezes (2009.08).&lt;BR /&gt;U-Boot has been booted using HAB and is at this point working and has the hab_status command from &lt;A _jive_internal="true" href="https://community.nxp.com/servlet/JiveServlet/download/325535-259256/secure_boot_on_imx6.pdf" title="https://community.freescale.com/servlet/JiveServlet/download/325535-259256/secure_boot_on_imx6.pdf"&gt;https://community.freescale.com/servlet/JiveServlet/download/325535-259256/secure_boot_on_imx6.pdf&lt;/A&gt; , this however, does work.&lt;/P&gt;&lt;P&gt;The first function I'm trying to call is hab_status_t(* entry )(void) - which I'm defining by doing this:&lt;/P&gt;&lt;P&gt;#define HAB_RVT_STATUS_ENTRY (*(uint32_t *) 0x00000098)&lt;/P&gt;&lt;P&gt;typedef hab_status_t hab_rvt_status_entry_t();&lt;/P&gt;&lt;P&gt;#define hab_rvt_status_entry ((hab_rvt_status_entry_t*)HAB_RVT_STATUS_ENTRY)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And then I'm calling hab_rvt_status_entry(); - this is where is freezes.&lt;/P&gt;&lt;P&gt;Other don't work either, I have tested status exit, status check, and image entry.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or ideas would be appreciated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2013 13:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282172#M32695</guid>
      <dc:creator>timstableford</dc:creator>
      <dc:date>2013-08-29T13:16:23Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Secure Boot HAB API within U-Boot calls freezing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282173#M32696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It was hanging because the clock for the CAAM isn't enabled by default and needs to be before calling HAB functions which use it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2013 10:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282173#M32696</guid>
      <dc:creator>timstableford</dc:creator>
      <dc:date>2013-09-02T10:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Secure Boot HAB API within U-Boot calls freezing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282174#M32697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There seems to be a similar issue with the imx28.&amp;nbsp; The processor is hanging in at the same point in u-boot after the call to the HAB API rvt_status function.&amp;nbsp; Do you have any more details on your fix for the mx6 that might translate?&amp;nbsp; There is a hab_rvt_clock_init function defined in the mainline hab.c for the i.mx6 but doesn't appear to be called. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&amp;nbsp; The reference manual RVT address was updated between document revison 1 (2010) and revision 2 (2013).&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2013 02:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Secure-Boot-HAB-API-within-U-Boot-calls-freezing/m-p/282174#M32697</guid>
      <dc:creator>dwc</dc:creator>
      <dc:date>2013-09-20T02:41:19Z</dc:date>
    </item>
  </channel>
</rss>