<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx28 EVK USB unpowered</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281982#M32643</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In which case everything looks good from the log file,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming you are using the host port (The big USB A Connector) and not the OSB OTG port.&lt;/P&gt;&lt;P&gt;I notice it is suspending the USB host functionality at the end, without going too far into it, it might just be power saving?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you get anything when you type : lsusb from the cmd prompt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, can you put a scope probe on the Vbus line as well as R194, You should be able to see some waveform activity?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll try a build later with my USB port enabled and see what happens on my EVK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Feb 2014 09:40:54 GMT</pubDate>
    <dc:creator>peteewg</dc:creator>
    <dc:date>2014-02-12T09:40:54Z</dc:date>
    <item>
      <title>imx28 EVK USB unpowered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281979#M32640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Freescale!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the imx28 EVK board running 2.6.35.3 kernel, I am trying to make the USB Host to work but I am only measuring up 0.5 V. Which is quite far from the required 5 V. Here is my kernel log with a USB memory stick attached to the port!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux version 2.6.35.3-571-gcca29a0 (madfsl@ubuntu) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #1 PREEMPT Thu Feb 6 05:28:44 MST 2014&lt;/P&gt;&lt;P&gt;CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177&lt;/P&gt;&lt;P&gt;CPU: VIVT data cache, VIVT instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale MX28EVK board&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writeback&lt;/P&gt;&lt;P&gt;On node 0 totalpages: 32768&lt;/P&gt;&lt;P&gt;free_area_init_node: node 0, pgdat c0534f88, node_mem_map c0580000&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA zone: 32 pages used for memmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA zone: 0 pages reserved&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA zone: 4064 pages, LIFO batch:0&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 224 pages used for memmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 28448 pages, LIFO batch:7&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 32512&lt;/P&gt;&lt;P&gt;Kernel command line: -e noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none gpmi&lt;/P&gt;&lt;P&gt;PID hash table entries: 512 (order: -1, 2048 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;Memory: 128MB = 128MB total&lt;/P&gt;&lt;P&gt;Memory: 120220k/120220k available, 10852k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xfde00000 - 0xffe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 32 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xc8800000 - 0xf0000000&amp;nbsp;&amp;nbsp; ( 632 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0xc0000000 - 0xc8000000&amp;nbsp;&amp;nbsp; ( 128 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0xbf000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 16 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0xc0008000 - 0xc0030000&amp;nbsp;&amp;nbsp; ( 160 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0xc0030000 - 0xc04f7000&amp;nbsp;&amp;nbsp; (4892 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0xc04f8000 - 0xc0535960&amp;nbsp;&amp;nbsp; ( 247 kB)&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;/P&gt;&lt;P&gt;Hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RCU-based detection of stalled CPUs is disabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Verbose stalled-CPUs detection is disabled.&lt;/P&gt;&lt;P&gt;NR_IRQS:288&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;console [ttyAM0] enabled&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Security Framework initialized&lt;/P&gt;&lt;P&gt;SELinux:&amp;nbsp; Initializing.&lt;/P&gt;&lt;P&gt;SELinux:&amp;nbsp; Starting in permissive mode&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;regulator: core version 0.5&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;regulator: vddd: 800 &amp;lt;--&amp;gt; 1575 mV at 1500 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: vdddbo: 800 &amp;lt;--&amp;gt; 1575 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: vdda: 1500 &amp;lt;--&amp;gt; 2275 mV at 1800 mV fast normal&lt;/P&gt;&lt;P&gt;vddio = 3380000, val=10&lt;/P&gt;&lt;P&gt;regulator: vddio: 2880 &amp;lt;--&amp;gt; 3680 mV at 3380 mV fast normal&lt;/P&gt;&lt;P&gt;regulator: overall_current: fast normal&lt;/P&gt;&lt;P&gt;regulator: vbus5v:&lt;/P&gt;&lt;P&gt;regulator: mxs-duart-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mxs-bl-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mxs-i2c-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mmc_ssp-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: mmc_ssp-2: fast normal&lt;/P&gt;&lt;P&gt;regulator: charger-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: power-test-1: fast normal&lt;/P&gt;&lt;P&gt;regulator: cpufreq-1: fast normal&lt;/P&gt;&lt;P&gt;i.MX IRAM pool: 124 KB@0xc8820000&lt;/P&gt;&lt;P&gt;Initializing GPMI pins&lt;/P&gt;&lt;P&gt;usb DR wakeup device is registered&lt;/P&gt;&lt;P&gt;IMX usb wakeup probe&lt;/P&gt;&lt;P&gt;the wakeup pdata is 0xc0500c1c&lt;/P&gt;&lt;P&gt;audit: cannot initialize inotify handle&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;Freescale USB OTG Driver loaded, $Revision: 1.55 $&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Version 1.0.23.&lt;/P&gt;&lt;P&gt;Switching to clocksource mxs clock source&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;IP route cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 4096 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;/P&gt;&lt;P&gt;TCP reno registered&lt;/P&gt;&lt;P&gt;UDP hash table entries: 256 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/P&gt;&lt;P&gt;Trying to unpack rootfs image as initramfs...&lt;/P&gt;&lt;P&gt;rootfs image is not initramfs (junk in compressed archive); looks like an initrd&lt;/P&gt;&lt;P&gt;Freeing initrd memory: 4096K&lt;/P&gt;&lt;P&gt;Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;IMX usb wakeup probe&lt;/P&gt;&lt;P&gt;the wakeup pdata is 0xc05010cc&lt;/P&gt;&lt;P&gt;usb h1 wakeup device is registered&lt;/P&gt;&lt;P&gt;mxs_cpu_init: cpufreq init finished&lt;/P&gt;&lt;P&gt;audit: initializing netlink socket (disabled)&lt;/P&gt;&lt;P&gt;type=2000 audit(0.670:1): initialized&lt;/P&gt;&lt;P&gt;VFS: Disk quotas dquot_6.5.2&lt;/P&gt;&lt;P&gt;Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;msgmni has been set to 242&lt;/P&gt;&lt;P&gt;alg: No test for stdrng (krng)&lt;/P&gt;&lt;P&gt;cryptodev: driver loaded.&lt;/P&gt;&lt;P&gt;Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 100x30&lt;/P&gt;&lt;P&gt;mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART&lt;/P&gt;&lt;P&gt;mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0&lt;/P&gt;&lt;P&gt;Found APPUART 3.1.0&lt;/P&gt;&lt;P&gt;mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1&lt;/P&gt;&lt;P&gt;Found APPUART 3.1.0&lt;/P&gt;&lt;P&gt;mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2&lt;/P&gt;&lt;P&gt;Found APPUART 3.1.0&lt;/P&gt;&lt;P&gt;mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3&lt;/P&gt;&lt;P&gt;Found APPUART 3.1.0&lt;/P&gt;&lt;P&gt;brd: module loaded&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;i.MX GPMI NFC&lt;/P&gt;&lt;P&gt;NFC: Version 1, 8-chip GPMI and BCH&lt;/P&gt;&lt;P&gt;Boot ROM: Version 1, Single-chip boot area, block mark swapping supported&lt;/P&gt;&lt;P&gt;Scanning for NAND Flash chips...&lt;/P&gt;&lt;P&gt;No NAND device found.&lt;/P&gt;&lt;P&gt;gpmi-nfc gpmi-nfc.0: Chip scan failed&lt;/P&gt;&lt;P&gt;mxs-spi mxs-spi.0: Max possible speed 24000 = 24000000/2 kHz&lt;/P&gt;&lt;P&gt;mxs-spi mxs-spi.0: at 0x80014000 mapped to 0xF0014000, irq=84, bus 1, DMA ver_major 4&lt;/P&gt;&lt;P&gt;FEC Ethernet Driver&lt;/P&gt;&lt;P&gt;fec_enet_mii_bus: probed&lt;/P&gt;&lt;P&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: irq 93, io base 0x80080000&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 2-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 2-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver...&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;USB Mass Storage support registered.&lt;/P&gt;&lt;P&gt;ARC USBOTG Device Controller driver (1 August 2005)&lt;/P&gt;&lt;P&gt;mice: PS/2 mouse device common for all mice&lt;/P&gt;&lt;P&gt;input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0&lt;/P&gt;&lt;P&gt;input: MXS touchscreen as /devices/virtual/input/input1&lt;/P&gt;&lt;P&gt;MXS RTC driver v1.0 hardware v2.3.0&lt;/P&gt;&lt;P&gt;mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0&lt;/P&gt;&lt;P&gt;IR NEC protocol handler initialized&lt;/P&gt;&lt;P&gt;IR RC5(x) protocol handler initialized&lt;/P&gt;&lt;P&gt;IR RC6 protocol handler initialized&lt;/P&gt;&lt;P&gt;IR JVC protocol handler initialized&lt;/P&gt;&lt;P&gt;IR Sony protocol handler initialized&lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00&lt;/P&gt;&lt;P&gt;mxs-pxp mxs-pxp.0: initialized&lt;/P&gt;&lt;P&gt;mxs watchdog: initialized, heartbeat 19 sec&lt;/P&gt;&lt;P&gt;mxs-mmc: MXS SSP Controller MMC Interface driver&lt;/P&gt;&lt;P&gt;mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96&lt;/P&gt;&lt;P&gt;Registered led device: led-pwm0&lt;/P&gt;&lt;P&gt;Registered led device: led-pwm1&lt;/P&gt;&lt;P&gt;dcp dcp.0: DCP crypto enabled.!&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hiddev&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: USB HID core driver&lt;/P&gt;&lt;P&gt;4P2 rail started.&amp;nbsp; 5V current limit&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set to 450mA&lt;/P&gt;&lt;P&gt;sgtl5000-i2c 0-000a: SGTL5000 revision 17&lt;/P&gt;&lt;P&gt;mxs-spdif mxs-spdif.0: MXS SPDIF Audio Transmitter&lt;/P&gt;&lt;P&gt;No device for codec mxs spdif&lt;/P&gt;&lt;P&gt;No device for DAI mxs spdif&lt;/P&gt;&lt;P&gt;No device for DAI mxs-saif&lt;/P&gt;&lt;P&gt;No device for DAI mxs-spdif&lt;/P&gt;&lt;P&gt;asoc: SGTL5000 &amp;lt;-&amp;gt; mxs-saif mapping ok&lt;/P&gt;&lt;P&gt;mmc0: new high speed SDHC card at address aaaa&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:aaaa SU04G 3.69 GiB&lt;/P&gt;&lt;P&gt; mmcblk0: p1 p2 p3&lt;/P&gt;&lt;P&gt;Failed to add route LINE_OUT-&amp;gt;Ext Spk&lt;/P&gt;&lt;P&gt;asoc: mxs spdif &amp;lt;-&amp;gt; mxs-spdif mapping ok&lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: mxs-evk (SGTL5000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; #1: mxs-evk (mxs spdif)&lt;/P&gt;&lt;P&gt;TCP cubic registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;can: controller area network core (rev 20090105 abi 8)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 29&lt;/P&gt;&lt;P&gt;can: raw protocol (rev 20090105)&lt;/P&gt;&lt;P&gt;mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:03:53 UTC (233)&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p3): warning: mounting unchecked fs, running e2fsck is recommended&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext2 filesystem) on device 179:3.&lt;/P&gt;&lt;P&gt;Freeing init memory: 160K&lt;/P&gt;&lt;P&gt;USB Host suspend begins&lt;/P&gt;&lt;P&gt;will suspend roothub and its children&lt;/P&gt;&lt;P&gt;ehci_fsl_bus_suspend, DR&lt;/P&gt;&lt;P&gt;host suspend ends&lt;/P&gt;&lt;P&gt;ehci_fsl_bus_suspend, Host 1&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p3): error: ext2_lookup: deleted inode referenced: 212676&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p3): error: ext2_lookup: deleted inode referenced: 212676&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p3): error: ext2_lookup: deleted inode referenced: 212676&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 14:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281979#M32640</guid>
      <dc:creator>jallocator</dc:creator>
      <dc:date>2014-02-06T14:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 EVK USB unpowered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281980#M32641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Dumb question,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You've switched the switch on board so that the usb is powered?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I'm at home now, but I'll get the refdes for you tomorrow. It's pretty obvious which one it is though.&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 19:43:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281980#M32641</guid>
      <dc:creator>peteewg</dc:creator>
      <dc:date>2014-02-11T19:43:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 EVK USB unpowered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281981#M32642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Peter, the USB 5V switch is switched on and it doesn't help:smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've used the USB OTG to update the kernel using the MFG tool and the EVK has enumerated as a USB HID device as well as using the USB OTG jack as the power source. So the USB OTG jack seems to work fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2014 08:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281981#M32642</guid>
      <dc:creator>jallocator</dc:creator>
      <dc:date>2014-02-12T08:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 EVK USB unpowered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281982#M32643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In which case everything looks good from the log file,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming you are using the host port (The big USB A Connector) and not the OSB OTG port.&lt;/P&gt;&lt;P&gt;I notice it is suspending the USB host functionality at the end, without going too far into it, it might just be power saving?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you get anything when you type : lsusb from the cmd prompt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, can you put a scope probe on the Vbus line as well as R194, You should be able to see some waveform activity?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll try a build later with my USB port enabled and see what happens on my EVK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2014 09:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281982#M32643</guid>
      <dc:creator>peteewg</dc:creator>
      <dc:date>2014-02-12T09:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 EVK USB unpowered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281983#M32644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running lsusb -v-t gives&lt;/P&gt;&lt;P&gt;&lt;EM&gt;cannot open /proc/bus/usb/devices, No such file or directory (2)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;forcing power to on makes the autosuspend to resume.&lt;/P&gt;&lt;P&gt;echo "on" &amp;gt; /sys/bus/usb/devices/2-0\:1.0/power/control&lt;/P&gt;&lt;P&gt;echo "on" &amp;gt; /sys/bus/usb/devices/1-0\:1.0/power/control&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ehci_fsl_bus_resume, Host 1&lt;BR /&gt;ehci_fsl_bus_resume, DR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I havn't been able to scope the R194 and the VBUS line, yet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 09:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-EVK-USB-unpowered/m-p/281983#M32644</guid>
      <dc:creator>jallocator</dc:creator>
      <dc:date>2014-02-14T09:19:33Z</dc:date>
    </item>
  </channel>
</rss>