<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAdd a custom codec component to OMXPlayer</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Add-a-custom-codec-component-to-OMXPlayer/m-p/160558#M3253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;In multimedia framework of 10.3.1 android, there are 3 players to play media. They are OMXPlayer，MidiFile，StagefrightPlayer.&lt;/P&gt;&lt;P&gt;OMXPlayer is provided by FSL as .so library. It includes omx core, omx codec component and omx data pipe.&lt;/P&gt;&lt;P&gt;Now I want to add a new codec(such as *.mymp4), also it should be displayed by ipu.&lt;/P&gt;&lt;P&gt;So could I add a new omx codec component(according to openmax IL interface)? Then I register it in /etc/component_register. Could OMXPlayer recognize and play it correctly?&lt;/P&gt;&lt;P&gt;Since there isn't any source code of OMXPlayer, is it reasonable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS：Although StagefrightPlayer supports to add a custom codec, but I don't think it use overlay. It should be displayed by SW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 May 2012 06:36:45 GMT</pubDate>
    <dc:creator>dorothyxsara</dc:creator>
    <dc:date>2012-05-11T06:36:45Z</dc:date>
    <item>
      <title>Add a custom codec component to OMXPlayer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-a-custom-codec-component-to-OMXPlayer/m-p/160558#M3253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;In multimedia framework of 10.3.1 android, there are 3 players to play media. They are OMXPlayer，MidiFile，StagefrightPlayer.&lt;/P&gt;&lt;P&gt;OMXPlayer is provided by FSL as .so library. It includes omx core, omx codec component and omx data pipe.&lt;/P&gt;&lt;P&gt;Now I want to add a new codec(such as *.mymp4), also it should be displayed by ipu.&lt;/P&gt;&lt;P&gt;So could I add a new omx codec component(according to openmax IL interface)? Then I register it in /etc/component_register. Could OMXPlayer recognize and play it correctly?&lt;/P&gt;&lt;P&gt;Since there isn't any source code of OMXPlayer, is it reasonable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS：Although StagefrightPlayer supports to add a custom codec, but I don't think it use overlay. It should be displayed by SW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 May 2012 06:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-a-custom-codec-component-to-OMXPlayer/m-p/160558#M3253</guid>
      <dc:creator>dorothyxsara</dc:creator>
      <dc:date>2012-05-11T06:36:45Z</dc:date>
    </item>
  </channel>
</rss>