<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Activating CAAM HW acceleration in linux kernel on i.mx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281541#M32514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am starting to work with an i.mx6 evaluation board and I can't activate CAAM in my linux kernel configuration.&lt;BR /&gt;It depends on the KConfig option "FSL_SOC" and this option is effectively not selected for the i.mx processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/caam/Kconfig?id=refs/tags/v3.10-rc7" title="https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/caam/Kconfig?id=refs/tags/v3.10-rc7"&gt;https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/caam/Kconfig?id=refs/tags/v3.10-rc7&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;config CRYPTO_DEV_FSL_CAAM&lt;BR /&gt;&amp;nbsp; tristate "Freescale CAAM-Multicore driver backend"&lt;BR /&gt;&amp;nbsp; depends on FSL_SOC&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it intended ?&lt;/P&gt;&lt;P&gt;Thanks in advance !&lt;/P&gt;&lt;P&gt;JM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2013 13:24:53 GMT</pubDate>
    <dc:creator>jean-michelhaut</dc:creator>
    <dc:date>2013-08-29T13:24:53Z</dc:date>
    <item>
      <title>Activating CAAM HW acceleration in linux kernel on i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281541#M32514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am starting to work with an i.mx6 evaluation board and I can't activate CAAM in my linux kernel configuration.&lt;BR /&gt;It depends on the KConfig option "FSL_SOC" and this option is effectively not selected for the i.mx processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/caam/Kconfig?id=refs/tags/v3.10-rc7" title="https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/caam/Kconfig?id=refs/tags/v3.10-rc7"&gt;https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/crypto/caam/Kconfig?id=refs/tags/v3.10-rc7&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;config CRYPTO_DEV_FSL_CAAM&lt;BR /&gt;&amp;nbsp; tristate "Freescale CAAM-Multicore driver backend"&lt;BR /&gt;&amp;nbsp; depends on FSL_SOC&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it intended ?&lt;/P&gt;&lt;P&gt;Thanks in advance !&lt;/P&gt;&lt;P&gt;JM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2013 13:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281541#M32514</guid>
      <dc:creator>jean-michelhaut</dc:creator>
      <dc:date>2013-08-29T13:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: Activating CAAM HW acceleration in linux kernel on i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281542#M32515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jean-Michel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default, &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;CAAM&lt;/STRONG&gt;&lt;/SPAN&gt; is disabled. If you want to use &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;CAAM&lt;/STRONG&gt;&lt;/SPAN&gt; module, please specify &lt;/P&gt;&lt;P&gt;"caam" to the kernel command line.&lt;/P&gt;&lt;P&gt;CAAM uses ALT7 mode of pad GPIO_0, which conflicts with any othermodule that using pad GPIO_0 on the board.&lt;/P&gt;&lt;P&gt;On this board &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;CAAM&lt;/STRONG&gt;&lt;/SPAN&gt; conflicts with audio codec (WM8962) and camera(ov5642) module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, it is needed to rebuild kernel in order to disable the codec and the cam.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next, to see &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;CAAM&lt;/STRONG&gt;&lt;/SPAN&gt; activities, please use /proc/interrupts of Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, the following community thread may be usefull &lt;/P&gt;&lt;P&gt;Freescale has some patches that address the &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;CAAM&lt;/STRONG&gt;&lt;/SPAN&gt; driver crash. &lt;/P&gt;&lt;P&gt;These patches will hopefully be included in the next BSP update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="335389" data-objecttype="2" href="https://community.freescale.com/message/335389#335389"&gt;https://community.freescale.com/message/335389#335389&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 15:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281542#M32515</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-09-05T15:54:03Z</dc:date>
    </item>
    <item>
      <title>Re: Activating CAAM HW acceleration in linux kernel on i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281543#M32516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have removed audio codec (WM8962) and camera(ov5642) module from kernel configs.&lt;/P&gt;&lt;P&gt;Appended 'caam=1' to kernel bootparm.&lt;/P&gt;&lt;P&gt;I still don't see any caam activity in kernel. :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2013 15:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281543#M32516</guid>
      <dc:creator>adnana</dc:creator>
      <dc:date>2013-09-23T15:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: Activating CAAM HW acceleration in linux kernel on i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281544#M32517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following may be useful :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/339153#339153"&gt;https://community.freescale.com/message/339153#339153&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2013 02:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281544#M32517</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-09-24T02:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: Activating CAAM HW acceleration in linux kernel on i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281545#M32518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also found same problem with Linux Kernel which I am using. Its strange &amp;amp; a obvious Bug :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Feb 2015 13:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Activating-CAAM-HW-acceleration-in-linux-kernel-on-i-mx6/m-p/281545#M32518</guid>
      <dc:creator>ravikiran</dc:creator>
      <dc:date>2015-02-16T13:49:45Z</dc:date>
    </item>
  </channel>
</rss>