<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Reg: UART Interrupts</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reg-UART-Interrupts/m-p/281316#M32400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vishva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the linux reference manual, in the chapter about the Universal Asynchronous Receiver/Transmitter (UART) Driver, you will see where the UART driver is (which uses interrupt method).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Source Code Structure&lt;/P&gt;&lt;P&gt;Universal Asynchronous Receiver/Transmitter (UART) Driver&lt;/P&gt;&lt;P&gt;&amp;lt;ltib_dir&amp;gt;/rpm/BUILD/linux/drivers/tty/serial.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That would be the only available example.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Sep 2013 17:21:10 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2013-09-04T17:21:10Z</dc:date>
    <item>
      <title>Reg: UART Interrupts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reg-UART-Interrupts/m-p/281315#M32399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using &lt;A href="http://I.MX/" target="_blank"&gt;I.MX&lt;/A&gt; sabre SDB. I am using 3 uarts in my EVB. i am using thm in polling method. I would like to use the same in Interrupt method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly give some pointers or sample codes to use Interrupts in the Processor under Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I already checked Linux Ref manual, but i didnt find any.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Vishva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2013 07:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reg-UART-Interrupts/m-p/281315#M32399</guid>
      <dc:creator>vishvapathi</dc:creator>
      <dc:date>2013-08-29T07:38:33Z</dc:date>
    </item>
    <item>
      <title>Re: Reg: UART Interrupts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reg-UART-Interrupts/m-p/281316#M32400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vishva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the linux reference manual, in the chapter about the Universal Asynchronous Receiver/Transmitter (UART) Driver, you will see where the UART driver is (which uses interrupt method).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Source Code Structure&lt;/P&gt;&lt;P&gt;Universal Asynchronous Receiver/Transmitter (UART) Driver&lt;/P&gt;&lt;P&gt;&amp;lt;ltib_dir&amp;gt;/rpm/BUILD/linux/drivers/tty/serial.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That would be the only available example.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2013 17:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reg-UART-Interrupts/m-p/281316#M32400</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-09-04T17:21:10Z</dc:date>
    </item>
  </channel>
</rss>