<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックInfo: Using older mxc_ipudev_test on newer BSP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160507#M3238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;The previous mxc_ipudev_test supplied in BSP 10.04 contains a lot of very useful sample code and tests which are completely missing from the latest ipudev test. The newer IPU libraries are not completely compatible with the older ipudev tests, so I've made the necessary changes to the older version so it runs with the newer libraries and I've attached it here in case it's useful to others.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336346"&gt;177-1004mxc_ipudev_test.tar.gz&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 May 2012 14:53:54 GMT</pubDate>
    <dc:creator>StevieRG</dc:creator>
    <dc:date>2012-05-11T14:53:54Z</dc:date>
    <item>
      <title>Info: Using older mxc_ipudev_test on newer BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160507#M3238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;The previous mxc_ipudev_test supplied in BSP 10.04 contains a lot of very useful sample code and tests which are completely missing from the latest ipudev test. The newer IPU libraries are not completely compatible with the older ipudev tests, so I've made the necessary changes to the older version so it runs with the newer libraries and I've attached it here in case it's useful to others.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336346"&gt;177-1004mxc_ipudev_test.tar.gz&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 May 2012 14:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160507#M3238</guid>
      <dc:creator>StevieRG</dc:creator>
      <dc:date>2012-05-11T14:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: Info: Using older mxc_ipudev_test on newer BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160508#M3239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale doesn't seem to provide this code anymore, so many thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 02:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160508#M3239</guid>
      <dc:creator>fcs</dc:creator>
      <dc:date>2012-10-17T02:29:44Z</dc:date>
    </item>
    <item>
      <title>Re: Info: Using older mxc_ipudev_test on newer BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160509#M3240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to convert bayer format into some other formats using this test code ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 11:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Info-Using-older-mxc-ipudev-test-on-newer-BSP/m-p/160509#M3240</guid>
      <dc:creator>ela_embedded</dc:creator>
      <dc:date>2015-01-05T11:30:04Z</dc:date>
    </item>
  </channel>
</rss>