<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NVCC_SRTC_POW's voltage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281097#M32342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Xiaobing,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; According to your description, It seems that there exists leakage of electricity at a certain place on your baord , and the issue should be caused by 3.3V output from LTC3589.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Could you tell me the following messages about your design ?&lt;/P&gt;&lt;P&gt;(1)Can the board normally boot ?&lt;/P&gt;&lt;P&gt;(2)Can SRTC normally work ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Oct 2013 03:34:24 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2013-10-28T03:34:24Z</dc:date>
    <item>
      <title>NVCC_SRTC_POW's voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281095#M32340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hello, I need your help.&lt;/P&gt;&lt;P&gt;The problem is like this. I use a LTC3589-1 as the power supply IC for iMX536. The NVCC_SRTC_POW is supplied by LTC3589-1's LDO1. Before power up of VIO_3.3V, LDO1 is 1.3V, but after Vio is powered on as 3.3V, LDO1's voltage becomes 1.87V. Disconnect the NVCC_SRTC_POW pad and LTC3589-1's LDO1, NVCC_SRTC_POW's voltage is 1.87V, and LDO1's voltage is 1.35V. It is my first time to use LTC3589-1 as a PMIC,&amp;nbsp; Is there something fault and the fault information show out through the pad?&lt;/P&gt;&lt;P&gt;3x for your attention.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2013 02:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281095#M32340</guid>
      <dc:creator>xiaobingtang</dc:creator>
      <dc:date>2013-10-16T02:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: NVCC_SRTC_POW's voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281096#M32341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I cut off the LT3589-1's Regulator 4 through U-boot,that is to say,there is no 3.3V power on the board,then I can measure the NVCC_SRTC_POW pad's voltage is about 0.68V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2013 08:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281096#M32341</guid>
      <dc:creator>xiaobingtang</dc:creator>
      <dc:date>2013-10-16T08:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: NVCC_SRTC_POW's voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281097#M32342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Xiaobing,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; According to your description, It seems that there exists leakage of electricity at a certain place on your baord , and the issue should be caused by 3.3V output from LTC3589.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Could you tell me the following messages about your design ?&lt;/P&gt;&lt;P&gt;(1)Can the board normally boot ?&lt;/P&gt;&lt;P&gt;(2)Can SRTC normally work ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2013 03:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-SRTC-POW-s-voltage/m-p/281097#M32342</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-10-28T03:34:24Z</dc:date>
    </item>
  </channel>
</rss>