<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6 ENET module not calculating CRC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280842#M32250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am reusing an ENET driver that worked on Kinetis on iMX6Q. It uses enhanced transmit buffer descriptors. The descriptor have the&amp;nbsp; PINS bit set, but an iCMP frame as seen by Wireshark has 0xFFFF for the CRC. When I turn off PINS and calculate my own CRC, I have no frame problems and a full working network stack.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have looked at all the bits in the descriptor and can't find anything unusual. As I said, this code has worked fine on Kinetis for lots of people. The only changes I made to the code was to enable RGMII and deal with pin mixing and enabling, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the frame is more than 64 bytes, so there should not be a problem related to padding. Note that the buffers used by the driver are all in OCRAM, nonchached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me if there is a known problem or what might cause the CRC not to calculate? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Dec 2013 00:25:35 GMT</pubDate>
    <dc:creator>MikeJones</dc:creator>
    <dc:date>2013-12-28T00:25:35Z</dc:date>
    <item>
      <title>iMX6 ENET module not calculating CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280842#M32250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am reusing an ENET driver that worked on Kinetis on iMX6Q. It uses enhanced transmit buffer descriptors. The descriptor have the&amp;nbsp; PINS bit set, but an iCMP frame as seen by Wireshark has 0xFFFF for the CRC. When I turn off PINS and calculate my own CRC, I have no frame problems and a full working network stack.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have looked at all the bits in the descriptor and can't find anything unusual. As I said, this code has worked fine on Kinetis for lots of people. The only changes I made to the code was to enable RGMII and deal with pin mixing and enabling, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the frame is more than 64 bytes, so there should not be a problem related to padding. Note that the buffers used by the driver are all in OCRAM, nonchached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me if there is a known problem or what might cause the CRC not to calculate? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Dec 2013 00:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280842#M32250</guid>
      <dc:creator>MikeJones</dc:creator>
      <dc:date>2013-12-28T00:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 ENET module not calculating CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280843#M32251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; I really recommend, if you need a bareboard driver for the FEC of the i.MX6Q you use the&amp;nbsp; one available in the SDK software package available in the official web page of the i.Mx6Q .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 18:48:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280843#M32251</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-01-23T18:48:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 ENET module not calculating CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280844#M32252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am aware of the SDK and have used large portions of it. In this case the driver I started with was converted to support RGMII and has worked flawlessly for over a month. Therefore, I am asking for help getting CRC to work, not for a substitute solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please give some insights as to what might prevent the CRC from calculating?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jan 2014 22:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280844#M32252</guid>
      <dc:creator>MikeJones</dc:creator>
      <dc:date>2014-01-24T22:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 ENET module not calculating CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280845#M32253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you share the configuration registers of the ENET that you are using?? or the modified code? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 22:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280845#M32253</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-01-28T22:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 ENET module not calculating CRC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280846#M32254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://sourceforge.net/p/ecosfreescale/code/HEAD/tree/trunk/packages/devs/eth/freescale/enet/current/"&gt;http://sourceforge.net/p/ecosfreescale/code/HEAD/tree/trunk/packages/devs/eth/freescale/enet/current/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This link takes you to the source code. There are only a couple of files. Note that I use it in RGMII mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 14:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-ENET-module-not-calculating-CRC/m-p/280846#M32254</guid>
      <dc:creator>MikeJones</dc:creator>
      <dc:date>2014-02-06T14:52:49Z</dc:date>
    </item>
  </channel>
</rss>