<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing CSI test generator mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160454#M3218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the CSI module and since the camera interface hardware is not ready, I am trying to make use of the test generator mode by following System Development Users Guide (chapter 20).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I can not make it working, and after hours of greping, searching, adding printks and what not through the complex mass of files and functions involved, I want to start over with a perhaps simpler task: Make the CSI0 generated chess board show up on the VGA monitor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it at all possible to use the CSI test mode this way without any additional hardware? And if so, can anyone walk me through it or give some guidance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Edit:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Does the test mode work without external clocks for instance? The user guide says that "The CSI generates a frame by itself and sends it to one of the destination units", but there might be a reason why the user guide also shows how to connect a camera...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Trond&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Oct 2012 10:42:48 GMT</pubDate>
    <dc:creator>tw_imx53_</dc:creator>
    <dc:date>2012-10-31T10:42:48Z</dc:date>
    <item>
      <title>Using CSI test generator mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160454#M3218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the CSI module and since the camera interface hardware is not ready, I am trying to make use of the test generator mode by following System Development Users Guide (chapter 20).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I can not make it working, and after hours of greping, searching, adding printks and what not through the complex mass of files and functions involved, I want to start over with a perhaps simpler task: Make the CSI0 generated chess board show up on the VGA monitor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it at all possible to use the CSI test mode this way without any additional hardware? And if so, can anyone walk me through it or give some guidance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Edit:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Does the test mode work without external clocks for instance? The user guide says that "The CSI generates a frame by itself and sends it to one of the destination units", but there might be a reason why the user guide also shows how to connect a camera...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Trond&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2012 10:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160454#M3218</guid>
      <dc:creator>tw_imx53_</dc:creator>
      <dc:date>2012-10-31T10:42:48Z</dc:date>
    </item>
    <item>
      <title>Re: Using CSI test generator mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160455#M3219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I have a document talk about this. Hope this can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2012 07:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160455#M3219</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2012-11-07T07:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: Using CSI test generator mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160456#M3220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The document provided was pretty much the same as found in the dev. guide, but the patch files were &lt;EM&gt;exactly&lt;/EM&gt; what I needed. I guess they are based on an earlier release than the L2.6.35_11.09.01 source bundle I use, but by applying the marked-up line changes and a little more tweaking I finally got the chess board on the screen. Finally I have something to work with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;P&gt;Trond&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2012 10:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160456#M3220</guid>
      <dc:creator>tw_imx53_</dc:creator>
      <dc:date>2012-11-07T10:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: Using CSI test generator mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160457#M3221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's great! :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2012 10:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-CSI-test-generator-mode/m-p/160457#M3221</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2012-11-07T10:49:47Z</dc:date>
    </item>
  </channel>
</rss>