<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Difference between USB recovery and USB boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280513#M32159</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, &lt;/P&gt;&lt;P&gt;according to section 11.4.3 (Software Functions/Recovery Mode) of the i.MX28 RM :&lt;/P&gt;&lt;P&gt;"When the PSWITCH pin is connected to VDDIO through a current limiting resistor, the&lt;/P&gt;&lt;P&gt;upper HW_POWER_STS_PSWITCH bit is also set. If this bit is set for more than five&lt;/P&gt;&lt;P&gt;seconds during ROM boot, the system executes the Freescale USB Firmware Recovery&lt;/P&gt;&lt;P&gt;function, as described in Boot Modes."&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2013 05:14:28 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-07-19T05:14:28Z</dc:date>
    <item>
      <title>Difference between USB recovery and USB boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280510#M32156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder what's the difference between entering USB recovery mode and changing boot switches to USB boot?&lt;/P&gt;&lt;P&gt;If I want to use mfgtools can I just plug USB OTG into my computer and set switches to USB boot and I'm all set to flash to nand and so on?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 12:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280510#M32156</guid>
      <dc:creator>rajtantajtan</dc:creator>
      <dc:date>2013-07-18T12:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between USB recovery and USB boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280511#M32157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right - to enter USB recovery mode the boot switch should be configured for USB boot.&lt;/P&gt;&lt;P&gt;Also USB recovery mode is entered automatically when boot, say from SD, is crashed (no SD inserted). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 04:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280511#M32157</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-19T04:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between USB recovery and USB boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280512#M32158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But what happens when you apply HIGH LEVEL voltage on PSWITCH?&amp;nbsp; Is this the same as changing boot switches to USB boot?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 05:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280512#M32158</guid>
      <dc:creator>rajtantajtan</dc:creator>
      <dc:date>2013-07-19T05:03:10Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between USB recovery and USB boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280513#M32159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, &lt;/P&gt;&lt;P&gt;according to section 11.4.3 (Software Functions/Recovery Mode) of the i.MX28 RM :&lt;/P&gt;&lt;P&gt;"When the PSWITCH pin is connected to VDDIO through a current limiting resistor, the&lt;/P&gt;&lt;P&gt;upper HW_POWER_STS_PSWITCH bit is also set. If this bit is set for more than five&lt;/P&gt;&lt;P&gt;seconds during ROM boot, the system executes the Freescale USB Firmware Recovery&lt;/P&gt;&lt;P&gt;function, as described in Boot Modes."&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 05:14:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-USB-recovery-and-USB-boot/m-p/280513#M32159</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-19T05:14:28Z</dc:date>
    </item>
  </channel>
</rss>