<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279427#M31936</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your boot command parameter is not correct. The kernel is looking for rootfs from mmcblk0p3.&lt;/P&gt;&lt;P&gt;"-e noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none gpmi"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For NAND it should be console=ttyAM0,115200 ubi.mtd=1 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;run ./ltib -m config -&amp;gt; Package list to set the correct boot command. &lt;/P&gt;&lt;P&gt;By default, 4 cmdlines are defined and cmdlines[0] is used as default boot. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jan 2014 04:05:41 GMT</pubDate>
    <dc:creator>GraceH</dc:creator>
    <dc:date>2014-01-17T04:05:41Z</dc:date>
    <item>
      <title>what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279420#M31929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what version of mfgtll should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should&amp;nbsp; i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i can't boot my board after using the Mfgtools-Rel-1.6.2.048 ,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 03:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279420#M31929</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2013-12-23T03:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279421#M31930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think both should be OK. What is the console output when you try to boot your board? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 07:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279421#M31930</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-12-23T07:39:20Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279422#M31931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;As Vladan said both are ok, the &lt;STRONG&gt;L2.6.35_1.1.0_130130_source is newer. &lt;/STRONG&gt;When you boot your board what problems happen, could you describe the details?&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 07:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279422#M31931</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2013-12-23T07:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279423#M31932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please remember the following patch &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX287&amp;amp;nodeId=018rH3ZrDRA24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_1.1.1_UPDATER_PATCH_UP&lt;/A&gt; for 1.1.0 release.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 07:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279423#M31932</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-12-23T07:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279424#M31933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DAN:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           I used an 1G BYTE nand flash. it seems that I can’t download the hole images into the flash by using  mfgtool .i can download the image into the SD card after fixing the SD plug .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but I can’t boot the board from SD card(see” boot SD err.txt”). I can boot the board and login in with root ,after boot from nand flash with SD card pulg in(see”boot nand with SD card .txt” ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I boot from  nand flash without SD card? How can I boot from SD card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Can you tell me the password of the user of the board?&lt;/P&gt;&lt;P&gt;Thanks .&lt;/P&gt;&lt;P&gt;best regard！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steven Zhang&lt;/P&gt;&lt;P&gt;TEL.138 7588 9660&lt;/P&gt;&lt;P&gt;410000&lt;/P&gt;&lt;P&gt;长沙市枫林三路889号万科城市花园4栋1807室&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;寄件者: Dan Wang &lt;/P&gt;&lt;P&gt;寄件日期: 2013年12月23日 15:45&lt;/P&gt;&lt;P&gt;收件者: Steven Zhang(張志星)(ChangSha)&lt;/P&gt;&lt;P&gt;主旨: Re:  - what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Dan Wang&amp;lt;https://community.freescale.com/people/b45499?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/370345?et=watches.email.thread#370345&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 14:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279424#M31933</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2013-12-23T14:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279425#M31934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DAN:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           I used an 1G BYTE nand flash. it seems that I can’t download the hole images into the flash by using  mfgtool .i can download the image into the SD card after fixing the SD plug .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but I can’t boot the board from SD card(see” boot SD err.txt”). I can boot the board and login in with root ,after boot from nand flash with SD card pulg in(see”boot nand with SD card .txt” ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I boot from  nand flash without SD card? How can I boot from SD card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Can you tell me the password of the user of the board?&lt;/P&gt;&lt;P&gt;Thanks .&lt;/P&gt;&lt;P&gt;best regard！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steven Zhang&lt;/P&gt;&lt;P&gt;TEL.138 7588 9660&lt;/P&gt;&lt;P&gt;410000&lt;/P&gt;&lt;P&gt;长沙市枫林三路889号万科城市花园4栋1807室&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;寄件者: Dan Wang &lt;/P&gt;&lt;P&gt;寄件日期: 2013年12月23日 15:45&lt;/P&gt;&lt;P&gt;收件者: Steven Zhang(張志星)(ChangSha)&lt;/P&gt;&lt;P&gt;主旨: Re:  - what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Dan Wang&amp;lt;https://community.freescale.com/people/b45499?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/370345?et=watches.email.thread#370345&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 16:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279425#M31934</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2013-12-23T16:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279426#M31935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;admin:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           I used an 1G BYTE nand flash. it seems that I can’t download the hole images into the flash by using  mfgtool .i can download the image into the SD card after fixing the SD plug .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but I can’t boot the board from SD card(see” boot SD err.txt”). I can boot the board and login in with root ,after boot from nand flash with SD card pulg in(see”boot nand with SD card .txt” ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I boot from  nand flash without SD card? How can I boot from SD card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Can you tell me the password of the user of the board?&lt;/P&gt;&lt;P&gt;Thanks .&lt;/P&gt;&lt;P&gt;best regard！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steven Zhang&lt;/P&gt;&lt;P&gt;TEL.138 7588 9660&lt;/P&gt;&lt;P&gt;410000&lt;/P&gt;&lt;P&gt;长沙市枫林三路889号万科城市花园4栋1807室&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;寄件者: Vladan Jovanovic &lt;/P&gt;&lt;P&gt;寄件日期: 2013年12月23日 15:40&lt;/P&gt;&lt;P&gt;收件者: Steven Zhang(張志星)(ChangSha)&lt;/P&gt;&lt;P&gt;主旨: Re:  - what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Vladan Jovanovic&amp;lt;https://community.freescale.com/people/VladanJovanovic?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/370344?et=watches.email.thread#370344&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2013 16:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279426#M31935</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2013-12-23T16:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279427#M31936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your boot command parameter is not correct. The kernel is looking for rootfs from mmcblk0p3.&lt;/P&gt;&lt;P&gt;"-e noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none gpmi"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For NAND it should be console=ttyAM0,115200 ubi.mtd=1 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;run ./ltib -m config -&amp;gt; Package list to set the correct boot command. &lt;/P&gt;&lt;P&gt;By default, 4 cmdlines are defined and cmdlines[0] is used as default boot. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2014 04:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279427#M31936</guid>
      <dc:creator>GraceH</dc:creator>
      <dc:date>2014-01-17T04:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279428#M31937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;my SD card socket is not good ,so i got the problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Apr 2014 03:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279428#M31937</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2014-04-21T03:08:04Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279429#M31938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;It's great that you have solved your problem. Would you please help close this thread for us, Thanks a lot~&lt;/P&gt;&lt;P&gt;Have a great day&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Apr 2014 04:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279429#M31938</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-04-21T04:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279430#M31939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how to close it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Apr 2014 05:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279430#M31939</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2014-04-21T05:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: what version of mfgtool should i use if a got a iMX28_EVK. it's sch-26241 rev D and 700-26241 rev x3 ,and should  i use L2.6.35_10.12.01_SDK or L2.6.35_1.1.0_130130_source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279431#M31940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;You can close it by clicking on the Correct Answer or Helpful Answer button.Thanks a lot.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Apr 2014 06:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/what-version-of-mfgtool-should-i-use-if-a-got-a-iMX28-EVK-it-s/m-p/279431#M31940</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-04-21T06:12:11Z</dc:date>
    </item>
  </channel>
</rss>