<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Windows 7 and imx25pdk - usb issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160228#M3173</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 May 2012 23:21:21 GMT</pubDate>
    <dc:creator>andrew_questps</dc:creator>
    <dc:date>2012-05-30T23:21:21Z</dc:date>
    <item>
      <title>Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160219#M3164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone been able to use the imx25pdk with windows 7 (64bit) ?&amp;nbsp; In particular, the ATK tool to program the pdk over usb ? (Serial works, but takes hours to get the filesystem on the pdk, where usb is just minutes)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It (eg ATK)&amp;nbsp; works fine with XP (32 bit), but they gave me a new computer at work with Windows7 (64 bit) and I can't get the ATK to recognize the board now.&amp;nbsp; I followed the instructions in the release notes and user guide and installed the usb drivers, but its still not recognized.&amp;nbsp; Anyone else seen this,&amp;nbsp; and know how to work around it ?&amp;nbsp; Same issue with the Mfgtool program, but I'm not exactly surprised about that.&amp;nbsp; Last time I spoke with our Freescale rep, the imx25 wasn't supported by the Mfgtool, but was "planned".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2012 14:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160219#M3164</guid>
      <dc:creator>Don_ng</dc:creator>
      <dc:date>2012-05-10T14:00:22Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160220#M3165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Don,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the mfg tool group:&lt;/P&gt;&lt;P&gt;&lt;A href="http://imxcommunity.org/group/manufacturing-tool-mfgtool"&gt;http://imxcommunity.org/group/manufacturing-tool-mfgtool&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There is a release for i.MX25 posted there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Renato&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2012 14:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160220#M3165</guid>
      <dc:creator>Frias</dc:creator>
      <dc:date>2012-05-10T14:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160221#M3166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ATK were designed for WinXP, but the emulator in Win7 should do the trick: &lt;A href="http://www.microsoft.com/windows/virtual-pc/download.aspx" rel="nofollow" target="_blank"&gt;http://www.microsoft.com/windows/virtual-pc/download.aspx&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2012 15:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160221#M3166</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2012-05-10T15:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160222#M3167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have tried to connect USB in our own i.mx258 board to windows 7, but could not connect, then asked to the Freescale, they suggest us to connect to a PC with XP. Then we have able to connected the USB to the ATK with PC(XP).&amp;nbsp;May be the boot code in the i.mx258 is compatible with only XP?&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 May 2012 11:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160222#M3167</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2012-05-11T11:11:33Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160223#M3168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The atk tool doesn't have 64-bit drivers, which will be the problem you are seeing. The manufacturing tool has 32 and 64-bit drivers, and the latest WinCE bsps have an example iMX25 UUT project for using creating the image required for the manufacturing tool.&lt;/P&gt;&lt;P&gt;Personally I re-wrote the usb layer for the atk-tool using libusb on both linux and windows which works fine for x64 as well as x86 as it annoyed me that my development machine couldn't program my units.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2012 02:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160223#M3168</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-05-28T02:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160224#M3169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andre&lt;/P&gt;&lt;P&gt;If you would agree, that's the kind of enhancement that could help others. So, feel free to share :-)&lt;/P&gt;&lt;P&gt;Thanks for the community&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 May 2012 12:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160224#M3169</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2012-05-29T12:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160225#M3170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've attached my windows version of the usb driver. I installed LibUsbDotNet as it also provides the libusb-win32 package which is the usb driver I use to talk to the imx25. I think that once libusbdotnet is installed under the libusb-win32 directory in the installation directory there is a install-filter-win.exe that you need to run once the imx is connected and in load mode, then you can install a filter for the device so you can communicate with it.&lt;/P&gt;&lt;P&gt;The linux project I haven't cleaned up in a while so I'm not going to post it, but it is the same interface, it's just the build process (Makefile) and linker stuff are all the main changes as I only have a console app for linux. Libusb is so easy to install and use on Ubuntu compared to Win7, no configuration needed! Although finding the correct imx is a different story.&lt;/P&gt;&lt;P&gt;Good thing about this is I can still use the manufacturing tool or the atk tool on the one Win7 x64 machine. Works in VMs as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 05:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160225#M3170</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-05-30T05:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160226#M3171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Should always compile the code before posting to make sure it works! I had an unsaved file in the project....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 05:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160226#M3171</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-05-30T05:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160227#M3172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for sharing. I don't know what went wrong, but the file can't be downloaded, there's a denied access. Do you mind re-posting it please?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 16:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160227#M3172</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2012-05-30T16:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160228#M3173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 23:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160228#M3173</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-05-30T23:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160229#M3174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hmmm, got the same result again. 3rd time lucky, maybe it didn't like the rar....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit: That worked, it really didn't like having a rar file for some reason.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 01:24:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160229#M3174</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-05-31T01:24:04Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160230#M3175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for the inconvenience, that works now. I wouldn't be surprised that rar or tar.gz would create issues.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 13:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160230#M3175</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2012-05-31T13:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160231#M3176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our problem is we are unable to work with cases&amp;nbsp; of&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When F=372 and D2 or 4 in SIM interface for imx258&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we achieve this by programming Divisor Reg as show in above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it is failing can we know the reason?&amp;nbsp; If we can achieve this by DIVISOR Reg we can save extra controller cost&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2012 06:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160231#M3176</guid>
      <dc:creator>rajansoma</dc:creator>
      <dc:date>2012-06-28T06:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 and imx25pdk - usb issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160232#M3177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;looking for a solution to run ATK on 64 bit windows.&amp;nbsp; I found this thread and the source code for your driver.&amp;nbsp; Not sure how to get from the source code to the LibUSBDotNet driver as a complete installer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 13:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Windows-7-and-imx25pdk-usb-issues/m-p/160232#M3177</guid>
      <dc:creator>philmac</dc:creator>
      <dc:date>2013-11-04T13:05:20Z</dc:date>
    </item>
  </channel>
</rss>