<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX25 Serial Boot Configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278660#M31651</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri, thanks for the reply I understand that is what is recommended.&amp;nbsp; Given the choice I would follow the PDK schematic.&amp;nbsp;&amp;nbsp; I have a board though that is NOT as recommended (not my design) and I'm trying to understand if it will properly serial boot or not.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2013 01:06:02 GMT</pubDate>
    <dc:creator>LI_Dave</dc:creator>
    <dc:date>2013-07-19T01:06:02Z</dc:date>
    <item>
      <title>i.MX25 Serial Boot Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278658#M31649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to boot a blank i.MX25 using the UART boot mode and have a question about what external boot pins really matter in this case.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I of course have BOOT_MODE_0 and BOOT_MODE_1 pulled high to select UART/USB Boot.&amp;nbsp; I've also got the three BT_UART_SRC lines pulled LOW to select UART1.&amp;nbsp; It would appear that nearly all the other boot config pin states are irrelevant to UART boot, but I'm not so sure about the BT_LPB_FREQ pins which configure the Low Power Boot mode.&amp;nbsp; Do they need to be set correctly (111)&amp;nbsp; to ensure successful UART boot?&amp;nbsp;&amp;nbsp; Is there anything else that needs to be tied to force a UART 1 Boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 02:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278658#M31649</guid>
      <dc:creator>LI_Dave</dc:creator>
      <dc:date>2013-07-18T02:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 Serial Boot Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278659#M31650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;General approach is as following - It is recommended to provide (proper / reasonable) configuration for all boot pins,&lt;/P&gt;&lt;P&gt;do not leave some of them free.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 03:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278659#M31650</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-18T03:15:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 Serial Boot Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278660#M31651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri, thanks for the reply I understand that is what is recommended.&amp;nbsp; Given the choice I would follow the PDK schematic.&amp;nbsp;&amp;nbsp; I have a board though that is NOT as recommended (not my design) and I'm trying to understand if it will properly serial boot or not.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 01:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-Serial-Boot-Configuration/m-p/278660#M31651</guid>
      <dc:creator>LI_Dave</dc:creator>
      <dc:date>2013-07-19T01:06:02Z</dc:date>
    </item>
  </channel>
</rss>