<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: vpudec does not like &amp;quot;queue(2)&amp;quot; in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278530#M31583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, that's sorted it :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please explain why there is a hard limit on the number of buffers in the pipeline? I thought that the limits were set by the elements and that it was this which set the limit in the pipeline.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2013 07:42:23 GMT</pubDate>
    <dc:creator>christapp</dc:creator>
    <dc:date>2013-07-19T07:42:23Z</dc:date>
    <item>
      <title>vpudec does not like "queue(2)"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278526#M31579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is best demonstrated using an example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;export GST_DEBUG="*:2"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1) gst-launch playbin2 uri=&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://media.w3.org/2010/05/sintel/trailer.webm"&gt;http://media.w3.org/2010/05/sintel/trailer.webm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2) gst-launch playbin2 uri=&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://media.w3.org/2010/05/sintel/trailer.webm"&gt;http://media.w3.org/2010/05/sintel/trailer.webm&lt;/A&gt;&lt;SPAN&gt; video-sink="multiqueue ! mfw_v4lsink"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3) gst-launch playbin2 uri=&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://media.w3.org/2010/05/sintel/trailer.webm"&gt;http://media.w3.org/2010/05/sintel/trailer.webm&lt;/A&gt;&lt;SPAN&gt; video-sink="queue ! mfw_v4lsink"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4) gst-launch playbin2 uri=&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://media.w3.org/2010/05/sintel/trailer.webm"&gt;http://media.w3.org/2010/05/sintel/trailer.webm&lt;/A&gt;&lt;SPAN&gt; video-sink="queue2 ! mfw_v4lsink"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Playback for 1) and 2) is good, where as playback for 3) and 4) starts of choppy, stalls and gets lots of messages of the form:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0:00:00.472157023&amp;nbsp; 7566 0x40d60150 WARN&amp;nbsp;&amp;nbsp;&amp;nbsp; vpudec vpudec.c:1578:gst_vpudec_chain: Got no frame buffer message, return 0x89, 10 frames in displaying queue!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GST_DEBUG=GST_ELEMENT_FACTORY:3 shows that playbin2 without the video-sink property uses 'multiqueue'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, it looks as if something is going on with 'vpudec' when the pipeline includes a 'queue' or 'queue2' element.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;This was running on a Wandboard Quad using an image built using Yocto.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Can anyone explain what's going on here?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2013 19:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278526#M31579</guid>
      <dc:creator>christapp</dc:creator>
      <dc:date>2013-07-17T19:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: vpudec does not like "queue(2)"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278527#M31580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another thread similar to this issue is &lt;A _jive_internal="true" href="https://community.nxp.com/message/339660"&gt;https://community.freescale.com/message/339660&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2013 22:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278527#M31580</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-07-17T22:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: vpudec does not like "queue(2)"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278528#M31581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it could well be related. The steps I've given above are repeatable without the 'random' behavior mentioned on the other issue, but it does also seem to be related to buffers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2013 23:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278528#M31581</guid>
      <dc:creator>christapp</dc:creator>
      <dc:date>2013-07-17T23:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: vpudec does not like "queue(2)"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278529#M31582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;UL style="list-style-type: disc;"&gt;&lt;LI&gt;1) and 2) is same as 1) will also add multiqueue element between VPU dec and V4lsink.&lt;/LI&gt;&lt;LI&gt;3) and 4) will add two queue between VPU dec and V4lsink. The pipeline is VPU dec-&amp;gt;multiqueue-&amp;gt;queue-&amp;gt;V4lsink.&lt;/LI&gt;&lt;LI&gt;Multiqueue will hold 3 buffer in it.&lt;/LI&gt;&lt;LI&gt;V4lsink need hold 2 buffer in it.&lt;/LI&gt;&lt;LI&gt;VPU dec default plus 6 frame buffer.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;So if add one queue between VPU dec and V4lsink will cause not enough frame buffer to run. So you command should be video-sink="queue max-size-buffers=1 max-size-bytes=0 max-size-time=0 ! mfw_v4lsink"&lt;/SPAN&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 07:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278529#M31582</guid>
      <dc:creator>jack_mao</dc:creator>
      <dc:date>2013-07-19T07:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: vpudec does not like "queue(2)"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278530#M31583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, that's sorted it :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please explain why there is a hard limit on the number of buffers in the pipeline? I thought that the limits were set by the elements and that it was this which set the limit in the pipeline.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 07:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278530#M31583</guid>
      <dc:creator>christapp</dc:creator>
      <dc:date>2013-07-19T07:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: vpudec does not like "queue(2)"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278531#M31584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the vpu buffers number can be set ,it should be in the VPU plugin, the default is 6, you could adjust it .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;frame-plus&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : set number of addtional frames for smoothly playback&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; flags: readable, writable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Integer. Range: 2 - 2147483647 Default: 6&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 08:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpudec-does-not-like-quot-queue-2-quot/m-p/278531#M31584</guid>
      <dc:creator>jack_mao</dc:creator>
      <dc:date>2013-07-19T08:15:33Z</dc:date>
    </item>
  </channel>
</rss>