<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SabreSD Kernel Not booting from TFTP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278516#M31574</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ben,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the numbers:&lt;/P&gt;&lt;P&gt;SCH-27392 REV C3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 700-27392 REV B&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is similar to Board#2 appart of C3 which is C4 on the board you mentioned.&lt;/P&gt;&lt;P&gt;However, my board exhibits the problem whereas the one you mentioned is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the mean time I managed to fully boot linux from NFS with the modified code and modified configuration as follows:&lt;/P&gt;&lt;P&gt;U-Boot 2009.08 (Apr 10 2013 - 18:58:57)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.2 at 792 MHz&lt;BR /&gt;Temperature:&amp;nbsp;&amp;nbsp; 34 C, calibration data 0x5ae50f7d&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 80000000Hz&lt;BR /&gt;cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 60000000Hz&lt;BR /&gt;ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 132000000Hz&lt;BR /&gt;axi clock&amp;nbsp;&amp;nbsp; : 264000000Hz&lt;BR /&gt;emi_slow clock: 29333333Hz&lt;BR /&gt;ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 528000000Hz&lt;BR /&gt;usdhc1 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc2 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc3 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc4 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 24000000Hz&lt;BR /&gt;Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]&lt;BR /&gt;Boot Device: SD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp;&amp;nbsp; 1 GB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Found PFUZE100! deviceid=10,revid=11&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; got MAC address from IIM: 00:04:9f:02:af:8b&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;MX6Q SABRESD U-Boot &amp;gt; pri&lt;BR /&gt;baudrate=115200&lt;BR /&gt;loadaddr=0x10800000&lt;BR /&gt;rd_loadaddr=0x11000000&lt;BR /&gt;netdev=eth0&lt;BR /&gt;ethprime=FEC0&lt;BR /&gt;fastboot_dev=mmc3&lt;BR /&gt;splashimage=0x30000000&lt;BR /&gt;splashpos=m,m&lt;BR /&gt;lvds_num=1&lt;BR /&gt;ethact=FEC0&lt;BR /&gt;bootdelay=6&lt;BR /&gt;kernel=uImage&lt;BR /&gt;bootcmd=booti mmc2&lt;BR /&gt;gateawayip=0.0.0.0&lt;BR /&gt;filesize=3AE998&lt;BR /&gt;fileaddr=10800000&lt;BR /&gt;netmask=255.255.255.0&lt;BR /&gt;ipaddr=192.168.42.30&lt;BR /&gt;serverip=192.168.42.1&lt;BR /&gt;boot_base=console=ttymxc0,115200&lt;BR /&gt;base_roots=/home/makis/imx6/ltib/rootfs&lt;BR /&gt;base_nfs=root=/dev/nfs ip=192.168.42.30 nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs,v3,tcp&lt;BR /&gt;bootargs=console=ttymxc0,115200 root=/dev/nfs ip=192.168.42.30 nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs,v3,tcp&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;stderr=serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then using:&lt;/P&gt;&lt;P&gt;tftp uImage&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;bootm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;got me to the free scale login screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As my board now seem to boot to linux, I assume is OK to use modified WDOG2 IOMUX setting to carry on with my work?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Jun 2013 16:20:34 GMT</pubDate>
    <dc:creator>makislivadas</dc:creator>
    <dc:date>2013-06-25T16:20:34Z</dc:date>
    <item>
      <title>SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278508#M31566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have iMX6q SabreSD board, that boots OK from SD card to Android.&lt;/P&gt;&lt;P&gt;I build basic Linux Kernel (minimal profile) and setup TFTP on the board.&lt;/P&gt;&lt;P&gt;I am using u-boot from Android SD card to boot Kernel via TFTP with NFS root file system.&lt;/P&gt;&lt;P&gt;TFTP is OK, as tftpboot will load the kernel to memory. When I use bootm to boot the kernel image the kernel boot will start but will fail very quickly and reboot the board. I tried a few kernel arguments by setting the bootargs environment variable in u-boot but did not have any success. I also tried to boot the kernel binary supplied by Freescale and it fails in the same way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any tips on how to do this? Setting bootargs looks tricky and there seems to be to many options to choose from which can be prone to error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 21:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278508#M31566</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-06-06T21:15:50Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278509#M31567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you try to print your bootup error message and uboot commands? let's check it. how did you set your uboot command for booting from tftp?&lt;/P&gt;&lt;P&gt;on my side, I can boot up the board using tftp, I tried the ubuntu image.&lt;/P&gt;&lt;P&gt;the steps are:&lt;/P&gt;&lt;P&gt;1)set up the host 2) restart the tftp and nfs 3) put the image to /tftpboot/, 4) set the uboot command&amp;nbsp; 4) run the bootcmd_net&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jun 2013 08:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278509#M31567</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2013-06-08T08:32:49Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278510#M31568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks you for your reply. I cannot try this untlil tuesday but will use your suggestion "run bootcmd_net" instead of what I am doing and see how is goiing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jun 2013 17:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278510#M31568</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-06-08T17:04:09Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278511#M31569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I set bootargs like in the trace below.&lt;/P&gt;&lt;P&gt;Then use "tftp uImage" to load kernel to RAM&lt;/P&gt;&lt;P&gt;Then use "bootm" to boot kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loading pre-build kernel image fails same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel will start booting but fails early on reseting the board. Console output is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;======================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bootargs=ip=192.168.42.30:192.168.42.1:0.0.0.0:255.255.255.0 console=ttymxc0,115200 root=nfs nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 617/8188 bytes&lt;BR /&gt;MX6Q SABRESD U-Boot &amp;gt; tftp uImage&lt;BR /&gt;FEC: Link is Up 796d&lt;BR /&gt;Using FEC0 device&lt;BR /&gt;TFTP from server 192.168.42.1; our IP address is 192.168.42.30&lt;BR /&gt;Filename 'uImage'.&lt;BR /&gt;Load address: 0x10800000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #################################################################&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #################################################################&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #################################################################&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ###&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 3851168 (3ac3a0 hex)&lt;BR /&gt;MX6Q SABRESD U-Boot &amp;gt; bootm&lt;BR /&gt;## Booting kernel from Legacy Image at 10800000 ...&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.0.35-2310-gc27cb38&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 3851104 Bytes =&amp;nbsp; 3.7 MB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;BR /&gt;OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Linux version 3.0.35-2310-gc27cb38 (makis@makis-virtual-machine) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #3 SMP PREEMPT Tue Jun 11 17:40:54 BST 2013&lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board&lt;BR /&gt;Ignoring unrecognised tag 0x54410008&lt;BR /&gt;Memory policy: ECC disabled, Data cache writealloc&lt;BR /&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;BR /&gt;PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 227328&lt;BR /&gt;Kernel command line: ip=192.168.42.30:192.168.42.1:0.0.0.0:255.255.255.0 console=ttymxc0,115200 root=nfs nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Memory: 640MB 256MB = 896MB total&lt;BR /&gt;Memory: 896880k/896880k available, 151696k reserved, 0K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xf4600000 - 0xffe00000&amp;nbsp;&amp;nbsp; ( 184 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xc0800000 - 0xf2000000&amp;nbsp;&amp;nbsp; ( 792 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (1024 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80008000 - 0x8003b000&amp;nbsp;&amp;nbsp; ( 204 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x8003b000 - 0x80a886d0&amp;nbsp;&amp;nbsp; (10550 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80a8a000 - 0x80ae8a40&amp;nbsp;&amp;nbsp; ( 379 kB)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80ae8a64 - 0x80b368ec&amp;nbsp;&amp;nbsp; ( 312 kB)&lt;BR /&gt;SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;NR_IRQS:496&lt;BR /&gt;MXC GPIO hardware&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;BR /&gt;arm_max_freq=2&lt;BR /&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200')&lt;BR /&gt;bootconsole [ttymxc0] enabled&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;BR /&gt;CPU1: Booted secondary processor&lt;BR /&gt;CPU2: Booted secondary processor&lt;BR /&gt;CPU3: Booted secondary processor&lt;BR /&gt;Brought up 4 CPUs&lt;BR /&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;BR /&gt;print_constraints: dummy:&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 700 mV fast normal&lt;BR /&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1150 mV fast normal&lt;BR /&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1200 mV fast normal&lt;BR /&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal&lt;BR /&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal&lt;BR /&gt;print_constraints: vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV fast normal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;&amp;lt;&amp;lt;&amp;lt;&amp;lt;&amp;lt;&amp;lt;&amp;lt;- Here is where it resets?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2009.08 (Apr 10 2013 - 18:58:57)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.2 at 792 MHz&lt;BR /&gt;Temperature:&amp;nbsp;&amp;nbsp; 44 C, calibration data 0x5ae50f7d&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 80000000Hz&lt;BR /&gt;cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 60000000Hz&lt;BR /&gt;ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 132000000Hz&lt;BR /&gt;axi clock&amp;nbsp;&amp;nbsp; : 264000000Hz&lt;BR /&gt;emi_slow clock: 29333333Hz&lt;BR /&gt;ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 528000000Hz&lt;BR /&gt;usdhc1 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc2 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc3 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc4 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 24000000Hz&lt;BR /&gt;Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]&lt;BR /&gt;Boot Device: SD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp;&amp;nbsp; 1 GB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Found PFUZE100! deviceid=10,revid=11&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; got MAC address from IIM: 00:04:9f:02:af:8b&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;MX6Q SABRESD U-Boot &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;===============================&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 16:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278511#M31569</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-06-13T16:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278512#M31570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer to your kernel comman:ip=192.168.42.30:192.168.42.1:0.0.0.0:255.255.255.0 console=ttymxc0,115200 root=nfs nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs&lt;/P&gt;&lt;P&gt; it seems doesn't correct, pls dont add ip address before the console.&lt;/P&gt;&lt;P&gt;I send to you my kernel command, hope helpful:&lt;/P&gt;&lt;P&gt;bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loaddaddr} ${kernel}; bootm&lt;/P&gt;&lt;P&gt;bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp video=mxcfb0:dev=ldb, LDB-XGA, if=RGB666 ldb=sin1 nfsroot=${serverip}:${nfsroot},v3,tcp&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 09:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278512#M31570</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2013-06-20T09:07:33Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278513#M31571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Cheers thanks. I tried to not use at all ip and it will die in the same way. The kernel resets well before it has time to use the ip information.&lt;/P&gt;&lt;P&gt;I did some debugging of the kernel and it seems that it dies when the following IOMUX_PAD is enabled:&lt;/P&gt;&lt;P&gt;#define _MX6Q_PAD_GPIO_1__WDOG2_WDOG_B&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IOMUX_PAD(0x05F4, 0x0224, 1, 0x0000, 0, 0)&lt;BR /&gt;Now looking at the schematics of my SabreSD board it appears that the GPIO_1 pin that implements the WDOG2 is connected to the PowerON pin which sort of explains why to board reboots. By removing this IOMUX_PAD entry from the pad list bellow:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static iomux_v3_cfg_t mx6q_sabresd_pads[] = {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* AUDMUX */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_CSI0_DAT4__AUDMUX_AUD3_TXC,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_CSI0_DAT5__AUDMUX_AUD3_TXD,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_CSI0_DAT6__AUDMUX_AUD3_TXFS,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_CSI0_DAT7__AUDMUX_AUD3_RXD,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* CAN1&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_KEY_ROW2__HDMI_TX_CEC_LINE,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* MX6Q_PAD_KEY_COL2__CAN1_TXCAN, */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_GPIO_1__WDOG2_WDOG_B,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*WDOG_B to reset pmic*/&amp;nbsp; &amp;lt;&amp;lt;--- removing or commenting out stops resetting the board&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_GPIO_2__GPIO_1_2,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* user defined red led */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6Q_PAD_GPIO_7__GPIO_1_7,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* NERR */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;............&lt;/P&gt;&lt;P&gt;The kernel will try to go further and it dies eventually again but from unrelated problem I suspect.&lt;/P&gt;&lt;P&gt;My question is if this finding is true why freescale will build kernel with default configuration that is not working out of the box? I also tried to download pre-build kernel binaries from here and they seem to die same way as the one I build.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 15:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278513#M31571</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-06-20T15:02:30Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278514#M31572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Makis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am seeing this same failure with a SabreSDB, but not on all boards. I'm hoping to narrow it down to specific board revisions. Can you please post what your SCH and 700 revision numbers are, and confirm that we are testing with the same kernel.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Details :&lt;/P&gt;&lt;P&gt;Using the kernel from the demo image L3.0.35_4.0.0_130424_images_MX6&lt;/P&gt;&lt;P&gt;md5sum : b9d2eccea53f0cac7d12dc1a09cfb0df&amp;nbsp; uImage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;board #1 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSDB SCH-27516 Rev C1, 700-27516 Rev A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SD boot (SW6 01000010), Slot SD3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result : full boot, no issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;board #2 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSDP SCH-27392 Rev C4, 700-27392 Rev B&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SB boot (SW6 01000010), Slot SD3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result: full boot, no issues&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;board #3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSDB SCH-27516 Rev C2, 700-27516 Rev A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SB boot (SW6 01000010), Slot SD3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result: boot reboots during print_constraints as you've shown&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; modified WDOG2 IOMUX setting allows board to continue boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Ben&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 17:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278514#M31572</guid>
      <dc:creator>foosechek</dc:creator>
      <dc:date>2013-06-21T17:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278515#M31573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ben,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Won't be able to check this one until tuesday (25 June) but will let you know.&lt;/P&gt;&lt;P&gt;It does look from what you saying that I have one of those boards though.(board3)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Makis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 20:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278515#M31573</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-06-21T20:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278516#M31574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ben,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the numbers:&lt;/P&gt;&lt;P&gt;SCH-27392 REV C3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 700-27392 REV B&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is similar to Board#2 appart of C3 which is C4 on the board you mentioned.&lt;/P&gt;&lt;P&gt;However, my board exhibits the problem whereas the one you mentioned is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the mean time I managed to fully boot linux from NFS with the modified code and modified configuration as follows:&lt;/P&gt;&lt;P&gt;U-Boot 2009.08 (Apr 10 2013 - 18:58:57)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.2 at 792 MHz&lt;BR /&gt;Temperature:&amp;nbsp;&amp;nbsp; 34 C, calibration data 0x5ae50f7d&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 80000000Hz&lt;BR /&gt;cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 60000000Hz&lt;BR /&gt;ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 132000000Hz&lt;BR /&gt;axi clock&amp;nbsp;&amp;nbsp; : 264000000Hz&lt;BR /&gt;emi_slow clock: 29333333Hz&lt;BR /&gt;ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 528000000Hz&lt;BR /&gt;usdhc1 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc2 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc3 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc4 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 24000000Hz&lt;BR /&gt;Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]&lt;BR /&gt;Boot Device: SD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp;&amp;nbsp; 1 GB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Found PFUZE100! deviceid=10,revid=11&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; got MAC address from IIM: 00:04:9f:02:af:8b&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;MX6Q SABRESD U-Boot &amp;gt; pri&lt;BR /&gt;baudrate=115200&lt;BR /&gt;loadaddr=0x10800000&lt;BR /&gt;rd_loadaddr=0x11000000&lt;BR /&gt;netdev=eth0&lt;BR /&gt;ethprime=FEC0&lt;BR /&gt;fastboot_dev=mmc3&lt;BR /&gt;splashimage=0x30000000&lt;BR /&gt;splashpos=m,m&lt;BR /&gt;lvds_num=1&lt;BR /&gt;ethact=FEC0&lt;BR /&gt;bootdelay=6&lt;BR /&gt;kernel=uImage&lt;BR /&gt;bootcmd=booti mmc2&lt;BR /&gt;gateawayip=0.0.0.0&lt;BR /&gt;filesize=3AE998&lt;BR /&gt;fileaddr=10800000&lt;BR /&gt;netmask=255.255.255.0&lt;BR /&gt;ipaddr=192.168.42.30&lt;BR /&gt;serverip=192.168.42.1&lt;BR /&gt;boot_base=console=ttymxc0,115200&lt;BR /&gt;base_roots=/home/makis/imx6/ltib/rootfs&lt;BR /&gt;base_nfs=root=/dev/nfs ip=192.168.42.30 nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs,v3,tcp&lt;BR /&gt;bootargs=console=ttymxc0,115200 root=/dev/nfs ip=192.168.42.30 nfsroot=192.168.42.1:/home/makis/imx6/ltib/rootfs,v3,tcp&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;stderr=serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then using:&lt;/P&gt;&lt;P&gt;tftp uImage&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;bootm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;got me to the free scale login screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As my board now seem to boot to linux, I assume is OK to use modified WDOG2 IOMUX setting to carry on with my work?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2013 16:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278516#M31574</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-06-25T16:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278517#M31575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you provide some details on how you set up the TFTP server. When I attempt to read the uImage across the network, the file is never found. It appears to be trying continuously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; run bootcmd_net&lt;/P&gt;&lt;P&gt;PHY indentify @ 0x7 = 0x00221621&lt;/P&gt;&lt;P&gt;FEC: Link is Up 796d&lt;/P&gt;&lt;P&gt;Using FEC0 device&lt;/P&gt;&lt;P&gt;TFTP from server 192.168.1.101; our IP address is 192.168.1.103&lt;/P&gt;&lt;P&gt;Filename 'uImage'.&lt;/P&gt;&lt;P&gt;Load address: 0x10800000&lt;/P&gt;&lt;P&gt;Loading: T T T T T T T T T T T T&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2013 22:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278517#M31575</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-07-10T22:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278518#M31576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use something like this on the host Ubuntu machine to set nfs and tftp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------&lt;/P&gt;&lt;P&gt;For NFS, Edit /etc/exports&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Courier New';"&gt;/home/&amp;lt;uid&amp;gt;/ltib/rootfs *(rw,no_root_squash)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="DefaultStyle"&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Courier New';"&gt;Install tftpd-hpa&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;CODE&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;sudo apt-get install tftpd-hpa&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;CODE&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Install &lt;/SPAN&gt;&lt;/CODE&gt;nfs-kernel-server&lt;CODE&gt; &lt;/CODE&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;CODE&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;sudo apt-get install &lt;/SPAN&gt;&lt;/CODE&gt;nfs-kernel-server&lt;/P&gt;&lt;P class="DefaultStyle"&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Courier New';"&gt;Then:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 0.0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Courier New';"&gt;Edit the file:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="DefaultStyle"&gt;&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;# /etc/default/tftpd-hpa&lt;BR /&gt; &lt;BR /&gt; TFTP_USERNAME="tftp"&lt;BR /&gt; TFTP_DIRECTORY="/tftpboot"&lt;BR /&gt; TFTP_ADDRESS="&lt;A href="http://0.0.0.0:69/"&gt;&lt;SPAN class="InternetLink"&gt;0.0.0.0:69&lt;/SPAN&gt;&lt;/A&gt;"&lt;BR /&gt; TFTP_OPTIONS="--secure"&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;Then run the services: (start_services.sh)&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;sudo service tftpd-hpa restart&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;sudo /etc/init.d/nfs-kernel-server restart&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;-----------------------------------------------------------------------&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;You can find numerous examples that show how to set up these.&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;In your case I woudl try to make sure your u-boot sees the server at all.&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;try to ping it&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;ping 192.168.1.101&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;It should say if it is alive or not. However I found this not alway reliable on sabre board.&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;In your case is possible that the tftp server is not started on the host, in which case it will try forever. Also make sure you put uImage in&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt; TFTP_DIRECTORY="/tftpboot"&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;However you can point the directory ro point to where ltib build uImage so you don't have to copy the uImage file to TFTP_DIRECTORY each time you build the kernel.&lt;/P&gt;&lt;P class="DefaultStyle" style="margin-bottom: 12pt;"&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 14:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278518#M31576</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-07-11T14:51:12Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278519#M31577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ben, can you please send me the schematics for SCH-27516 Rev C2, 700-27516 Rev A. We are seeing the same problem. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Aug 2013 05:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278519#M31577</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2013-08-11T05:39:34Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD Kernel Not booting from TFTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278520#M31578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If it helps you, I found the following behaviour.&lt;/P&gt;&lt;P&gt;Original problem was showing up when Linux kernel was booted using u-boot from the Android SD card labeled:&lt;/P&gt;&lt;P&gt;Android 13.4.1&lt;/P&gt;&lt;P&gt;110-77478 C&lt;/P&gt;&lt;P&gt;When I do "v" on uboot command line I get version: &lt;/P&gt;&lt;P class="MsoNormal" style="tab-stops: 361.5pt;"&gt;U-Boot 2009.08 (Apr 10 2013 - 18:58:57)&lt;/P&gt;&lt;P class="MsoNormal" style="tab-stops: 361.5pt;"&gt;I reprogrammed another SD card with the Linux Image from freescale site which has a different u-boot &lt;/P&gt;&lt;P&gt;When I do "v" on uboot command line I get version: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="MsoNormal" style="tab-stops: 361.5pt;"&gt;U-Boot 2009.08 (Apr 25 2013 - 01:17:52)&lt;/P&gt;&lt;P class="MsoNormal" style="tab-stops: 361.5pt;"&gt;Linux image will then boot without any issues. I am guessing that the PADs can be modified within u-boot causig the kernel to boot normally!&lt;/P&gt;&lt;P class="MsoNormal" style="tab-stops: 361.5pt;"&gt;Makis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2013 09:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-Kernel-Not-booting-from-TFTP/m-p/278520#M31578</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2013-08-12T09:53:39Z</dc:date>
    </item>
  </channel>
</rss>