<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Prototyping board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160068#M3138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the answer, even though I wonder almost between IMX53QSB (quick start board) and iWave Q7&lt;/P&gt;&lt;P&gt;as ignore if the QSB is enough to be used as is: just with the board and no additional connectors or adaptation to use it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Nov 2012 08:39:47 GMT</pubDate>
    <dc:creator>mouha</dc:creator>
    <dc:date>2012-11-02T08:39:47Z</dc:date>
    <item>
      <title>Prototyping board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160066#M3136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm a Linux embedded developer who already own some board like the mini2440, or TS7260.&lt;/P&gt;&lt;P&gt;I'm new here, and admit to be lost about the i.MX53 which seems to be great :&lt;/P&gt;&lt;P&gt;- what board do I need to easily go prototyping when I see the freescale devboard but also a iWave Q7 one : does it means that the Devboard is not enough to get connectors&amp;nbsp; (GPIO, Ethernet, Sata, etc) and to power it ? in other words : what advice to choose a protyping board ?&lt;/P&gt;&lt;P&gt;- according to the numerous document Linux&amp;nbsp; (not Android) is easily provided for this board but how far when I want to access to accelermoter ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DL&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2012 13:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160066#M3136</guid>
      <dc:creator>mouha</dc:creator>
      <dc:date>2012-10-31T13:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: Prototyping board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160067#M3137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have two reference designs based on i.mx53. One is i.mx53QSB, the other one is SABRE for tablets. And SABRE is discounted to $999 now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the comparison table of these two boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SABRE for tablets vs. QSB - Comparison.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38670iBE51EB33481B263A/image-size/large?v=v2&amp;amp;px=999" role="button" title="SABRE for tablets vs. QSB - Comparison.JPG" alt="SABRE for tablets vs. QSB - Comparison.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2012 02:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160067#M3137</guid>
      <dc:creator>hippo</dc:creator>
      <dc:date>2012-11-01T02:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: Prototyping board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160068#M3138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the answer, even though I wonder almost between IMX53QSB (quick start board) and iWave Q7&lt;/P&gt;&lt;P&gt;as ignore if the QSB is enough to be used as is: just with the board and no additional connectors or adaptation to use it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Nov 2012 08:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Prototyping-board/m-p/160068#M3138</guid>
      <dc:creator>mouha</dc:creator>
      <dc:date>2012-11-02T08:39:47Z</dc:date>
    </item>
  </channel>
</rss>