<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB Tethering PPPD in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Tethering-PPPD/m-p/277679#M31341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im not familiar with USB Tethering.&lt;/P&gt;&lt;P&gt;I have custom device which is connected to another by serial wire.&lt;/P&gt;&lt;P&gt;I would like if there any chances to improve stability, and performance of this connection, by replaicing it by USB tethering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my solution:&lt;/P&gt;&lt;P&gt;|1 DEVICE|&amp;lt;=&amp;gt;FTDI&amp;lt;=&amp;gt;SERIAL&amp;lt;=&amp;gt;FTDI&amp;lt;=&amp;gt;|2 DEVICE|&lt;/P&gt;&lt;P&gt;To my device this serial is connected thru FTDI.&lt;/P&gt;&lt;P&gt;I have USB port (/dev/ttyUSB_N for example) in my system which is responsible for this type of connection.&lt;/P&gt;&lt;P&gt;Im using PPPD and L2TP to make it possible to bridge this connection with normal ETH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have usb0 interface in my system.&lt;/P&gt;&lt;P&gt;Is it possible to tell usb0 to use /dev/ttyUSB_N ?&lt;/P&gt;&lt;P&gt;usb0 is able to use bridge without PPPD and L2TP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Toxic &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Dec 2013 12:54:27 GMT</pubDate>
    <dc:creator>ToxicAvenger</dc:creator>
    <dc:date>2013-12-24T12:54:27Z</dc:date>
    <item>
      <title>USB Tethering PPPD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Tethering-PPPD/m-p/277679#M31341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im not familiar with USB Tethering.&lt;/P&gt;&lt;P&gt;I have custom device which is connected to another by serial wire.&lt;/P&gt;&lt;P&gt;I would like if there any chances to improve stability, and performance of this connection, by replaicing it by USB tethering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my solution:&lt;/P&gt;&lt;P&gt;|1 DEVICE|&amp;lt;=&amp;gt;FTDI&amp;lt;=&amp;gt;SERIAL&amp;lt;=&amp;gt;FTDI&amp;lt;=&amp;gt;|2 DEVICE|&lt;/P&gt;&lt;P&gt;To my device this serial is connected thru FTDI.&lt;/P&gt;&lt;P&gt;I have USB port (/dev/ttyUSB_N for example) in my system which is responsible for this type of connection.&lt;/P&gt;&lt;P&gt;Im using PPPD and L2TP to make it possible to bridge this connection with normal ETH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have usb0 interface in my system.&lt;/P&gt;&lt;P&gt;Is it possible to tell usb0 to use /dev/ttyUSB_N ?&lt;/P&gt;&lt;P&gt;usb0 is able to use bridge without PPPD and L2TP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Toxic &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 12:54:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Tethering-PPPD/m-p/277679#M31341</guid>
      <dc:creator>ToxicAvenger</dc:creator>
      <dc:date>2013-12-24T12:54:27Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tethering PPPD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Tethering-PPPD/m-p/277680#M31342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What progress have you made on this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suspect that you should connect to the FTDI site and view their software/drivers/samples there is a wealth of info regarding serial communication via a USB-to-serial adapter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I myself have been working on a similar problem.&amp;nbsp; I am running Android R10.4 (Android 2.3.7) and trying to get serial over USB working (via an FTDI USB-to-serial adapter).&amp;nbsp; So far it appears FTDI has many pieces but they primarily target Android 3.1/3.2 and above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you're running Android perhaps we are working down a similar path...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 15:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Tethering-PPPD/m-p/277680#M31342</guid>
      <dc:creator>mbp</dc:creator>
      <dc:date>2014-02-06T15:17:44Z</dc:date>
    </item>
  </channel>
</rss>