<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Video fast update on iMX53</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277508#M31251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to create an application, using gstreamer/gobject/glib libraries. A pipeline is actually an object where you can attach to it a bus (another object); in turn, it has a switch statement all you need to specify which messages you are listening to.... About the message/event/signal types, I do not know, but this is the gstreamer way to communicate between application-pipeline (alias elements), there is no other way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Aug 2013 18:39:32 GMT</pubDate>
    <dc:creator>LeonardoSandova</dc:creator>
    <dc:date>2013-08-28T18:39:32Z</dc:date>
    <item>
      <title>Video fast update on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277504#M31247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are actually two parts to this question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can the application be informed of a decoding error in mfw_vpudecoder?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And much more importantly, how to force mfw_vpuencoder to immediately send a new key frame (aka Intra-frame) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Background:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When transmitting video over an Internet connection, packets get lost. If this happens the decoder fails and you can get artefacts in the picture. This remains until the next key frame refreshes the whole picture, which can be many seconds. To speed this up protocols such as SIP/H.323 have a fast update mechanism, but this requires that we can force the decoder to send a new key frame. This clears up the corrupted picture as soon as possible, improving the user experience.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2013 13:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277504#M31247</guid>
      <dc:creator>rjongbloed</dc:creator>
      <dc:date>2013-08-27T13:42:10Z</dc:date>
    </item>
    <item>
      <title>Re: Video fast update on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277505#M31248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert, this is what I think you can do:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. You need a BUS (&lt;A href="http://gstreamer.freedesktop.org/data/doc/gstreamer/head/manual/html/chapter-bus.html" title="http://gstreamer.freedesktop.org/data/doc/gstreamer/head/manual/html/chapter-bus.html"&gt;Chapter 7. Bus&lt;/A&gt;), this way the element can communicate messages to an app. In resume, Read the GStreamer Application &lt;A href="http://gstreamer.freedesktop.org/data/doc/gstreamer/head/manual/manual.pdf"&gt;Manual&lt;/A&gt; :smileyhappy:&lt;/P&gt;&lt;P&gt;2. For this feature, You may need to send an event to the pipeline, and this one has to be attended by the decoder, which in turn you can send the new key frame.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/DaianeAngolini"&gt;DaianeAngolini&lt;/A&gt;, do you think the key frame can be injected the way Robert mentioned?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2013 14:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277505#M31248</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-08-27T14:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: Video fast update on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277506#M31249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a pipeline, I have a bus on that pipeline.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, what's the message to be sent?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the event I should receive?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-inpect of the modules do not have any events indicated, which is worrying.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 00:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277506#M31249</guid>
      <dc:creator>rjongbloed</dc:creator>
      <dc:date>2013-08-28T00:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: Video fast update on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277507#M31250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo, I don´t think it is implemented on the current source code, but I believe it may be implemented....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 16:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277507#M31250</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2013-08-28T16:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: Video fast update on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277508#M31251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to create an application, using gstreamer/gobject/glib libraries. A pipeline is actually an object where you can attach to it a bus (another object); in turn, it has a switch statement all you need to specify which messages you are listening to.... About the message/event/signal types, I do not know, but this is the gstreamer way to communicate between application-pipeline (alias elements), there is no other way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 18:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-fast-update-on-iMX53/m-p/277508#M31251</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-08-28T18:39:32Z</dc:date>
    </item>
  </channel>
</rss>