<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX536 NVCC_SRTC Abnormal</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX536-NVCC-SRTC-Abnormal/m-p/277368#M31184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check the following signals in your schematic:&lt;/P&gt;&lt;P&gt;CKIL, ECKIL, PMIC_ON_REQ, PMIC_STBY_REQ.&lt;/P&gt;&lt;P&gt;These signals also use NVCC_SRTC_POW as power source.&lt;/P&gt;&lt;P&gt;Probably, you had one of these signals connected to IC that uses 1.8V level,&lt;/P&gt;&lt;P&gt;and it got leaked to NVCC_SRTC_POW pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Oct 2013 01:53:48 GMT</pubDate>
    <dc:creator>DonnyChiu</dc:creator>
    <dc:date>2013-10-18T01:53:48Z</dc:date>
    <item>
      <title>iMX536 NVCC_SRTC Abnormal</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX536-NVCC-SRTC-Abnormal/m-p/277367#M31183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hello，I come here for your help！&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is like this： Use LTC3589-1 as a PMIC For iMX536, connet LDO1 to NVCC_SRTC_1V3. When not Powrn ON, the LDO1 out is 1.3V,after power on,LDO1 changes to 1.8V.when I Cut off the connectiong between NVCC_SRTC_1V3 and LTC3589-1's LDO1,NVCC_SRTC_1V3's voltage is 1.8V,and LDO1's voltage is 1.3V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is there something settings wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PS: LDO power input VDD_REG is measured as 2.5V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2013 07:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX536-NVCC-SRTC-Abnormal/m-p/277367#M31183</guid>
      <dc:creator>xiaobingtang</dc:creator>
      <dc:date>2013-10-14T07:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX536 NVCC_SRTC Abnormal</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX536-NVCC-SRTC-Abnormal/m-p/277368#M31184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check the following signals in your schematic:&lt;/P&gt;&lt;P&gt;CKIL, ECKIL, PMIC_ON_REQ, PMIC_STBY_REQ.&lt;/P&gt;&lt;P&gt;These signals also use NVCC_SRTC_POW as power source.&lt;/P&gt;&lt;P&gt;Probably, you had one of these signals connected to IC that uses 1.8V level,&lt;/P&gt;&lt;P&gt;and it got leaked to NVCC_SRTC_POW pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2013 01:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX536-NVCC-SRTC-Abnormal/m-p/277368#M31184</guid>
      <dc:creator>DonnyChiu</dc:creator>
      <dc:date>2013-10-18T01:53:48Z</dc:date>
    </item>
  </channel>
</rss>