<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx50 ecspi ss_ctl control</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277240#M31155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Michael, if Peter's answer is good, please click Correct Answer.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Mar 2013 03:56:43 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2013-03-25T03:56:43Z</dc:date>
    <item>
      <title>imx50 ecspi ss_ctl control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277238#M31153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an IMX50 EVK that I am trying to connect to a spi device. Our implementation requires the ss_ctl line to be active low during the entire 2 bytes transmit transaction. I have configured ecspi2 to be the master device and I am using the provided mxc_spi.c delivered with the MCIMX50EVK dev D board. I configured spidev2.0 to be my particular user space spi driver. I am attempting to send 2 bytes (0x5511) out the escpi2 device. Using an oscilloscope I can see the 2 data bytes and the associated clock. The slave select line goes low during the time each byte is transmitted. However, in between each byte the slave select line transitions high. I need this to remain low until the 2 bytes have been transmitted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I am reading setting bit 8 in ECSPIx_CONFIGREG and configuring ECSPIx_PERIODREG to 0 should produce a slave select waveform such that the slave select line remains low during idle byte periods. What am I missing here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2013 00:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277238#M31153</guid>
      <dc:creator>michaelcarrier</dc:creator>
      <dc:date>2013-02-28T00:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: imx50 ecspi ss_ctl control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277239#M31154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From i.MX50 reference manual 22.3.5.1.3, ECSPIx_CONFIGREG bit 8 should be clear (SS_CTL[0] is clear) for no SS negate between the SPI bursts. ECSPIx_CONREG:SMC must be 1 when using ECSPIx_CONFIGREG:SS_CTL to control the SS waveform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, you can set the ECSPIx_CONREG:BURST LENGTH=0x1F for 16 bit SPI burst and write 16-bit data to lower nibble of ECSPIx_TXDATA.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2013 09:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277239#M31154</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2013-03-20T09:58:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx50 ecspi ss_ctl control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277240#M31155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Michael, if Peter's answer is good, please click Correct Answer.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2013 03:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx50-ecspi-ss-ctl-control/m-p/277240#M31155</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-03-25T03:56:43Z</dc:date>
    </item>
  </channel>
</rss>