<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6: Debug UART at ROM level?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276737#M31014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jun 2013 08:02:49 GMT</pubDate>
    <dc:creator>EgleTeam</dc:creator>
    <dc:date>2013-06-06T08:02:49Z</dc:date>
    <item>
      <title>iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276733#M31010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do any of&amp;nbsp; iMX6 UART ports is configured by default for debugging while ROM code is executed?. I mean: something like in other families (i.e: iMX28) where one of the UARTs can send&amp;nbsp; ROM error codes before loading uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not: Is there any alternative way for debugging before loading uboot?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 18:36:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276733#M31010</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2013-06-05T18:36:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276734#M31011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I.MX6 boot ROM supports only USB as serial bootloader, UART is not supported as for other i.MX parts.&lt;/P&gt;&lt;P&gt;(I mean boot_mode = 01 Serial Downloader). Next, only i.MX28 / 23 provide boot ROM messages&lt;BR /&gt;to the Debug UART. This feature does not take place for the other i.MX devices.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 05:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276734#M31011</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-06-06T05:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276735#M31012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so... with the boot pins configured for "internal boot mode", USB-OTG cable connected to a PC and mfgtool running:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. If nothing happens: there's something fundamentally wrong on the SoC and/or supply rails.&lt;/P&gt;&lt;P&gt;2. If the Soc connects to the mfgtool: ROM can't boot from selected device by the GPIOs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please correct me if the above approach is wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We look for a quick way to know the reason if our custom board (finishing the design) doesn't boot the OS at the first attempt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 07:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276735#M31012</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2013-06-06T07:11:38Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276736#M31013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just as a&amp;nbsp; test, if a (Windows) USB insertion activity occurs (somewhat as new device found), &lt;BR /&gt;when i.MX6 board is connected. If - yes - this good sign, we can hope to run the MFG.&lt;BR /&gt;If - no, system cannot start, try standard bring up procedure.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 07:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276736#M31013</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-06-06T07:41:11Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276737#M31014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 08:02:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276737#M31014</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2013-06-06T08:02:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276738#M31015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;finally we have our hardware fabricated with iMX6 DualLite installed. Unfortunately we can't bring up the boards. Windows can see an USB device connected but can't get VID &amp;amp; PID. Clock and all power domains are OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, we have tried to boot Android and Ubuntu prebuilt images on a SD port. We can see how Windows don't see the USB OTG port when a valid SD card is inserted, as well as we can see activity on the CLK line with a scope as well as different power consumption in Ubuntu and Android: what make us think that the iMX6 begins to read uboot but fails in some point. Unfortunately we can't see anything on the UART port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does uboot begin to send messages over the debug UART port all along or first checks any critical hardware (i.e.: DDR3)? What do you recommend us in order to find what is going wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2013 14:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276738#M31015</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2013-08-06T14:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6: Debug UART at ROM level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276739#M31016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our mistake: we were testing with Android &amp;amp; Ubuntu images for Quad core. The uboot image for DL boots right. SOLVED.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB OTG still being not recognized when there's no another boot device but this is not important right now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2013 18:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Debug-UART-at-ROM-level/m-p/276739#M31016</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2013-08-06T18:08:40Z</dc:date>
    </item>
  </channel>
</rss>