<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCombining keypad and touchscreen functions in DirectFB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Combining-keypad-and-touchscreen-functions-in-DirectFB/m-p/159889#M3079</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class="lia-message-body lia-component-body"&gt;&lt;DIV class="lia-message-body-content"&gt;&lt;P&gt;Hiya,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to run an i.MX233 EVK application interfaces to DirectFB using both the LCD touchpanel as well as the eight buttons that are included on the EVK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't been successful finding example code that brings in the touch panel (DirectFB&amp;nbsp; was built with the ltib touchscreen option selected) so I decided to go a more basic route and read the touchscreen using the traditional ts functions.&amp;nbsp; This seems to supersede the (LRADC based) keyboard read,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody have some sample i.MX233 DirectFB code that I could take a look at that accesses the touchpanel so I don't have to include the ts functions and I can run with both the touchscreen and the buttons?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jun 2011 20:10:49 GMT</pubDate>
    <dc:creator>myke_predko</dc:creator>
    <dc:date>2011-06-28T20:10:49Z</dc:date>
    <item>
      <title>Combining keypad and touchscreen functions in DirectFB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Combining-keypad-and-touchscreen-functions-in-DirectFB/m-p/159889#M3079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class="lia-message-body lia-component-body"&gt;&lt;DIV class="lia-message-body-content"&gt;&lt;P&gt;Hiya,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to run an i.MX233 EVK application interfaces to DirectFB using both the LCD touchpanel as well as the eight buttons that are included on the EVK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't been successful finding example code that brings in the touch panel (DirectFB&amp;nbsp; was built with the ltib touchscreen option selected) so I decided to go a more basic route and read the touchscreen using the traditional ts functions.&amp;nbsp; This seems to supersede the (LRADC based) keyboard read,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody have some sample i.MX233 DirectFB code that I could take a look at that accesses the touchpanel so I don't have to include the ts functions and I can run with both the touchscreen and the buttons?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2011 20:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Combining-keypad-and-touchscreen-functions-in-DirectFB/m-p/159889#M3079</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2011-06-28T20:10:49Z</dc:date>
    </item>
  </channel>
</rss>