<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Fingerprint property missing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Fingerprint-property-missing/m-p/275954#M30742</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I discovered that my fingerprint value was exceeding the maximum length of a property (defined to be PROPERTY_VALUE_MAX 92 in system/core/include/cutils/properties.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Robbeloth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Aug 2013 17:56:05 GMT</pubDate>
    <dc:creator>michaelrobbelot</dc:creator>
    <dc:date>2013-08-26T17:56:05Z</dc:date>
    <item>
      <title>Fingerprint property missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fingerprint-property-missing/m-p/275953#M30741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if anyone might know why ro.build.fingerprint would not show in an android build. I can clearly see that it is getting generated and is included in out/product/.../system/build.prop, but does not show up on the running build when you issue the getprop command or run the appropriate CTS test that looks for ro.build.fingerprint. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Robbeloth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2013 16:37:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fingerprint-property-missing/m-p/275953#M30741</guid>
      <dc:creator>michaelrobbelot</dc:creator>
      <dc:date>2013-08-26T16:37:56Z</dc:date>
    </item>
    <item>
      <title>Re: Fingerprint property missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fingerprint-property-missing/m-p/275954#M30742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I discovered that my fingerprint value was exceeding the maximum length of a property (defined to be PROPERTY_VALUE_MAX 92 in system/core/include/cutils/properties.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Robbeloth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2013 17:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fingerprint-property-missing/m-p/275954#M30742</guid>
      <dc:creator>michaelrobbelot</dc:creator>
      <dc:date>2013-08-26T17:56:05Z</dc:date>
    </item>
  </channel>
</rss>