<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic sgtl5000 in MX6q board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/sgtl5000-in-MX6q-board/m-p/275693#M30613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;config:&lt;/P&gt;&lt;P&gt;static struct mxc_audio_platform_data mx6_sabrelite_audio_data = {&lt;/P&gt;&lt;P&gt;&amp;nbsp; .ssi_num = 1,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .src_port = 2,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .ext_port = 5,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .init = mx6_sabrelite_sgtl5000_init,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .hp_gpio = -1,&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I input the :&lt;STRONG&gt;aplay test.wav&lt;/STRONG&gt; command in terminal&lt;/P&gt;&lt;P&gt;But no any sound i can heard it So i check the sgtl5000 GPIO .The power 、I2c 、clock is ok. because i can see the right wave in the Oscilloscope ！&lt;/P&gt;&lt;P&gt;But i can not see any wave in the I2S GPIO, The I2S RXD GPIO Voltage is high ,the I2S TXD GPIO Voltage is LOW !&lt;/P&gt;&lt;P&gt;Why ? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Oct 2013 14:57:15 GMT</pubDate>
    <dc:creator>xmphoenix</dc:creator>
    <dc:date>2013-10-11T14:57:15Z</dc:date>
    <item>
      <title>sgtl5000 in MX6q board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sgtl5000-in-MX6q-board/m-p/275693#M30613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;config:&lt;/P&gt;&lt;P&gt;static struct mxc_audio_platform_data mx6_sabrelite_audio_data = {&lt;/P&gt;&lt;P&gt;&amp;nbsp; .ssi_num = 1,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .src_port = 2,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .ext_port = 5,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .init = mx6_sabrelite_sgtl5000_init,&lt;/P&gt;&lt;P&gt;&amp;nbsp; .hp_gpio = -1,&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I input the :&lt;STRONG&gt;aplay test.wav&lt;/STRONG&gt; command in terminal&lt;/P&gt;&lt;P&gt;But no any sound i can heard it So i check the sgtl5000 GPIO .The power 、I2c 、clock is ok. because i can see the right wave in the Oscilloscope ！&lt;/P&gt;&lt;P&gt;But i can not see any wave in the I2S GPIO, The I2S RXD GPIO Voltage is high ,the I2S TXD GPIO Voltage is LOW !&lt;/P&gt;&lt;P&gt;Why ? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2013 14:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sgtl5000-in-MX6q-board/m-p/275693#M30613</guid>
      <dc:creator>xmphoenix</dc:creator>
      <dc:date>2013-10-11T14:57:15Z</dc:date>
    </item>
    <item>
      <title>Re: sgtl5000 in MX6q board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sgtl5000-in-MX6q-board/m-p/275694#M30614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think this may helpful for your problem. &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/322387"&gt;Re: SGTL5000 Audio CODEC and i.MX6Q&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2013 02:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sgtl5000-in-MX6q-board/m-p/275694#M30614</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-10-18T02:40:50Z</dc:date>
    </item>
  </channel>
</rss>