<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Using the CSI inputs on IMX6DQCEC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275640#M30591</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are 3 kinds of camera interface:&lt;/P&gt;&lt;P&gt;(1)CS0 port (parallel interface)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119460i60E6B4932952C293/image-size/large?v=v2&amp;amp;px=999" title="CSI0.png" alt="CSI0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(2)CS1 port (parallel interface)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119461i54629B788D23FA6C/image-size/large?v=v2&amp;amp;px=999" title="CSI1.png" alt="CSI1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(3)MIPI port (serial interface)&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119462i76F18D3770FFF8C5/image-size/large?v=v2&amp;amp;px=999" title="MIPI.png" alt="MIPI.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In addition, DSI port is display output . Not camera signal input .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jun 2013 13:23:15 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2013-06-05T13:23:15Z</dc:date>
    <item>
      <title>Using the CSI inputs on IMX6DQCEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275639#M30590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to drive the CSI inputs from a DSI (Display Serial Interface: in effect, serialized BT.565) signal source, but from what I can see, the serial camera inputs only accept proprietary signal standards such as MIPI. Will DSI work, or alternatively, are there any other public serial data standards which CSI can accept?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards &amp;amp; TIA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 09:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275639#M30590</guid>
      <dc:creator>davidbrooks</dc:creator>
      <dc:date>2013-06-05T09:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: Using the CSI inputs on IMX6DQCEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275640#M30591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are 3 kinds of camera interface:&lt;/P&gt;&lt;P&gt;(1)CS0 port (parallel interface)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119460i60E6B4932952C293/image-size/large?v=v2&amp;amp;px=999" title="CSI0.png" alt="CSI0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(2)CS1 port (parallel interface)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119461i54629B788D23FA6C/image-size/large?v=v2&amp;amp;px=999" title="CSI1.png" alt="CSI1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(3)MIPI port (serial interface)&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119462i76F18D3770FFF8C5/image-size/large?v=v2&amp;amp;px=999" title="MIPI.png" alt="MIPI.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In addition, DSI port is display output . Not camera signal input .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 13:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275640#M30591</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-06-05T13:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: Using the CSI inputs on IMX6DQCEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275641#M30592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many thanks, Weidong.&lt;/P&gt;&lt;P&gt;Those picture make it all clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jun 2013 00:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-CSI-inputs-on-IMX6DQCEC/m-p/275641#M30592</guid>
      <dc:creator>davidbrooks</dc:creator>
      <dc:date>2013-06-08T00:16:35Z</dc:date>
    </item>
  </channel>
</rss>