<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 PCIe WiFi for iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-WiFi-for-iMX6/m-p/275127#M30450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a reference of PCIe WiFi card that is known to work with iMX6Q on the SABRE-SD board?&lt;/P&gt;&lt;P&gt;Would you know if the required BSP porting efforts are high for that module based on the FSL BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A customer is looking for higher throughput on the WiFi connection than the actual used solution over SDIO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Aug 2013 11:04:50 GMT</pubDate>
    <dc:creator>bfac</dc:creator>
    <dc:date>2013-08-26T11:04:50Z</dc:date>
    <item>
      <title>PCIe WiFi for iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-WiFi-for-iMX6/m-p/275127#M30450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a reference of PCIe WiFi card that is known to work with iMX6Q on the SABRE-SD board?&lt;/P&gt;&lt;P&gt;Would you know if the required BSP porting efforts are high for that module based on the FSL BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A customer is looking for higher throughput on the WiFi connection than the actual used solution over SDIO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2013 11:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-WiFi-for-iMX6/m-p/275127#M30450</guid>
      <dc:creator>bfac</dc:creator>
      <dc:date>2013-08-26T11:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe WiFi for iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-WiFi-for-iMX6/m-p/275128#M30451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use intel &lt;SPAN style="font-size: 14.0pt; font-family: 'Calibri','sans-serif'; color: #1f497d;"&gt;iwl4965&lt;/SPAN&gt;. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use above wifi card, needn't port. Kernel already supported it.&lt;/P&gt;&lt;P&gt;If you use other wifi card, need thirdpart provide wifi card driver. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Frank Li&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2013 01:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-WiFi-for-iMX6/m-p/275128#M30451</guid>
      <dc:creator>FrankLi1z</dc:creator>
      <dc:date>2013-08-29T01:51:52Z</dc:date>
    </item>
  </channel>
</rss>