<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: shell tool to write flash via ROM bootloader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275094#M30434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not aware of any shell-tool like what you are looking for. Only the MFG tool but is GUI based.&lt;/P&gt;&lt;P&gt;One think that comes to my mind is fastboot (like in Android devices) but that imply that you have an auxiliar u-boot in place&amp;nbsp; (like booting from SD) that puts the device in fastboot mode, then you can start flashing the device using fastboot tool. But that implies some significant effort in the u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jun 2013 15:04:55 GMT</pubDate>
    <dc:creator>juangutierrez</dc:creator>
    <dc:date>2013-06-19T15:04:55Z</dc:date>
    <item>
      <title>shell tool to write flash via ROM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275093#M30433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;We developed a product employing a NAND flash as boot code device.&lt;/P&gt;&lt;P&gt;We need to program it on production line, using the ROM bootloader and USB connection to a PC with windows.&lt;/P&gt;&lt;P&gt;We are already using ATK to program the boards during the debug stages, but it works only in GUI mode,&lt;/P&gt;&lt;P&gt;while we need something that can be easily integrated on the production line, and doesn't require the intervention of the operator.&lt;/P&gt;&lt;P&gt;Basically we need a tool that can be launched from shell, passing all relevant parameters as options.&lt;/P&gt;&lt;P&gt;Is there somewhere a tool like this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Andrea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 08:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275093#M30433</guid>
      <dc:creator>andpas</dc:creator>
      <dc:date>2013-06-05T08:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: shell tool to write flash via ROM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275094#M30434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not aware of any shell-tool like what you are looking for. Only the MFG tool but is GUI based.&lt;/P&gt;&lt;P&gt;One think that comes to my mind is fastboot (like in Android devices) but that imply that you have an auxiliar u-boot in place&amp;nbsp; (like booting from SD) that puts the device in fastboot mode, then you can start flashing the device using fastboot tool. But that implies some significant effort in the u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2013 15:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275094#M30434</guid>
      <dc:creator>juangutierrez</dc:creator>
      <dc:date>2013-06-19T15:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: shell tool to write flash via ROM bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275095#M30435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Andrea, please click Correct Answe/Helpful Answer if your question had been answered.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 06:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/shell-tool-to-write-flash-via-ROM-bootloader/m-p/275095#M30435</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-06-21T06:23:50Z</dc:date>
    </item>
  </channel>
</rss>