<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX28 splash screen uboot/linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274954#M30388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fabio,&lt;/P&gt;&lt;P&gt;thanks for your answer. Unfortunately I must initialize my display via SPI as it has different interface modes (and RGB ist not standard). I'm afraid I need a modified uboot or do you have an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Nov 2013 15:55:12 GMT</pubDate>
    <dc:creator>michaelkoelbl</dc:creator>
    <dc:date>2013-11-13T15:55:12Z</dc:date>
    <item>
      <title>iMX28 splash screen uboot/linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274951#M30385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to add a splash screen. There are some threads but they have other software (WinCE). Afaik Uboot should allow a splash screen. Can anyone give me instructions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2013 09:57:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274951#M30385</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2013-11-13T09:57:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 splash screen uboot/linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274952#M30386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Mike&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I used to develop lcdif splash screen feature on WinCE several years ago, I think you can try to download the wince release of i.MX28 EVK board, the eboot should already support this feature, you can refer to wince code, the steps should be as below:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. load a picture to DRAM;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. Initialize lcdif's hardware, IOMUX, clock and working mode;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3. Call lcdif interface to display the picture in DRAM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2013 10:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274952#M30386</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-11-13T10:13:04Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 splash screen uboot/linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274953#M30387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Splash screen in U-boot 2013.10 is supported for mx28evk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After you boot this version, then set the videomode variable:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setenv videomode video=ctfb:x:800,y:480,depth:24,mode:0,pclk:29851,le:89,ri:164,up:23,lo:10,hs:10,vs:10,sync:0,vmode:0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reboot the board, and then you will see the U-boot logo in the LCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2013 11:48:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274953#M30387</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-11-13T11:48:10Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 splash screen uboot/linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274954#M30388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fabio,&lt;/P&gt;&lt;P&gt;thanks for your answer. Unfortunately I must initialize my display via SPI as it has different interface modes (and RGB ist not standard). I'm afraid I need a modified uboot or do you have an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2013 15:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274954#M30388</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2013-11-13T15:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 splash screen uboot/linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274955#M30389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case you need to write a driver in U-boot for your SPI controlled display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2013 16:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-splash-screen-uboot-linux/m-p/274955#M30389</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-11-13T16:32:46Z</dc:date>
    </item>
  </channel>
</rss>