<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTOUCH Screen coordinate Jitter .CRAZY!!!!!</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TOUCH-Screen-coordinate-Jitter-CRAZY/m-p/274726#M30295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we used the i.MX536&amp;amp;DA9053 design a hand-in meter.it has an 5.6" LCD SCREEN combine with a touch screen .we use the DA9053 touch screen interface.&lt;/P&gt;&lt;P&gt;in the HIM. a visual keyboard exist. but when we use finger touch the visual keyboard frame.it keep jitter and never-ending. in the SCH ,the touch screen path is very short.we use 4-cap on the X+,X-,Y+,Y- to filtering the jitter. but has no effect.evreyone,have u used have this problem? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jun 2013 03:16:31 GMT</pubDate>
    <dc:creator>peigao</dc:creator>
    <dc:date>2013-06-05T03:16:31Z</dc:date>
    <item>
      <title>TOUCH Screen coordinate Jitter .CRAZY!!!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TOUCH-Screen-coordinate-Jitter-CRAZY/m-p/274726#M30295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we used the i.MX536&amp;amp;DA9053 design a hand-in meter.it has an 5.6" LCD SCREEN combine with a touch screen .we use the DA9053 touch screen interface.&lt;/P&gt;&lt;P&gt;in the HIM. a visual keyboard exist. but when we use finger touch the visual keyboard frame.it keep jitter and never-ending. in the SCH ,the touch screen path is very short.we use 4-cap on the X+,X-,Y+,Y- to filtering the jitter. but has no effect.evreyone,have u used have this problem? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 03:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TOUCH-Screen-coordinate-Jitter-CRAZY/m-p/274726#M30295</guid>
      <dc:creator>peigao</dc:creator>
      <dc:date>2013-06-05T03:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: TOUCH Screen coordinate Jitter .CRAZY!!!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TOUCH-Screen-coordinate-Jitter-CRAZY/m-p/274727#M30296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;1. please add the tslib package in the Package List in LTIB Configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;2. please try to delete the pointercal file and do the calibration again. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Before run the ts_calibrate, please try to "export" the followings:&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_ROOT=/usr&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_TSDEVICE=/dev/input/event2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (please change it if your touchscreen device node is different)&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_CALIBFILE=/etc/pointercal&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_CONFFILE=$TSLIB_ROOT/etc/ts.conf&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_PLUGINDIR=$TSLIB_ROOT/lib/ts&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_CONSOLEDEVICE=none&lt;/P&gt;&lt;P&gt;&amp;nbsp; export TSLIB_FBDEVICE=/dev/fb0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The existing /etc/ts.conf should look like this.&lt;/P&gt;&lt;P&gt;&amp;nbsp; module_raw input&lt;/P&gt;&lt;P&gt;&amp;nbsp; module pthres pmin=1&lt;/P&gt;&lt;P&gt;&amp;nbsp; module variance delta=30&lt;/P&gt;&lt;P&gt;&amp;nbsp; module dejitter delta=100&lt;/P&gt;&lt;P&gt;&amp;nbsp; module linear&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;3. If the GUI is Ubuntu, please read the i.MX5x_EVK_Ubuntu_9.10_StartupGuide.pdf or i.MX5x_EVK_Ubuntu_10.04_StartupGuide.pdf&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;4. you can try to use the evtest to check the touchscreen input.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 07:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TOUCH-Screen-coordinate-Jitter-CRAZY/m-p/274727#M30296</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-06-05T07:17:03Z</dc:date>
    </item>
  </channel>
</rss>