<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: PMIC MC34708 not coming up?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274601#M30217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Satyan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The issue is not related to load . mc34708 is designed for single li-cell battery with standard 3.7V input, So for a single li-cell battery, it is MAX voltage is 4.2V, if you use 3.3V to be input of BATT pin on mc34708, It is really too low. We ofter use a 5v--&amp;gt;3.8v DC-DC power IC to be input of MC34708, this DC-DC is just like a signle li-cell battery !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jul 2013 14:14:32 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2013-07-30T14:14:32Z</dc:date>
    <item>
      <title>PMIC MC34708 not coming up?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274598#M30214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using PMIC MC34708 in one of the iMx537 design. The PMIC chip is not coming up. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am giving 3.3V as the BP input. The reference voltages are coming correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help in this regard is greatly appreciated. Thanks in advance. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 11:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274598#M30214</guid>
      <dc:creator>ss12</dc:creator>
      <dc:date>2013-07-16T11:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC MC34708 not coming up?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274599#M30215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Satyan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have 2 suggestions about your design :&lt;/P&gt;&lt;P&gt;(1) BP Voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.3V is too low. BP pin is for single battery input , It's normal input voltage should be 3.5~4.2V.&lt;/P&gt;&lt;P&gt;(2)WDI pin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if MC34708 doesn't work, please measure WDI pin to check if this pin is High . If the level is low, MC34708 doesn't work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 03:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274599#M30215</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-07-18T03:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC MC34708 not coming up?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274600#M30216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your reply. The said design is part of the bigger system and this is a module in it and has input power that is 3.3V only. I do not have any option to increase the voltage. &lt;STRONG&gt;Is there any other alternative chip available. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; WDI pin is showing low only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have isolated all the loads from the chip completely to check if it was overloading. Now if I give 3.6V from an external source it tries to come up and goes down immediately.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is the load necessary for the PMIC to come up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with best regards,&lt;/P&gt;&lt;P&gt;S.Satyan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 09:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274600#M30216</guid>
      <dc:creator>ss12</dc:creator>
      <dc:date>2013-07-19T09:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC MC34708 not coming up?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274601#M30217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Satyan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The issue is not related to load . mc34708 is designed for single li-cell battery with standard 3.7V input, So for a single li-cell battery, it is MAX voltage is 4.2V, if you use 3.3V to be input of BATT pin on mc34708, It is really too low. We ofter use a 5v--&amp;gt;3.8v DC-DC power IC to be input of MC34708, this DC-DC is just like a signle li-cell battery !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jul 2013 14:14:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274601#M30217</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-07-30T14:14:32Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC MC34708 not coming up?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274602#M30218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your reply. The chip is coming up now. I pulled the WDI to high. All the voltages are coming up even at 3.3V. :smileyhappy: Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with best regards,&lt;/P&gt;&lt;P&gt;S.Satyan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2013 09:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274602#M30218</guid>
      <dc:creator>ss12</dc:creator>
      <dc:date>2013-08-05T09:48:18Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC MC34708 not coming up?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274603#M30219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Satyan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Good Job !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I still suggest you should notice the value of VCC_BP, 3.3V input is &lt;SPAN style="background-color: #ffffff; text-indent: -17px; color: #333333;"&gt;courageous&lt;SPAN class="Apple-converted-space"&gt; design, You are a brave guy ! :smileyhappy: ,Hope you can use standard Voltage (3.7/3.8V) to be BATT input of MC34708 in other designs.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2013 13:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-MC34708-not-coming-up/m-p/274603#M30219</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-08-06T13:52:36Z</dc:date>
    </item>
  </channel>
</rss>