<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Performance SDMA transfer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Performance-SDMA-transfer/m-p/274510#M30185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPBA bus is preferred, since it is dedicated to SDMA, and thus bus swithch, bus competition(specailly for IP bus which connected with a lot of peripheral), if Functional Unit Peripheral used,&amp;nbsp; can be avoided.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Mar 2013 03:13:21 GMT</pubDate>
    <dc:creator>JerryFan</dc:creator>
    <dc:date>2013-03-06T03:13:21Z</dc:date>
    <item>
      <title>Performance SDMA transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-SDMA-transfer/m-p/274509#M30184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'd like to know which type of " uart 2 external memory" sdma transfer is faster. Should i use a shared Uart connect to SDMA via SPBA or is the access over the Functional Unit Peripheral/Burst Units for "normal" Uarts faster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks and regards &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2013 12:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-SDMA-transfer/m-p/274509#M30184</guid>
      <dc:creator>larstraeger</dc:creator>
      <dc:date>2013-02-26T12:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: Performance SDMA transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-SDMA-transfer/m-p/274510#M30185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPBA bus is preferred, since it is dedicated to SDMA, and thus bus swithch, bus competition(specailly for IP bus which connected with a lot of peripheral), if Functional Unit Peripheral used,&amp;nbsp; can be avoided.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2013 03:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-SDMA-transfer/m-p/274510#M30185</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2013-03-06T03:13:21Z</dc:date>
    </item>
  </channel>
</rss>