<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックfeed RTC_XTALI with square wave</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274113#M30100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not found anything about this in the datasheet.&lt;/P&gt;&lt;P&gt;Is it possible to feed the (analog) pin RTC_XTALI from the i.MX28 with a square wave?&lt;/P&gt;&lt;P&gt;For example the square wave output from an external RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Apr 2013 07:47:06 GMT</pubDate>
    <dc:creator>chris321</dc:creator>
    <dc:date>2013-04-18T07:47:06Z</dc:date>
    <item>
      <title>feed RTC_XTALI with square wave</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274113#M30100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not found anything about this in the datasheet.&lt;/P&gt;&lt;P&gt;Is it possible to feed the (analog) pin RTC_XTALI from the i.MX28 with a square wave?&lt;/P&gt;&lt;P&gt;For example the square wave output from an external RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2013 07:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274113#M30100</guid>
      <dc:creator>chris321</dc:creator>
      <dc:date>2013-04-18T07:47:06Z</dc:date>
    </item>
    <item>
      <title>Re: feed RTC_XTALI with square wave</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274114#M30101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, a squared wave can feed the RTC_XTALI. yous be sure that it meets the specs in the RM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Since the internal RTC circuitry is powered from VDDXTAL which &lt;/P&gt;&lt;P&gt;voltage level is around 1.0V, the input 32K clock signal level on&amp;nbsp; &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RTC_XTALI&lt;/STRONG&gt;&lt;/SPAN&gt; should be 1V also. "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2013 17:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274114#M30101</guid>
      <dc:creator>4guin4g4</dc:creator>
      <dc:date>2013-04-22T17:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: feed RTC_XTALI with square wave</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274115#M30102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;I&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;do not want to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;embarrass myself, but in wich Reference Manual did you found this &lt;/SPAN&gt;&lt;/SPAN&gt;sentence?&lt;/P&gt;&lt;P&gt;The downloadable version is Rev. 1, 2010, in this version I did not found it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I feed the XTALI with a 1V squared wave, what about the XTALO? Put it to GND, or let it floated?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2013 06:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/274115#M30102</guid>
      <dc:creator>chris321</dc:creator>
      <dc:date>2013-04-23T06:53:12Z</dc:date>
    </item>
    <item>
      <title>Re: feed RTC_XTALI with square wave</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/2252664#M242550</link>
      <description>l aslo meet the same question with you.&lt;BR /&gt;Refer to below link&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2252653#M242549" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Can-RTC-XTALI-connect-to-RTC-SQW/m-p/2252653#M242549&lt;/A&gt;</description>
      <pubDate>Tue, 02 Dec 2025 02:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/feed-RTC-XTALI-with-square-wave/m-p/2252664#M242550</guid>
      <dc:creator>WSLJ</dc:creator>
      <dc:date>2025-12-02T02:30:06Z</dc:date>
    </item>
  </channel>
</rss>