<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem building alsa-utils in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146834#M301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dingram,&lt;/P&gt;&lt;P&gt;Thanks a lot for the reply. I've managed to build alsa-utils after I've checked the prerequirements packs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now I have another problem with arecord.&lt;/P&gt;&lt;P&gt;I'm trying to test the board mic and speakers with arecord and apaly.&lt;/P&gt;&lt;P&gt;this are my board sound devices:&lt;/P&gt;&lt;P&gt;**** List of CAPTURE Hardware Devices ****&lt;BR /&gt;card 0: mxsevk [mxs-evk], device 0: SGTL5000 SGTL5000-0 []&lt;BR /&gt; Subdevices: 1/1&lt;BR /&gt; Subdevice #0: subdevice #0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;**** List of PLAYBACK Hardware Devices ****&lt;BR /&gt;card 0: mxsevk [mxs-evk], device 0: SGTL5000 SGTL5000-0 []&lt;BR /&gt; Subdevices: 1/1&lt;BR /&gt; Subdevice #0: subdevice #0&lt;BR /&gt;card 1: mxsevk_1 [mxs-evk], device 0: MXS SPDIF mxs spdif-0 []&lt;BR /&gt; Subdevices: 1/1&lt;BR /&gt; Subdevice #0: subdevice #0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I try to record a file with:&lt;/P&gt;&lt;P&gt;arecord -d 5 -c 2 -f S16_LE -N -M -r 8000 -D hw:0,0 file.wav&lt;/P&gt;&lt;P&gt;the file is created but when i play it :&lt;/P&gt;&lt;P&gt;aplay file.wav&lt;/P&gt;&lt;P&gt;no sound is heard.&lt;/P&gt;&lt;P&gt;I've tested aplay with an downloaded .wav file and it work OK.&lt;/P&gt;&lt;P&gt;But the file created by arecord has no sound or I'm not setting the params&amp;nbsp;correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If some one could help me with this I will&amp;nbsp;highly&amp;nbsp;appreciate it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Mar 2012 19:10:29 GMT</pubDate>
    <dc:creator>GabrielO</dc:creator>
    <dc:date>2012-03-21T19:10:29Z</dc:date>
    <item>
      <title>Problem building alsa-utils</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146832#M299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I can't build alsa-utils. I've managed to build alsa-lib in ltib but I'm getting an error when I'm trying to build alsa-utils:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lucid@ubuntu:~/ltib$ ./ltib -m scbuild -p alsa-utils.spec&lt;/P&gt;&lt;P&gt;Processing: alsa-utils&lt;BR /&gt;========================&lt;BR /&gt;Build path taken because: directory build, build key set, no prebuilt rpm,&lt;/P&gt;&lt;P&gt;rpmbuild --dbpath /home/lucid/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/lucid/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/lucid/ltib/tmp' --define '_rpmdir /home/lucid/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/lucid/ltib/dist/lfs-5.1/alsa-utils/alsa-utils.spec&lt;BR /&gt;Building target platforms: arm&lt;BR /&gt;Building for target arm&lt;BR /&gt;Executing(%build): /bin/sh -e /home/lucid/ltib/tmp/rpm-tmp.49584&lt;BR /&gt;+ umask 022&lt;BR /&gt;+ cd /home/lucid/ltib/rpm/BUILD&lt;BR /&gt;+ cd alsa-utils-1.0.11rc2&lt;BR /&gt;+ [ -n ]&lt;BR /&gt;+ [ arm = m68knommu ]&lt;BR /&gt;+ eval ./configure --prefix=/usr --host=arm-linux --build=i686-pc-linux-gnu -C&lt;BR /&gt;+ ./configure --prefix=/usr --host=arm-linux --build=i686-pc-linux-gnu -C&lt;BR /&gt;configure: loading cache config.cache&lt;BR /&gt;checking for a BSD-compatible install... /usr/bin/install -c&lt;BR /&gt;checking whether build environment is sane... yes&lt;BR /&gt;checking for gawk... gawk&lt;BR /&gt;checking whether make sets $(MAKE)... yes&lt;BR /&gt;checking for arm-linux-strip... arm-linux-strip&lt;BR /&gt;checking whether NLS is requested... yes&lt;BR /&gt;checking for msgfmt... /usr/bin/msgfmt&lt;BR /&gt;checking for gmsgfmt... /usr/bin/msgfmt&lt;BR /&gt;checking for xgettext... /usr/bin/xgettext&lt;BR /&gt;checking for msgmerge... /usr/bin/msgmerge&lt;BR /&gt;checking for style of include used by make... GNU&lt;BR /&gt;checking for arm-linux-gcc... gcc&lt;BR /&gt;checking for C compiler default output file name... a.out&lt;BR /&gt;checking whether the C compiler works... yes&lt;BR /&gt;checking whether we are cross compiling... yes&lt;BR /&gt;checking for suffix of executables... &lt;BR /&gt;checking for suffix of object files... o&lt;BR /&gt;checking whether we are using the GNU C compiler... yes&lt;BR /&gt;checking whether gcc accepts -g... yes&lt;BR /&gt;checking for gcc option to accept ANSI C... none needed&lt;BR /&gt;checking dependency style of gcc... gcc3&lt;BR /&gt;checking build system type... i686-pc-linux-gnu&lt;BR /&gt;checking host system type... arm-unknown-linux-gnu&lt;BR /&gt;checking for ld used by GCC... ld&lt;BR /&gt;checking if the linker (ld) is GNU ld... yes&lt;BR /&gt;checking for shared library run path origin... done&lt;BR /&gt;checking whether NLS is requested... yes&lt;BR /&gt;checking for GNU gettext in libc... yes&lt;BR /&gt;checking whether to use NLS... yes&lt;BR /&gt;checking where the gettext function comes from... libc&lt;BR /&gt;checking for cross-compiler... gcc&lt;BR /&gt;checking for arm-linux-gcc... (cached) gcc&lt;BR /&gt;checking whether we are using the GNU C compiler... (cached) yes&lt;BR /&gt;checking whether gcc accepts -g... (cached) yes&lt;BR /&gt;checking for gcc option to accept ANSI C... (cached) none needed&lt;BR /&gt;checking dependency style of gcc... (cached) gcc3&lt;BR /&gt;checking for a BSD-compatible install... /usr/bin/install -c&lt;BR /&gt;checking whether ln -s works... yes&lt;BR /&gt;checking for ALSA CFLAGS... &lt;BR /&gt;checking for ALSA LDFLAGS... -lasound -lm -ldl -lpthread&lt;BR /&gt;checking for libasound headers version &amp;gt;= 1.0.9... found.&lt;BR /&gt;checking for snd_ctl_open in -lasound... yes&lt;BR /&gt;checking how to run the C preprocessor... gcc -E&lt;BR /&gt;checking for egrep... grep -E&lt;BR /&gt;checking for ANSI C header files... yes&lt;BR /&gt;checking for initscr in -lncurses... no&lt;BR /&gt;checking for initscr in -lcurses... no&lt;BR /&gt;configure: error: this packages requires a curses library&lt;BR /&gt;error: Bad exit status from /home/lucid/ltib/tmp/rpm-tmp.49584 (%build)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can any one help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 16:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146832#M299</guid>
      <dc:creator>GabrielO</dc:creator>
      <dc:date>2012-03-21T16:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: Problem building alsa-utils</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146833#M300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gabriel:&lt;/P&gt;&lt;P&gt;If you run './ltib -c', scroll down to the "Package list", highlight "alsa-utils" and select "Help", "Selects: PKG_ALSA_LIB &amp;amp;&amp;amp; PKG_NCURSES" tells you these are required.&amp;nbsp; When you select "alsa-utils", the two requirements will be selected automatically [...].&amp;nbsp; When 'ltib' rebuilds, this should fix your "configure: error: this packages requires a curses library".&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Darrell&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 17:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146833#M300</guid>
      <dc:creator>dingram1z</dc:creator>
      <dc:date>2012-03-21T17:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: Problem building alsa-utils</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146834#M301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dingram,&lt;/P&gt;&lt;P&gt;Thanks a lot for the reply. I've managed to build alsa-utils after I've checked the prerequirements packs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now I have another problem with arecord.&lt;/P&gt;&lt;P&gt;I'm trying to test the board mic and speakers with arecord and apaly.&lt;/P&gt;&lt;P&gt;this are my board sound devices:&lt;/P&gt;&lt;P&gt;**** List of CAPTURE Hardware Devices ****&lt;BR /&gt;card 0: mxsevk [mxs-evk], device 0: SGTL5000 SGTL5000-0 []&lt;BR /&gt; Subdevices: 1/1&lt;BR /&gt; Subdevice #0: subdevice #0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;**** List of PLAYBACK Hardware Devices ****&lt;BR /&gt;card 0: mxsevk [mxs-evk], device 0: SGTL5000 SGTL5000-0 []&lt;BR /&gt; Subdevices: 1/1&lt;BR /&gt; Subdevice #0: subdevice #0&lt;BR /&gt;card 1: mxsevk_1 [mxs-evk], device 0: MXS SPDIF mxs spdif-0 []&lt;BR /&gt; Subdevices: 1/1&lt;BR /&gt; Subdevice #0: subdevice #0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I try to record a file with:&lt;/P&gt;&lt;P&gt;arecord -d 5 -c 2 -f S16_LE -N -M -r 8000 -D hw:0,0 file.wav&lt;/P&gt;&lt;P&gt;the file is created but when i play it :&lt;/P&gt;&lt;P&gt;aplay file.wav&lt;/P&gt;&lt;P&gt;no sound is heard.&lt;/P&gt;&lt;P&gt;I've tested aplay with an downloaded .wav file and it work OK.&lt;/P&gt;&lt;P&gt;But the file created by arecord has no sound or I'm not setting the params&amp;nbsp;correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If some one could help me with this I will&amp;nbsp;highly&amp;nbsp;appreciate it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 19:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-building-alsa-utils/m-p/146834#M301</guid>
      <dc:creator>GabrielO</dc:creator>
      <dc:date>2012-03-21T19:10:29Z</dc:date>
    </item>
  </channel>
</rss>